<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: MPC 8280</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246594#M6528</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure you followed the steps from 8280_AM_README.txt:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"NOTE: ROM Version target&lt;/P&gt;&lt;P&gt;------------------------&lt;/P&gt;&lt;P&gt;The ROM version target creates a bootable image for the application at 0xFFF00000.&lt;/P&gt;&lt;P&gt;To boot the ROM image you must assure first that the Hard Configuration Word (HCW)&lt;/P&gt;&lt;P&gt;stored in the first flash sector is set to boot-high. To change the value of the &lt;/P&gt;&lt;P&gt;HCW you should follow the next steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Save First Flash Sector to a binary file&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. Modify using a hex-editor the HCW in the above file from 0x0A068700&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; to 0x08040700 (to set boot high, move the exception vectors to&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xFFFn_nnnn and set an initial IMMR value of 0xF0000000)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3. Erase the first flash sector using the Flash Programmer &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4. Re-flash the first sector with the modified binary file&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5. Reset the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After writing to flash the ROM image of the default application, the board should &lt;/P&gt;&lt;P&gt;output "Welcome to CodeWarrior!" on the serial monitor port (SMC1) after reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMPORTANT NOTE !!! &lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;If the board is set to boot-high you must use 8280_AM_Rattler_init_high.cfg and &lt;/P&gt;&lt;P&gt;8280_AM_Rattler_init_ROM_high.cfg as debugger and Flash Programmer target initialization &lt;/P&gt;&lt;P&gt;files. &lt;/P&gt;&lt;P&gt;Both files can be found in &amp;lt;CodeWarrior&amp;gt;\PowerPC_EABI_Support\Initialization_Files\Jtag&lt;/P&gt;&lt;P&gt;folder."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jan 2014 10:16:18 GMT</pubDate>
    <dc:creator>addiyi</dc:creator>
    <dc:date>2014-01-27T10:16:18Z</dc:date>
    <item>
      <title>MPC 8280</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246589#M6523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using cw 8.8 with MPC 8280. I want to run my application from Flash. What steps are to be followed for it? Is 'ROM version' required for this purpose?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2014 09:03:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246589#M6523</guid>
      <dc:creator>monalihaware</dc:creator>
      <dc:date>2014-01-21T09:03:16Z</dc:date>
    </item>
    <item>
      <title>Re: MPC 8280</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246590#M6524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To download an application in flash memory, you should use ROM version for Build Configurations option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2014 09:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246590#M6524</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2014-01-21T09:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: MPC 8280</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246591#M6525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried doing that. I even wrote an LCF file also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually i have an application with prints a statement through serial port(using SCM uart). NOw when the application is run in 'Debug' version, i see the output in the hyperterminal. So debug version has no problem. But whereas when i go for ROM version, and after dumping the program in FLASH, On power up, hyoerterminal comes blank. Seems that code is not burned properly in Flash. How to find regarding where the mistake is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Monali Haware&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Corporate R&amp;amp;D&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Electronic Corporation of India Ltd(ECIL)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A Government of India Enterprise(Department of Atomic Energy)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ECIL Post, Hyderabad, A.P (India)-500062&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ph No: +91-40-27186812,Fax No: +91-40-27121318&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mail id:monali@ecil.co.in&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;URL:www.ecil.co.in&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt;		&lt;/P&gt;&lt;P&gt;			&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			-- Original Message --&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			From: Adrian-Mihai Stoica &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			To: monali haware &amp;lt;monali@ecil.co.in&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			Date: Tue, 21 Jan 2014 02:38:55 -0700&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			Subject: Re:  - MPC 8280&lt;/P&gt;&lt;P&gt;                                                                                MPC 8280 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;reply from &amp;lt;https://community.freescale.com/people/addiyi?et=watches.email.thread&amp;gt;Adrian-Mihai Stoica in Classic/Legacy CodeWarrior - &amp;lt;https://community.freescale.com/message/374772?et=watches.email.thread#374772&amp;gt;View the full discussion&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;To download an application in flash memory, you should use ROM version for Build Configurations option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;										&lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;												&lt;/P&gt;&lt;P&gt;Reply to this message by replying to this email, or &amp;lt;https://community.freescale.com/message/374772?et=watches.email.thread#374772&amp;gt;go to the message on Freescale Community &lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;												&lt;/P&gt;&lt;P&gt;Start a new discussion in Classic/Legacy CodeWarrior by &amp;lt;discussions-community-codewarrior-classic@freescale.hosted.jivesoftware.com&amp;gt;email or at &amp;lt;https://community.freescale.com/choose-container.jspa?contentType=1&amp;amp;amp;containerType=14&amp;amp;amp;container=2031&amp;amp;amp;et=watches.email.thread&amp;gt;Freescale Community &lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;												&lt;/P&gt;&lt;P&gt;Following &amp;lt;https://community.freescale.com/message/374772?et=watches.email.thread#374772&amp;gt;MPC 8280 in these streams: Inbox                                                                                &lt;/P&gt;&lt;P&gt;::DISCLAIMER::&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2014 10:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246591#M6525</guid>
      <dc:creator>monalihaware</dc:creator>
      <dc:date>2014-01-21T10:00:22Z</dc:date>
    </item>
    <item>
      <title>Re: MPC 8280</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246592#M6526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you use init_file for ROM (should be something like: 8280_init_ROM.cfg), when you download the application to target board? Also, please take a look in 8280_AM_README.txt (available in PowerPC_EABI_Support\Documentation\PQ2\), ROM Version target section. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2014 10:26:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246592#M6526</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2014-01-21T10:26:55Z</dc:date>
    </item>
    <item>
      <title>Re: MPC 8280</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246593#M6527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using it indeed. sending you 1 copy. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Flash base address is 0x00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDRAM base address is 0x20000000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This same file i had been using  with 'debug version'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Monali&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;	&lt;/P&gt;&lt;P&gt;		&lt;/P&gt;&lt;P&gt;			&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			-- Original Message --&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			From: Adrian-Mihai Stoica &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			To: monali haware &amp;lt;monali@ecil.co.in&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			Date: Tue, 21 Jan 2014 03:27:55 -0700&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;			Subject: Re:  - MPC 8280&lt;/P&gt;&lt;P&gt;                                                                                MPC 8280 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;reply from &amp;lt;https://community.freescale.com/people/addiyi?et=watches.email.thread&amp;gt;Adrian-Mihai Stoica in Classic/Legacy CodeWarrior - &amp;lt;https://community.freescale.com/message/374776?et=watches.email.thread#374776&amp;gt;View the full discussion&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;Did you use init_file for ROM (should be something like: 8280_init_ROM.cfg), when you download the application to target board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;									&lt;/P&gt;&lt;P&gt;										&lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;												&lt;/P&gt;&lt;P&gt;Reply to this message by replying to this email, or &amp;lt;https://community.freescale.com/message/374776?et=watches.email.thread#374776&amp;gt;go to the message on Freescale Community &lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;												&lt;/P&gt;&lt;P&gt;Start a new discussion in Classic/Legacy CodeWarrior by &amp;lt;discussions-community-codewarrior-classic@freescale.hosted.jivesoftware.com&amp;gt;email or at &amp;lt;https://community.freescale.com/choose-container.jspa?contentType=1&amp;amp;amp;containerType=14&amp;amp;amp;container=2031&amp;amp;amp;et=watches.email.thread&amp;gt;Freescale Community &lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;											&lt;/P&gt;&lt;P&gt;												&lt;/P&gt;&lt;P&gt;Following &amp;lt;https://community.freescale.com/message/374776?et=watches.email.thread#374776&amp;gt;MPC 8280 in these streams: Inbox                                                                                &lt;/P&gt;&lt;P&gt;::DISCLAIMER::&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jan 2014 03:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246593#M6527</guid>
      <dc:creator>monalihaware</dc:creator>
      <dc:date>2014-01-25T03:39:36Z</dc:date>
    </item>
    <item>
      <title>Re: MPC 8280</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246594#M6528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please make sure you followed the steps from 8280_AM_README.txt:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"NOTE: ROM Version target&lt;/P&gt;&lt;P&gt;------------------------&lt;/P&gt;&lt;P&gt;The ROM version target creates a bootable image for the application at 0xFFF00000.&lt;/P&gt;&lt;P&gt;To boot the ROM image you must assure first that the Hard Configuration Word (HCW)&lt;/P&gt;&lt;P&gt;stored in the first flash sector is set to boot-high. To change the value of the &lt;/P&gt;&lt;P&gt;HCW you should follow the next steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Save First Flash Sector to a binary file&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. Modify using a hex-editor the HCW in the above file from 0x0A068700&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; to 0x08040700 (to set boot high, move the exception vectors to&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xFFFn_nnnn and set an initial IMMR value of 0xF0000000)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3. Erase the first flash sector using the Flash Programmer &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4. Re-flash the first sector with the modified binary file&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5. Reset the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After writing to flash the ROM image of the default application, the board should &lt;/P&gt;&lt;P&gt;output "Welcome to CodeWarrior!" on the serial monitor port (SMC1) after reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMPORTANT NOTE !!! &lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;If the board is set to boot-high you must use 8280_AM_Rattler_init_high.cfg and &lt;/P&gt;&lt;P&gt;8280_AM_Rattler_init_ROM_high.cfg as debugger and Flash Programmer target initialization &lt;/P&gt;&lt;P&gt;files. &lt;/P&gt;&lt;P&gt;Both files can be found in &amp;lt;CodeWarrior&amp;gt;\PowerPC_EABI_Support\Initialization_Files\Jtag&lt;/P&gt;&lt;P&gt;folder."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2014 10:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC-8280/m-p/246594#M6528</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2014-01-27T10:16:18Z</dc:date>
    </item>
  </channel>
</rss>