<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Classic codewarrior 7.1.1, Windows 7 64-bit, and PEmicro debugger incompatible</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Classic-codewarrior-7-1-1-Windows-7-64-bit-and-PEmicro-debugger/m-p/237652#M6510</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;I am recently responsible for maintaining a codebase with a coldfire V2 target (MCF52277) that includes MQX RTOS 3.0.1.&amp;nbsp; This codebase will compile under codewarrior 7.1.1.&amp;nbsp; I would like to use the existing tool chain (codewarrior 7.1.1 and PEmicro Coldfire Multilink debugger, USB-ML-CFE) to compile, debug, and build the firmware.&amp;nbsp; I have a Windows 7 64-bit machine and have been unsuccessful at using the PEmicro debugger with Codewarrior.&amp;nbsp; I tried the following two methods and both failed.&amp;nbsp; Do you have any suggestions?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Method #1&lt;/P&gt;&lt;P&gt;I followed the freescale recommended procedure to install classic codewarrior 7.1.1 on a 64 bit machine (see instructions here&amp;nbsp; &lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/soft_dev_tools/doc/app.../AN3936.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app.../AN3936.pdf&lt;/A&gt; ).&amp;nbsp; I installed Windows Virtual PC and Windows XP mode.&amp;nbsp; I installed codewarrior 7.1 in the windows XP virtual machine.&amp;nbsp; This allowed me to compile my code.&amp;nbsp; I plug in the pemicro debugger to the USB port and my Windows 7 device found it (latest pemicro drivers were installed).&amp;nbsp; However, when I try to attach in XP mode, it will not attach the USB device.&amp;nbsp;&amp;nbsp; I most cases when I try to attached on several USB ports, it will not attach to the virtual machine and so I can not run the debugger.&amp;nbsp; In a few attempts, the virtual machine did attach, but the lights on the USB multilink turn off and a message appears in XP Mode that the USB device has become non-functional.&amp;nbsp; I have tried multiple PE debuggers and encountered the same problem.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Method #2&lt;/P&gt;&lt;P&gt;I installed codewarrior 7.1.1 directly on my Windows 7 64 bit machine.&amp;nbsp; There were a view warnings/errors during installation, but I ignored these and codewarrior seemed to install ok.&amp;nbsp; I was able to compile the code.&amp;nbsp; The USB Multilink 2.0 device shows up in the windows devices list.&amp;nbsp; However, when I try to connect or run the debugger, Codewarrior produces the following error "ColdFire PE Protocol Adapter: No USB connection found" message.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I appreciate your help. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Mar 2013 20:16:06 GMT</pubDate>
    <dc:creator>mikegr</dc:creator>
    <dc:date>2013-03-22T20:16:06Z</dc:date>
    <item>
      <title>Classic codewarrior 7.1.1, Windows 7 64-bit, and PEmicro debugger incompatible</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Classic-codewarrior-7-1-1-Windows-7-64-bit-and-PEmicro-debugger/m-p/237652#M6510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All,&lt;/P&gt;&lt;P&gt;I am recently responsible for maintaining a codebase with a coldfire V2 target (MCF52277) that includes MQX RTOS 3.0.1.&amp;nbsp; This codebase will compile under codewarrior 7.1.1.&amp;nbsp; I would like to use the existing tool chain (codewarrior 7.1.1 and PEmicro Coldfire Multilink debugger, USB-ML-CFE) to compile, debug, and build the firmware.&amp;nbsp; I have a Windows 7 64-bit machine and have been unsuccessful at using the PEmicro debugger with Codewarrior.&amp;nbsp; I tried the following two methods and both failed.&amp;nbsp; Do you have any suggestions?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Method #1&lt;/P&gt;&lt;P&gt;I followed the freescale recommended procedure to install classic codewarrior 7.1.1 on a 64 bit machine (see instructions here&amp;nbsp; &lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/soft_dev_tools/doc/app.../AN3936.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app.../AN3936.pdf&lt;/A&gt; ).&amp;nbsp; I installed Windows Virtual PC and Windows XP mode.&amp;nbsp; I installed codewarrior 7.1 in the windows XP virtual machine.&amp;nbsp; This allowed me to compile my code.&amp;nbsp; I plug in the pemicro debugger to the USB port and my Windows 7 device found it (latest pemicro drivers were installed).&amp;nbsp; However, when I try to attach in XP mode, it will not attach the USB device.&amp;nbsp;&amp;nbsp; I most cases when I try to attached on several USB ports, it will not attach to the virtual machine and so I can not run the debugger.&amp;nbsp; In a few attempts, the virtual machine did attach, but the lights on the USB multilink turn off and a message appears in XP Mode that the USB device has become non-functional.&amp;nbsp; I have tried multiple PE debuggers and encountered the same problem.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Method #2&lt;/P&gt;&lt;P&gt;I installed codewarrior 7.1.1 directly on my Windows 7 64 bit machine.&amp;nbsp; There were a view warnings/errors during installation, but I ignored these and codewarrior seemed to install ok.&amp;nbsp; I was able to compile the code.&amp;nbsp; The USB Multilink 2.0 device shows up in the windows devices list.&amp;nbsp; However, when I try to connect or run the debugger, Codewarrior produces the following error "ColdFire PE Protocol Adapter: No USB connection found" message.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I appreciate your help. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2013 20:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Classic-codewarrior-7-1-1-Windows-7-64-bit-and-PEmicro-debugger/m-p/237652#M6510</guid>
      <dc:creator>mikegr</dc:creator>
      <dc:date>2013-03-22T20:16:06Z</dc:date>
    </item>
    <item>
      <title>Re: Classic codewarrior 7.1.1, Windows 7 64-bit, and PEmicro debugger incompatible</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Classic-codewarrior-7-1-1-Windows-7-64-bit-and-PEmicro-debugger/m-p/237653#M6511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to get Method #1 in original description working using Windows XP Mode, although it is flakey.&amp;nbsp; I am not sure what fixed the problem, but I downloaded and installed the latest firmware to the PE USB Multilink device.&amp;nbsp; I also installed the latest PE driver both on the Windows 7 machine AND the virtual Windows XP machine.&amp;nbsp; Finally, I made the observation that when attaching the USB device for the first time to the virtual machine, the debugger turns off.&amp;nbsp; If you then remove the USB connector from the PC and plug it back in, it will be attached to the virtual PC. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2013 22:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Classic-codewarrior-7-1-1-Windows-7-64-bit-and-PEmicro-debugger/m-p/237653#M6511</guid>
      <dc:creator>mikegr</dc:creator>
      <dc:date>2013-03-28T22:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: Classic codewarrior 7.1.1, Windows 7 64-bit, and PEmicro debugger incompatible</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Classic-codewarrior-7-1-1-Windows-7-64-bit-and-PEmicro-debugger/m-p/237654#M6512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found out later that my answer above was only partially correct.&amp;nbsp; I was able to use the flash programmer to download data but not step through the debugger.&amp;nbsp; I now have the debugger working completely.&amp;nbsp; See thread below for final answer&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/323667"&gt;https://community.freescale.com/message/323667&lt;/A&gt;#&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 23:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Classic-codewarrior-7-1-1-Windows-7-64-bit-and-PEmicro-debugger/m-p/237654#M6512</guid>
      <dc:creator>mikegr</dc:creator>
      <dc:date>2013-04-11T23:37:27Z</dc:date>
    </item>
  </channel>
</rss>