<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How-to Directly Install CodeWarrior 6.3 Classic in Windows 10 or 7 x64 (Unofficial Method) in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220599#M6445</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have installed CW 6.3 on Windows 10 64bit Operating System using the new one step method posted here by Rodney. I’m using the P&amp;amp;E Multilink/Cyclone Pro connection (USB MON08 Multilink) with HC08 (HC908QB8).&lt;/P&gt;&lt;P&gt;I can make the Project and when I enter in debug mode, the target is automatically detected. However, when I start the execution, it is halted and stops in a specific instruction every time. I’ve noticed that it is able to run Step Over, but the execution is also halted in the same instruction after a few steps (it’s an endless loop). I can’t set any breakpoints either, it shows an error message on console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m able to run without problems the debug session with the same hardware using CW 6.2 on Windows 7 32bit Operating System. I’ve noticed using the Step Over that it often shows on console “Preset breakpoint encountered” before going to the next step.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’ve also compared P&amp;amp;E’s debugger DLL versions for HC08 devices, the ICD08sw_dll.dll. It’s inside P&amp;amp;E folder. I checked the versions for HC908QB8 in ngs_devices_hc08.ini file. In CW 6.2 on Windows 7, in which I can set breakpoints and run the program smoothly, the version used is ICD08sw_dll_v230.dll. &amp;nbsp;But CW 6.3 on Windows 10 was using ICD08sw_dll_v681.dll. I changed the configuration file so that CW 6.3 would use v230 DLLs in the fields PROG, ICD and PROG_INTERACTIVE. After that, I added wdapi900.dll from a CW 10.7 installation, so that my target coud be recognized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Despite that, when the program starts, the execution is still halted on the same instruction I mentioned previously. But Step Over can now reach more instructions than with v681 DLLs. I still can’t set breakpoints, but now the error messages are displayed in two separate HI-WAVE windows. "Could not set the hardware breakpoint at address $(address)", immediately followed by "Was not able to set the breakpoint at $(adress)".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the problems seems to be related with the breakpoints, that can’t be set. The execution seems to be halted because the debugger can’t set and clear breakpoints. I reached that conclusion since during the correct single-step execution (on Windows 7) the message “Preset breakpoint encountered” is shown several times.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would really appreciate if someone could help me solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 May 2020 20:32:29 GMT</pubDate>
    <dc:creator>hiandra_tomasi</dc:creator>
    <dc:date>2020-05-27T20:32:29Z</dc:date>
    <item>
      <title>How-to Directly Install CodeWarrior 6.3 Classic in Windows 10 or 7 x64 (Unofficial Method)</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220513#M6359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline; font-size: 14pt; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;CodeWarrior 6.3 is for most RS08, S08, ColdFire V1 Processors*&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&lt;SPAN style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 8pt;"&gt;*&lt;STRONG&gt;Not&lt;/STRONG&gt;&lt;/SPAN&gt; &lt;SPAN style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;&lt;SPAN style="font-size: 11px; line-height: 16px;"&gt;&lt;STRONG&gt;compatibile&lt;/STRONG&gt;&lt;/SPAN&gt; &lt;SPAN style="font-size: 8pt;"&gt;with (S08: RN, RNA, PA, PT, &lt;SPAN style="color: #646464; font-family: Arial, sans-serif;"&gt;Kinetis (including Tower), ColdFire V2&lt;/SPAN&gt; ...)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px; font-family: arial, helvetica, sans-serif;"&gt;&lt;STRONG&gt;This post describes installing &lt;A href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fsoftware-development-tools%2Fcodewarrior-development-tools%2Fcodewarrior-development-studios%2Fcodewarrior-for-microcontrollers%2Fcodewarrior-for-microcontrollers-classic-ide-rs08-hcs08-coldfire-v1-v6.3%3ACW-MICROCONTROLLERS" rel="nofollow noopener noreferrer" target="_blank"&gt;CodeWarrior for Microcontrollers (Classic IDE) - RS08/HC(S)08, ColdFire V1 v6.3&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px; font-family: arial, helvetica, sans-serif;"&gt;&lt;STRONG&gt;on 64-bit modern versions of Microsoft's operating systems e.g. Windows 7 and Windows 10.&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-size: 12px; font-family: arial, helvetica, sans-serif;"&gt;Some people could argue to use the Eclipse-based CodeWarrior and they have their points (some devices and situations require it). On the other hand Freescale long knew that Eclipse-based CodeWarrior is cumbersome. Here is a great article (now only available by archive since it was deleted) article by James Trudeau (formally of Freescale) about his teams unfinished but thoughtful effort: &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fweb.archive.org%2Fweb%2F20130401224611%2Fhttps%3A%2F%2Fcommunity.freescale.com%2Fcommunity%2Fthe-embedded-beat%2Fblog%2F2012%2F09%2F25%2Fcodewarrior-ide-v103-a-whole-new-perspective" rel="nofollow noopener noreferrer" target="_blank"&gt;CodeWarrior 10.3 a new perspective&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12px;"&gt;&lt;SPAN style="color: #000000; font-family: arial, helvetica, sans-serif;"&gt;Also&lt;/SPAN&gt; &lt;SPAN style="color: #000000; font-family: arial, helvetica, sans-serif;"&gt;for those who fondly remember programming Motorola parts with an Metrowerks IDE, give this a shot.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Typically you will get the error "CodeWarrior Development Studio for Microcontrollers v6.3 is not compatible with Windows XP 64-bit installations" when trying to install under Windows 7/10 x64.&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE __default_attr="warning" __jive_macro_name="alert" alert="warning" class="jive_text_macro jive_macro_alert" modifiedtitle="true"&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN style="font-size: 22px;"&gt;&lt;EM&gt;These methods are&amp;nbsp;UN&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 22px;"&gt;&lt;EM&gt;OFFICIAL&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 22px;"&gt;&lt;EM&gt;&amp;nbsp;and are not supported by NXP&lt;/EM&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 22px; "&gt;&lt;EM&gt;–&amp;nbsp;&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 22px;"&gt;&lt;EM&gt;Do not contact NXP support for these methods.&amp;nbsp;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/PRE&gt;&lt;PRE __default_attr="success" __jive_macro_name="alert" alert="success" class="jive_text_macro jive_macro_alert" modifiedtitle="true"&gt;&lt;P&gt;&lt;SPAN style="font-size: 30px;"&gt;&lt;STRONG&gt;NEW METHOD - ONE STEP :&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;UNOFFICIAL community version Special Edition CodeWarrior "6.3.2"&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Download and install here:&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;&lt;A class="link-bare" href="http://mirror.lug.udel.edu/pub/community-projects/freescale/cw-632-se-installer-r1.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;http://mirror.lug.udel.edu/pub/community-projects/freescale/cw-632-se-installer-r1.exe&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Includes all updates, fixes, and&amp;nbsp;service packs&lt;/SPAN&gt;&lt;/P&gt;&lt;/PRE&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11px;"&gt;For P&amp;amp;E Micro&amp;nbsp;- just check the box for the install options - no extra steps needed&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11px;"&gt;For USBDM &lt;SPAN&gt;- just check the box for the install options - use the USBDM firmware updater (start menu) if needed&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="; text-decoration: underline; font-size: 11px;"&gt;&lt;STRONG&gt;&lt;SPAN style="font-size: 22px;"&gt;DONE&amp;nbsp;–&amp;nbsp;NO EXTRA STEPS NEEDED&lt;/SPAN&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13px;"&gt;Any issues?&amp;nbsp;Ask questions in this forum.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE __default_attr="info" __jive_macro_name="alert" alert="info" class="jive_text_macro jive_macro_alert" modifiedtitle="true"&gt;&lt;P style="text-align: left;"&gt;&lt;SPAN style="font-size: 30px;"&gt;&lt;STRONG&gt;OLD&amp;nbsp;METHOD:&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; font-size: 14pt;"&gt;Partial instructional video&lt;STRONG&gt;:&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; font-size: 14pt;"&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fyoutu.be%2FvtIHv-ze1DQ" rel="nofollow noopener noreferrer" style="font-size: 11px; color: #167ac6; font-family: Roboto, arial, sans-serif;" target="_blank"&gt;&lt;SPAN style="font-size: 12pt;"&gt;F&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;SPAN style="font-size: 12pt;"&gt;reescale/NXP CodeWarrior Classic 6.3 Windows 10 x64 HCS08 RS08 CFV1 P&amp;amp;E Micro BDM -&lt;/SPAN&gt; YouTube&lt;/SPAN&gt;&lt;/A&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Note: The video doesn't show the PE_Plugin.dll update or the P&amp;amp;E fix. Also the files names may be a little different. &amp;nbsp;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt;"&gt;&lt;EM&gt;&lt;STRONG&gt;Main Installation steps (Windows 7/10 64-bit)&lt;/STRONG&gt;:&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt;"&gt;&lt;SPAN style="line-height: 1.5em;"&gt;1. Download: CodeWarrior for Micro-controllers &lt;A href="https://freescaleesd.flexnetoperations.com/337170/441/8309441/CodeWarrior%20for%20Microcontrollers%20(RS08HC(S)08-ColdFire%20V1)%20v6.3.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;here&lt;/A&gt;&amp;nbsp;(or here&amp;nbsp;&lt;A href="https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=5901331" rel="nofollow noopener noreferrer" target="_blank"&gt;alt link&lt;/A&gt;):&lt;/SPAN&gt;&lt;SPAN style="color: #2873ee;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="line-height: 1.5em;"&gt;which is for most RS08, S08, ColdFire V1&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif; font-size: 10pt;"&gt;2. Install &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.7-zip.org%2F" rel="nofollow noopener noreferrer" style="font-family: arial, helvetica, sans-serif;" target="_blank"&gt;7Zip&lt;/A&gt;, and extract the exe&amp;nbsp;(instead of running the exe; right click it and extract) to a folder&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;3. Download and e&lt;SPAN style="font-size: 13.3333330154419px;"&gt;xtract&lt;/SPAN&gt; &lt;EM&gt;RemoveOSCheck.vbs.zip&lt;/EM&gt; (attached below or &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fpastebin.com%2FRUTqukN3" rel="nofollow noopener noreferrer" target="_blank"&gt;mirror&lt;/A&gt;) and move it your extracted folder.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;4. &lt;SPAN style="font-size: 10pt;"&gt;Drag and drop&lt;/SPAN&gt; CW_MCUs_V6_3.msi onto RemoveOSCheck.vbs giving a series of messages like "Launch Conditions Removed"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;5. Run the &lt;STRONG&gt;&lt;EM&gt;setup.exe&lt;/EM&gt;&lt;/STRONG&gt; file located in the&lt;/SPAN&gt; &lt;SPAN style="font-size: 13.3333330154419px; font-family: arial, helvetica, sans-serif;"&gt;extracted folder. Do&amp;nbsp;&lt;SPAN style="font-size: 15px;"&gt;a&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 15px; line-height: 1.5em; font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;custom install and uncheck the ICEbase and Softec under debugger drivers in the customization&amp;nbsp;options. When you get a prompt skip the auto-updates process.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="; font-size: 8pt; line-height: 1.5em; font-family: arial, helvetica, sans-serif;"&gt;&lt;STRONG&gt;Note&lt;/STRONG&gt;: If you get an error &lt;STRONG&gt;"The wizard was interrupted ..."&lt;/STRONG&gt; see this link&amp;nbsp;&lt;A class="link-titled" href="#comment-1103754" rel="nofollow noopener noreferrer" title="https://community.nxp.com/thread/302974#comment-1095686" target="_blank"&gt;#comment-1103754&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; font-family: arial, helvetica, sans-serif;"&gt;6. Install the updates listed below (most are not offered by the updater).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; font-family: arial, helvetica, sans-serif;"&gt;7. In the CW6.3 install folder in&amp;nbsp;Program Files (x86) folder, under&amp;nbsp;bin\plugins\com, *replace*&amp;nbsp;PE_Plugin.dll with the one extracted from zip&amp;nbsp;attachment at the bottom of this post.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; font-family: arial, helvetica, sans-serif;"&gt;8. Run the software as administrator (using right click menu) at least once.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;9. If your code is 64k or smaller use the free Special Edition license below.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;EM style="font-size: large; "&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;&lt;SPAN style="font-size: large;"&gt;&lt;STRONG&gt;License Issues or&amp;nbsp;lab cloning&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: large;"&gt;:&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;This license linked below was posted online by Freescale&amp;nbsp;and is open to&amp;nbsp;ANY&amp;nbsp;hostid and doesn't expire which great for cloning machines. Is it a special edition license file limited to 64K or less of code.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Assuming 7 or better, goto the "Start menu", type Notepad, right click the icon select&amp;nbsp;&lt;STRONG&gt;run as administrator&lt;/STRONG&gt;. Goto File -&amp;gt; Open and goto&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;C:\Program Files (x86)\Freescale\CodeWarrior for Microcontrollers V6.3\license.dat, then&amp;nbsp;&lt;STRONG&gt;open this &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fweb.archive.org%2Fweb%2F20160409223744%2Fhttps%3A%2F%2Fcache.nxp.com%2Ffiles%2Fsoft_dev_tools%2Fsoftware%2Fapp_software%2Fcode_examples%2Flicense.dat" rel="nofollow noopener noreferrer" target="_blank"&gt;license link (Freescale archive)&lt;/A&gt;&amp;nbsp;to view the file&amp;nbsp;&lt;/STRONG&gt;in your browser. Highlight all the text (starting with # lines and down) in the browser and COPY and in notepad PASTE&amp;nbsp;it over ALL the existing text in license.dat, then goto File -&amp;gt; Save. &amp;nbsp;This avoids any nasty file permission issues.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11px;"&gt;If your&amp;nbsp;license file only works when you run as CW as administrator, this is because of inherited permissions. I would delete the&amp;nbsp;whole "CodeWarrior for Microcontrollers V6.3"&amp;nbsp;folder reinstall and use the copy paste&amp;nbsp;method&amp;nbsp;above.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;List of updates for CW 6.3&amp;nbsp;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fnxp.flexnetoperations.com%2Fcontrol%2Ffrse%2Fdownload%3Fagree%3DAccept%26element%3D5901331" rel="nofollow noopener noreferrer" target="_blank"&gt;backup link to downloads&lt;/A&gt;:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;Always install these two:&amp;nbsp;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescaleesd.flexnetoperations.com/337170/537/9681537/CW%20MCU%20v6.3%20PE%20V3.09%20-%20Patch.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 PE V3.09 - Patch.exe&lt;/A&gt;&amp;nbsp;&lt;SPAN style="font-size: 12px;"&gt;(It will warn about&amp;nbsp;derivative updates not being installed; this is ok)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescaleesd.flexnetoperations.com/337170/881/8311881/CW%20MCU%20v6.3.1%20-%20Patch.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3.1 - Patch.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Install these if you want this derivative updates:&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescaleesd.flexnetoperations.com/337170/781/8311781/CW%20MCU%20v6.3%20AG128%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 AG128 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/781/8311781/CW%20MCU%20v6.3%20AG128%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 AW16A Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/801/8311801/CW%20MCU%20v6.3%20AW60%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 AW60 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/811/8311811/CW%20MCU%20v6.3%20ColdFire%20V1%20EM256-EM128%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 ColdFire V1 EM256-EM128 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/821/8311821/CW%20MCU%20v6.3%20HCS08%20QE32%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 HCS08 QE32 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/831/8311831/CW%20MCU%20v6.3%20LH64-LL64%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 LH64-LL64 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/841/8311841/CW%20MCU%20v6.3%20MM128JE128%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 MM128JE128 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/851/8311851/CW%20MCU%20v6.3%20MM256-JE256%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 MM256-JE256 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/861/8311861/CW%20MCU%20v6.3%20S08%20AC128%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 S08 AC128 Service Pack.exe&lt;/A&gt;
&lt;A href="https://freescaleesd.flexnetoperations.com/337170/871/8311871/CW%20MCU%20v6.3%20S08%20SF4%20Service%20Pack.exe" rel="nofollow noopener noreferrer" target="_blank"&gt;CW MCU v6.3 S08 SF4 Service Pack.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: line-through;"&gt;CW08_V6_3_PE_V3_08_SP.exe&lt;/SPAN&gt; (Obsolete - Do not install/download)
&lt;SPAN style="text-decoration: line-through;"&gt;CW MCU v6.3 - Flash Patch.exe&lt;/SPAN&gt; (Obsolete - Do not install/download - Instead see P&amp;amp;E instructions below)
&lt;SPAN style="text-decoration: line-through;"&gt;CW MCU v6.3 PE V3.08 - Patch.exe&lt;/SPAN&gt; (Obsolete - Do not install/download)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt; line-height: 1.5em;"&gt;&lt;EM&gt;&lt;STRONG&gt;P&amp;amp;E Micro BDM steps:&lt;/STRONG&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;SPAN style="line-height: 1.5em;"&gt;
&lt;/SPAN&gt;&lt;SPAN style="line-height: 1.5em; font-size: 8pt;"&gt;Cyclone Pro, Cyclone Universal, USB BDM Multilink*, USB Multilink Universal, USB Multilink Universal FX.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt;"&gt;*Note: Rev. A of the USB-ML-12 is not supported in Windows 7/10 – Rev. C &lt;STRONG&gt;is supported&lt;/STRONG&gt; but is discontinued product&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030; font-family: arial, helvetica, sans-serif;"&gt;1. Download and install the &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.pemicro.com%2Fdownloads%2Fdownload_file.cfm%3Fdownload_id%3D53" rel="nofollow noopener noreferrer" target="_blank"&gt;latest drivers&lt;/A&gt; &lt;SPAN style="color: #303030;"&gt;(free login required)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&lt;SPAN style="color: #303030;"&gt;2. According to this&lt;/SPAN&gt; &lt;SPAN style="color: #303030;"&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.pemicro.com%2Ffaqs%2Ffaq_view.cfm%3Fid%3D211" rel="nofollow noopener noreferrer" target="_blank"&gt;FAQ&lt;/A&gt;,&lt;/SPAN&gt; download this zip &lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.pemicro.com%2Fdownloads%2Fdownload_file.cfm%3Fdownload_id%3D415" rel="nofollow noopener noreferrer" target="_blank"&gt;Patch for CFV1/S08/RS08/MON08 3rd Party Software&lt;/A&gt;&lt;SPAN style="color: #303030;"&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #303030; font-family: 'Helvetica Neue';"&gt;extract it and follow the rest of steps in the README text file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030; font-size: 13px; font-family: 'Helvetica Neue';"&gt;(Basically you need to merge the files from inside the "Patch" folder in the zip into "&lt;/SPAN&gt;&lt;SPAN style="color: #303030; font-family: arial, helvetica, sans-serif; font-size: 13px;"&gt;&lt;SPAN style="color: #303030; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;C:\Program Files (x86)\Freescale\CodeWarrior for Microcontrollers V6.3\prog\P&amp;amp;E".&lt;/SPAN&gt;&lt;SPAN style="color: #303030; font-family: 'Helvetica Neue';"&gt;&lt;STRONG&gt;If you do it correctly, it should prompt you about overwriting a few files&lt;/STRONG&gt;, do it.)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030; font-size: 12pt; font-family: arial, helvetica, sans-serif;"&gt;3. Run CW&amp;nbsp;as administrator (using right click menu) including building and debugging/programming once.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="font-size: 14pt;"&gt;&lt;EM&gt;&lt;SPAN style="line-height: 1.5em;"&gt;&lt;STRONG&gt;USBD&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="line-height: 1.5em;"&gt;&lt;STRONG&gt;M&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="color: #303030;"&gt;I personally used this for a HCS08SH microcontroller with a Wytec USBDM with the latest and it works great. &lt;SPAN style="line-height: 1.5em; font-size: 10pt;"&gt;If you don't consider it because they are a fifth the price of other programmers and are open source hardware and software. You can also buy them on eBay for about $15 dollars US (white-ish box with three leds, black letters on the outside&amp;nbsp;that says "USBDM" are the ones I have tested), but throw away the CD that&amp;nbsp;comes with them. Follow the YouTube instructions below. &amp;nbsp;The project is currently hosted on &lt;SPAN style="color: #2873ee;"&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fusbdm.sourceforge.net%2F" rel="nofollow noopener noreferrer" target="_blank"&gt;https://usbdm.sourceforge.net/&lt;/A&gt;&lt;/SPAN&gt;.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="color: #303030; font-size: 10pt; line-height: 1.5em;"&gt;&lt;EM&gt;Watch a video on the process:&lt;/EM&gt;&lt;/SPAN&gt; &lt;SPAN style="color: #303030; font-size: 10pt; line-height: 1.5em;"&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3D-ZylqEk7ZQE" rel="nofollow noopener noreferrer" target="_blank"&gt;USBDM CodeWarrior 6.3 5.1 5.2 Windows 10 x64 Install and Update Firmware - YouTube&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="color: #303030; font-size: 15px; line-height: 1.5em;"&gt;&lt;STRONG&gt;Steps:&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="color: #303030;"&gt;&lt;SPAN style="line-height: 1.5em; font-size: 10pt;"&gt;1. (Uninstall and re)Install &lt;STRONG&gt;latest&lt;/STRONG&gt; USBDM software &lt;STRONG&gt;AFTER&lt;/STRONG&gt; installing&lt;/SPAN&gt;&amp;nbsp;Codewarrior 6.3&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="color: #303030;"&gt;2. (Uninstall the re)Install&amp;nbsp;&lt;STRONG&gt;latest signed driver&lt;/STRONG&gt; before plugging it in USB.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="font-size: 10pt; color: #303030;"&gt;3. Use the &lt;STRONG&gt;firmware updater&lt;/STRONG&gt; from the start menu to make sure the firmware is up to date&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="font-size: 10pt; color: #303030;"&gt;(TIP:&amp;nbsp; Try the verify button before trying to update to make sure all "update mode" drivers are installed; it may crash/hang the 1st verify, fail on the 2nd verify, but that is OK, thirdly do the update)&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="font-size: 13.3333330154419px;"&gt;&lt;SPAN style="font-size: 10pt; color: #303030;"&gt;4. &lt;SPAN style="line-height: 1.5em; font-size: 10pt;"&gt;You'll need to select "HCS08 Open Source BDM" in the new project wizard in CW 6.3&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8pt; color: #303030;"&gt;Note that the automatic calculation of the clock trim doesn't work directly from CW6.3 debug you need to use the standalone USBDM HCS08 external programmer from the start menu (see posts below from USBDM dev PGO).&lt;/SPAN&gt;&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN style="color: #252525; font-family: sans-serif;"&gt;&lt;STRONG&gt;&lt;STRONG&gt;Dead Collector:&lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/SPAN&gt; Bring out yer dead!&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;&lt;STRONG&gt;Freescale&lt;/STRONG&gt;&lt;/SPAN&gt;: Here's one.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #252525; font-family: sans-serif;"&gt;&lt;STRONG&gt;CodeWarrior Classic&lt;/STRONG&gt;&lt;/SPAN&gt;: "I'm not dead".&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #252525; font-family: sans-serif;"&gt;&lt;STRONG&gt;Dead Collector:&lt;/STRONG&gt;&lt;/SPAN&gt; 'Ere, he says he's not dead.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #252525; font-family: sans-serif;"&gt;&lt;STRONG&gt;&lt;STRONG&gt;Freescale&lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;: Well, he will be soon, he's very ill.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #252525; font-family: sans-serif;"&gt;&lt;STRONG&gt;CodeWarrior Classic&lt;/STRONG&gt;&lt;/SPAN&gt;: I'm getting better. I work with Windows 10 x64 now.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #303030;"&gt;&lt;STRONG&gt;NXP&lt;/STRONG&gt;&lt;/SPAN&gt;: What about this one?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #252525; font-family: sans-serif;"&gt;&lt;STRONG&gt;&lt;STRONG&gt;Freescale&lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;: Who me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2012 02:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220513#M6359</guid>
      <dc:creator>RodneyMcGee</dc:creator>
      <dc:date>2012-12-29T02:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220514#M6360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The install went great but I'm having problems with the PE Multilink interface. I'm trying to connect to a DEMO9S08QG8 board with integrated BDM and it will not connect. I downloaded the latest drivers for WIndow 7 64 bit from PE and the OS indicates the driver is associated with the USB port. I tried v10.3 and it will connect but other issues make it unusable. I guess I'll have to drag out the old XP laptop and hope it does not die. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Jan 2013 20:16:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220514#M6360</guid>
      <dc:creator>deaninkc</dc:creator>
      <dc:date>2013-01-01T20:16:13Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220515#M6361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can connect to the &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;DEMO9S08QG8&lt;/SPAN&gt; board with 10.3 and I was able to compile a run a program on it. With 10.3 they got rid of the Classic project import wizard that was in 10.2 however. I put in an SR and the confirmed that they deleted the wizard in 10.3 and said I needed to create a new project and import the files from the old project one at a time. They seem to be bound and determined to make things difficult. I've already wasted way too much time on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2013 15:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220515#M6361</guid>
      <dc:creator>deaninkc</dc:creator>
      <dc:date>2013-01-03T15:40:15Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220516#M6362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rodney,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am too a convinced user of CW6.3. I never tried to switch to Eclipse partly because I am lazy but I am going to think it is either bulkier and perhaps more difficult than CW6. In any case it is my convinced opinion that the things which works well and which you know well must not be changed if there are not &lt;SPAN style="color: #000000; font-size: 10pt;"&gt;very&lt;/SPAN&gt; good reasons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Well, after this prologue, I bought a notebook with Win7 64 bit some 2 years ago and I found it was very difficult or impossible to run CW6.3 on it. I tried some tricks like that already discussed here at the time, I was able to install drivers (PE BDM lights on) but anyway there is no communication. I resigned and installed Virtual XP: fortunately my Windows version supported that. Now I run well CW6.3 with only minor annoyances as to manually (re-)assign USB ports and limited connectivity to LAN.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;I have an original PE Multilink USB programmer and many demo boards with embedded multilink: they all works well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Nevertheless PE multilink is not exactly cheap for an hobbyist and embedded multilink are (now) software limited to a single flavor of the S08 garden, that one of the demo board. Once it was not so. So I bought a pair of the incredibly cheap USBDM one year and half ago and after some initial problem I was able to install the new drivers which finally worked on my environment (several PCs with Win XP). USBDM works now pretty well but it is not able to make initial oscillator trimming on the uCU: I read this was a known bug which is not present on Eclipse 10.x.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Do you know if this problems was resolved? Many programs and in particular communication with RS232 does not work well, or not at all, if the oscillator is untrimmed. What can you say on this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;Salvatore&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2013 23:39:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220516#M6362</guid>
      <dc:creator>Encoder1</dc:creator>
      <dc:date>2013-01-03T23:39:06Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220517#M6363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the the lastest documentation in &lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JMxx/html/page_history.html" style="font-size: 10pt; line-height: 1.5em;" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JMxx/html/page_history.html"&gt;USBDM 4.10.4: History &amp;amp; Issue&lt;/A&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;Trim programming is not supported on older Codewarrior version. It is only available in the Eclipse version and stand-alone programmers. Trimming is done by Codewarrior not USBDM in the earlier versions. It is simply not implemented by CodeWarrior (despite there being a nice dialogue box!). I can't do anything about this. It is NOT a bug in USBDM&lt;/P&gt;






&lt;/BLOCKQUOTE&gt;&lt;P&gt;He is referring to the CW interface the that USBDM hooks into that was originally for the OSBDM. The P&amp;amp;E Micro has its own interface and has those kind of settings actually work when you can get your Multilink working anyway.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll tell you what I do. I use the standalone "HCS08 Programmer" to trim and program. You have type in the proper trim address for your chip and the trim value within the allowable range from the datasheet. I still use the CodeWarrior Real-Time Debugger and Programmer to do debugging as long as you left the device unsecured. Debugging from CW a board that is already programmed and running also works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my development workflow, I generally hit the "Make" button in CW 6.3. Then Alt+Tab over the USBDM Standalone programmer and hit "Load and Go" with the projects S19 file from the project directory. Done! &lt;SPAN style="font-size: 10pt;"&gt;Check out this picture: &lt;/SPAN&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_FlashProgrammers/html/TargetTab(CFV1).png" style="font-size: 10pt;" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_FlashProgrammers/html/TargetTab(CFV1).png"&gt;RS08, HCS08, CFV1, DSC, ARM Dialog for USBDM Standalone Programmer. &lt;/A&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I also use the command line version of the USBDM standalone programmer to automate programming on our assembly factory floor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also if you have a USBDM that is 1.5 years old ... make sure you &lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JMxx/html/Bootloader.png" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JMxx/html/Bootloader.png"&gt;Update the BDM Firmware&lt;/A&gt; using the USBDM Flash Programmer. &lt;SPAN style="line-height: 1.5em; font-size: 10pt;"&gt;If you have general &lt;/SPAN&gt;&lt;SPAN style="line-height: 1.5em; font-size: 10pt;"&gt;problems with your USBDM check out the &lt;A href="https://community.nxp.com/space/2024"&gt;OSBDM and TBDML Forum.&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 01:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220517#M6363</guid>
      <dc:creator>RodneyMcGee</dc:creator>
      <dc:date>2013-01-04T01:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220518#M6364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rodney,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an alternative to the above juggling between Codewarrior V6.3 &amp;amp; the USBDM programmer that I find useful for debugging with a selected chip i.e. you are using the same chip each debugging session.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Use the stand-alone USBDM programmer to program the chip with trim.&amp;nbsp; The programmer will report the trim value(s) it calculates.&amp;nbsp; &lt;/LI&gt;&lt;LI&gt;Modify the project source code to incorporate creating the trim memory locations for programming and initialise them with the values determined in 1. above.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This should produce a workable system for debugging that is a bit more convenient.&lt;/P&gt;&lt;P&gt;The USBDM programmer manual has some examples of clock trimming that use this approach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 03:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220518#M6364</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-01-04T03:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220519#M6365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot Rodney and Pgo for your suggestions and clarification. It is clear the problem lies on CW6.3 and on discontinued support on this program.&lt;/P&gt;&lt;P&gt;Unfortunately this cannot help peoples who are still bounded to CW6.3 and has not a Multilink programmer or people who buy the new demo boards which now incorporate USBDM. Perhaps this case is not so hurting for the new processors which are supported only by Eclipse: I will discover as soon as I will try to turn on my recently acquired S08PT60 tower system. I fear I will be obliged to finally convert to Eclipse!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bye and tanks,&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 09:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220519#M6365</guid>
      <dc:creator>Encoder1</dc:creator>
      <dc:date>2013-01-04T09:48:31Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220520#M6366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;very nice, good job Rodney.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;xiaolaba&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 14:33:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220520#M6366</guid>
      <dc:creator>xiaolaba</dc:creator>
      <dc:date>2013-01-04T14:33:03Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220521#M6367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Salvatore,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just to clarify/correct a minor point in your summary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;USBDM is an open source independent BDM and is not related to the OSBDM-JM60 used on the Freescale boards - such as the S08PT60 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a version of the USBDM software that works with the tower HCS08 boards.&amp;nbsp; To use this it is necessary to re-program the JM60 chip on the board.&amp;nbsp; It is also possible to use an external BDM (such as USBDM) with the tower boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2013 05:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220521#M6367</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-01-07T05:11:34Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220522#M6368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks again PGO for you precisation.&lt;/P&gt;&lt;P&gt;I confess I do a little confusion about USBDM and OSBDM....&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;P&gt;:smileysilly:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2013 18:01:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220522#M6368</guid>
      <dc:creator>Encoder1</dc:creator>
      <dc:date>2013-01-07T18:01:31Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220523#M6369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;howdy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anyone successful installing on Win8 ?&lt;/P&gt;&lt;P&gt;I can get the installer to run, but shortly after "copying new files", the installer terminates&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Oskar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Jan 2013 02:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220523#M6369</guid>
      <dc:creator>oskaratk</dc:creator>
      <dc:date>2013-01-19T02:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220524#M6370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Microsoft did it again. Broke a great deal of technical software with the transition to Windows 7 and gave us a really bad "Windows XP Mode" to make our programs run, which works 10% of the time. Henceforth I am transitioning to Linux completely as far as possible. In the meantime however I sit with these same problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Eclipse based Codewarrior is in a word- TERRIBLE. I cannot be productive with such slow software. Texas Instruments' use the same Eclipse IDE and they are ready to debug in 0.7 sec. I have been complaining to Freescale via my local FAE since early 2010, its 2013 and there is still no solution. I have even suggested to Freescale to talk to TI and find out how they got Eclipse to be that fast. I hate Eclipse and always will, I tolerate it for the sake of getting the job done!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not all of us can afford to throw a Core i7 processor and 16Gbytes of RAM at Codewarrior 10.3 to make it work somewhat acceptably quick. And now, with Windows 7 my hands have been cut off because the last decent version of Codewarrior, version 6.3 doesn't install.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the trick above, doesn't work on the latest updated copy of Windows 7 Pro. I get the same error as Oskar.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really wish that Freescale, seeing that V6.3 is basically retired, would release its source code under GNU license, then people like me can fix the problems and recompile it for Windows 7. The days of proprietary, licensed IDEs for micros is coming to an end, especially since a friend and I were able to create a toolchain using GCC for another micro, in Linux and it all works, for free, no $495 license required. Unfortunately GCC does not support the HCS08 at this time to my knowledge and to update it for that, spare time is a luxury.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rather focus on silicon sales, instead of trying to make money on software.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 08:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220524#M6370</guid>
      <dc:creator>JTech</dc:creator>
      <dc:date>2013-01-25T08:12:43Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220525#M6371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found that there is a permissions problem. When I fixed that, I was able to install. However there were other problems which I fixed but this exercise took most of my working day today. I posted the full solution elsewhere on these forums, the URL is &lt;A href="https://community.nxp.com/thread/57404"&gt;Codewarrior 6.2 on a Widows 7 system&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Right at the bottom of the thread!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 14:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220525#M6371</guid>
      <dc:creator>JTech</dc:creator>
      <dc:date>2013-01-25T14:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220526#M6372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I added a slightly modified version of info from the 6.2 thread up at the top. &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;This should help people with P&amp;amp;E Micro Multilink BDM. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;It got my dusty old P&amp;amp;E working right away.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Jan 2013 18:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220526#M6372</guid>
      <dc:creator>RodneyMcGee</dc:creator>
      <dc:date>2013-01-26T18:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220527#M6373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this. Running fast in Win7-64 bit with P&amp;amp;E USB Multilink interface.&amp;nbsp; This really was helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 18:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220527#M6373</guid>
      <dc:creator>embeddedprogram</dc:creator>
      <dc:date>2013-06-20T18:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220528#M6374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all.&amp;nbsp;&amp;nbsp; The instructions to install CW 6.3 on Win7-64 work great,&amp;nbsp; what a relief!&amp;nbsp;&amp;nbsp; Working to get the debugger connected.&amp;nbsp; I have both the old USB Multilink and USBDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the Multilink,&amp;nbsp; I followed all the instructions,&amp;nbsp; and everything loaded fine,&amp;nbsp; but when trying to debug I get&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="PE_error.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49527i408F621AB48AE70A/image-size/large?v=v2&amp;amp;px=999" role="button" title="PE_error.jpg" alt="PE_error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try installing the USBDM software I get:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="USBDM_PolicyError.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49528iBED3B088CCC0A0C2/image-size/large?v=v2&amp;amp;px=999" role="button" title="USBDM_PolicyError.jpg" alt="USBDM_PolicyError.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm really close on this,&amp;nbsp; I have followed all the hints and stuff on the web about policies,&amp;nbsp; unblocked the msi in rightClick-&amp;gt;properties,&amp;nbsp; fiddled with the registry,&amp;nbsp; sorta lost here..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit:&amp;nbsp; disabling user account control (UAC),&amp;nbsp; (control panel -&amp;gt; user accounts) let me install the software.&amp;nbsp; The driver install was giving windows installer errors,&amp;nbsp; but I think that was because Windows was trying to install updates or something.&amp;nbsp; A few reboots and updates and then the drivers installed.&amp;nbsp; Updated the USBDM firmware and it seems to be working.&amp;nbsp;&amp;nbsp; I haven't tried to fix the PE stuff,&amp;nbsp; if USBDM will get the job done,&amp;nbsp; then I am happy...&amp;nbsp; !&amp;nbsp; I hope this is helpful.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 16:34:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220528#M6374</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2015-01-23T16:34:31Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220529#M6375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0px 0px 8pt;"&gt;&lt;SPAN style="color: #000000; font-family: Calibri; font-size: 12pt;"&gt;CW 6.3, WIN7 Prof 64B, PEMicro USB Multilink Rev. C&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0px 0px 8pt;"&gt;&lt;SPAN style="font-family: Calibri;"&gt;&lt;SPAN style="color: #000000; font-size: 12pt;"&gt;Your work-around as described in your July 3, 2014 post worked perfectly for me in all respects for about 3 weeks. &lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt;"&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt;"&gt;Then, suddenly I could no longer connect with the target board (m68demo908gb60) to which I had connected successfully numerous times during the 3 week period.&lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt;"&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt;"&gt;Both the blue and yellow leds are illuminated, but every time I try to connect prior to debugging, the command window in CW indicates “Notice-Cyclone Pro/Max USB driver did not initialize (20000021) – Library=WDAPI900.DLL.”&lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt;"&gt;I have removed and reloaded CW/the work around thinking that maybe the program or the driver may have been corrupted but the problem remains. I have also attempted to connect to another identical demo board of known good health without success. I am wondering if the work-around is unstable in some way or if the Multilink has failed but I don’t know enough about the internals of CW or the Multilink to determine if either is the case. I no longer have an XP machine so I cannot test the Multilink on a known working copy of CW. Do you or anyone have any ideas on this?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0px 0px 8pt;"&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;Any help would be greatly appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0px 0px 8pt;"&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;Tnx!&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0px 0px 8pt;"&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;Pete&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Feb 2015 18:04:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220529#M6375</guid>
      <dc:creator>nhpete</dc:creator>
      <dc:date>2015-02-01T18:04:29Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220530#M6376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can install XP emulation via Virtual PC (Windows) or VirtualBox.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After to have installed the MCU V6.3, you can link an USB connection to the XP emulation.&lt;/P&gt;&lt;P&gt;Sometimes you need to un-plug / re-plug the multilink to be correctly recognized by XP emulation.&lt;/P&gt;&lt;P&gt;At the end the tool will work as real XP OS.&lt;/P&gt;&lt;P&gt;By this way you could check the interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Feb 2015 12:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220530#M6376</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-02-02T12:55:50Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220531#M6377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Pascale:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tnx for the suggestion.&amp;nbsp; I am unfamiliar with setting up the XP emulation and am concerned that the interface might not work on that basis alone.&amp;nbsp; Instead, I decided on another first approach.&amp;nbsp; I have Downloaded and installed the Eclipse v10.6 which is supposed to support the Multilink interface as well.&amp;nbsp; If it works on v10.6, I'll assume there is some instability on the v6.3 workaround and get up to speed on Eclipse.&amp;nbsp; If it doesn't, I'll assume the Multilink has failed, get another one, and stick with v6.3 work around.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Feb 2015 01:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220531#M6377</guid>
      <dc:creator>nhpete</dc:creator>
      <dc:date>2015-02-06T01:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: Install CodeWarrior v6.3 directly under Windows 7 x64</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220532#M6378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes good option too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Feb 2015 07:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-Directly-Install-CodeWarrior-6-3-Classic-in-Windows-10-or/m-p/220532#M6378</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2015-02-06T07:38:59Z</dc:date>
    </item>
  </channel>
</rss>