<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: Installing Code Warrior 8.7 on Windows 7 (64-bit)</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219755#M6339</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure if Natep's&amp;nbsp; solution for CW for S12 V5.0 is applicable for CW for PowerPC:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A __default_attr="57404" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/57404" jivemacro="thread" title="https://community.freescale.com/thread/57404"&gt;https://community.freescale.com/thread/57404&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the symptoms were the same -&amp;nbsp;"was interrupted" message. Hope it will work also for CW for PowerPC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You need&amp;nbsp;to find working 32bits Win XP machine and install CW there. Then:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Copy whole CW folder from&amp;nbsp;Win32 machine to Win7 machine&amp;nbsp;(Program Files\CodeWarrior xxxx)&lt;/P&gt;&lt;P&gt;3) Now, this step is the MOST&amp;nbsp;IMPORTANT:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Look at the file "Mwregsvr.exe" in the c:\Program Files(x86)\Freescale\CodeWarrior for Microcontrollers V6.1\bin and click the right button on this file, then click properties.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Now, in the compatibility tab,set the compatibility to WindowsXp (sp2) and set the checkbox&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; to run in administrator mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Now, click apply button&amp;nbsp;then click OK button.&lt;/P&gt;&lt;P&gt;4) In the same folder, run once the file regservers.bat&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; When windows ask for the permisions, just click yes everytime.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;5) &amp;nbsp;You may want to create a desktop icon at this point.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Aug 2010 22:52:29 GMT</pubDate>
    <dc:creator>kef</dc:creator>
    <dc:date>2010-08-27T22:52:29Z</dc:date>
    <item>
      <title>Installing Code Warrior 8.7 on Windows 7 (64-bit)</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219754#M6338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I realise this isn't officially supported, but my laptop was recently upgraded to a machine running Windows 7 64-bit. I am trying to install CodeWarrior for PowerPC 5XX v8.7 (using "run as administrator") but the installer eventually errors out saying:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"The wizard was interrupted before CodeWarrior Development Studio, MPC5xx Edition, v8.7 could be completely installed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your system has not been modified. To complete installation at another time, please run setup again"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Click Finish to exit the wizard".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anybody come across this or tried to install Code Warrior for MPC5xx v8.7 on Windows 7? Is there a workaround?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Arnaud&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Aug 2010 22:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219754#M6338</guid>
      <dc:creator>am304</dc:creator>
      <dc:date>2010-08-27T22:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Code Warrior 8.7 on Windows 7 (64-bit)</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219755#M6339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure if Natep's&amp;nbsp; solution for CW for S12 V5.0 is applicable for CW for PowerPC:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A __default_attr="57404" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/57404" jivemacro="thread" title="https://community.freescale.com/thread/57404"&gt;https://community.freescale.com/thread/57404&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the symptoms were the same -&amp;nbsp;"was interrupted" message. Hope it will work also for CW for PowerPC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You need&amp;nbsp;to find working 32bits Win XP machine and install CW there. Then:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Copy whole CW folder from&amp;nbsp;Win32 machine to Win7 machine&amp;nbsp;(Program Files\CodeWarrior xxxx)&lt;/P&gt;&lt;P&gt;3) Now, this step is the MOST&amp;nbsp;IMPORTANT:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Look at the file "Mwregsvr.exe" in the c:\Program Files(x86)\Freescale\CodeWarrior for Microcontrollers V6.1\bin and click the right button on this file, then click properties.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Now, in the compatibility tab,set the compatibility to WindowsXp (sp2) and set the checkbox&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; to run in administrator mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Now, click apply button&amp;nbsp;then click OK button.&lt;/P&gt;&lt;P&gt;4) In the same folder, run once the file regservers.bat&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; When windows ask for the permisions, just click yes everytime.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;5) &amp;nbsp;You may want to create a desktop icon at this point.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Aug 2010 22:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219755#M6339</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-08-27T22:52:29Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Code Warrior 8.7 on Windows 7 (64-bit)</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219756#M6340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, that worked a treat!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Arnaud&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Sep 2010 20:34:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219756#M6340</guid>
      <dc:creator>am304</dc:creator>
      <dc:date>2010-09-02T20:34:49Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Code Warrior 8.7 on Windows 7 (64-bit)</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219757#M6341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone know if using SP3 is better or worse than SP2 for this application?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Sep 2010 06:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Installing-Code-Warrior-8-7-on-Windows-7-64-bit/m-p/219757#M6341</guid>
      <dc:creator>sbsoccermike</dc:creator>
      <dc:date>2010-09-15T06:13:04Z</dc:date>
    </item>
  </channel>
</rss>