<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックCW 6.3 on WinXP 32 bit issues !!</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-6-3-on-WinXP-32-bit-issues/m-p/217382#M6232</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I bought a XL_Star sample kit from element14. Installed the supplied copy of CW as per instructions, installed without any errors. Launching the program gives me " The exception unknown software (0xc000000d) occurred in the application at loacation 0x00edf841"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help would be apprecaiated&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2011 05:26:37 GMT</pubDate>
    <dc:creator>Garry_Aus</dc:creator>
    <dc:date>2011-06-24T05:26:37Z</dc:date>
    <item>
      <title>CW 6.3 on WinXP 32 bit issues !!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-6-3-on-WinXP-32-bit-issues/m-p/217382#M6232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I bought a XL_Star sample kit from element14. Installed the supplied copy of CW as per instructions, installed without any errors. Launching the program gives me " The exception unknown software (0xc000000d) occurred in the application at loacation 0x00edf841"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help would be apprecaiated&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2011 05:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-6-3-on-WinXP-32-bit-issues/m-p/217382#M6232</guid>
      <dc:creator>Garry_Aus</dc:creator>
      <dc:date>2011-06-24T05:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: CW 6.3 on WinXP 32 bit issues !!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-6-3-on-WinXP-32-bit-issues/m-p/217383#M6233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have administrator rights on the PC you are installing on to? The CodeWarrior install requires that you do.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just in case the CD you have has been mis-copied I suggest downloading and installing Special Edition CodeWarrior for Microcontrollers V6.3 (Classic Windows Hosted) from the Freescale link below -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-SPECIAL&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-SPECIAL&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will also need to apply the &lt;A href="http://cache.freescale.com/lgfiles/updates/CWHC08/CW08_V6_3_HCS08_MM128_JE128_SP.exe?WT_TYPE=Updates%20and%20Patches&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads" rel="nofollow" target="_blank"&gt;CW MCU v6.3 MM128/JE128 Service Pack&lt;/A&gt; MM128 patch available at -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and finally the Processor Expert update -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=CW08_V6_3_PE_V3_09_SP&amp;amp;nodeId=015210272600618680&amp;amp;location=overview&amp;amp;WT_TYPE=Updates%20and%20Patches&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=exe&amp;amp;WT_ASSET=Downloads&amp;amp;Parent_nodeId=1260805682870742228680&amp;amp;Parent_pageType=overview" rel="nofollow" target="_blank"&gt;CodeWarrior for MCU V6.3 Processor Expert V3.09 Update&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2011 13:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-6-3-on-WinXP-32-bit-issues/m-p/217383#M6233</guid>
      <dc:creator>PBH</dc:creator>
      <dc:date>2011-07-06T13:18:19Z</dc:date>
    </item>
  </channel>
</rss>