<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: CW10.1, Project &amp;gt; Change Device/Connection issue</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-1-Project-gt-Change-Device-Connection-issue/m-p/215111#M6145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your quick reply, I just worked it out by finding another help file which is correct, (which also is a match to what you have posted).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The help file headed "&lt;SPAN&gt;P&amp;amp;E USB BDM &lt;SPAN&gt;Multilink&lt;/SPAN&gt; or USB &lt;SPAN&gt;Multilink&lt;/SPAN&gt; Universal&lt;/SPAN&gt;﻿" is not correct. The help file headed "&lt;SPAN&gt;P&amp;amp;E USB BDM &lt;SPAN&gt;Multilink&lt;/SPAN&gt; or USB &lt;SPAN&gt;Multilink&lt;/SPAN&gt; Universal&lt;/SPAN&gt;﻿" is correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2011 07:55:48 GMT</pubDate>
    <dc:creator>CarlFST60L</dc:creator>
    <dc:date>2011-06-15T07:55:48Z</dc:date>
    <item>
      <title>CW10.1, Project &gt; Change Device/Connection issue</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-1-Project-gt-Change-Device-Connection-issue/m-p/215109#M6143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am a long time pre CW10 user and finally have been forced to learn CW10 (Eclipse).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This should be a simple one I hope, I have downloaded and installed:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Special Edition: CodeWarrior for Microcontrollers (Eclipse, Windows hosted)&lt;BR /&gt;Code Size Restriction: RS08/HCS08 - 32KB, ColdFire V1 - 64KB, ColdFire V2-V4/Kinetis - 128K, MPC56xx – 512K&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also downloaded and installed FSLMQX3.7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have done a general import of the up the 'hello world' example in MQX, built the project and there are no errors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I now need to burn the flash in my hardware, but, I use the Multilink USB programmer (for this test), not the TWR OSBDM programmer. After reading, and searching the help, I found the section that describes changing the connection to another flash programmer for the project (I found this by searching Multilink). It says go "Project &amp;gt; Change Device/Connection", when I do this I a message box saying:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"To use this wizard, please make sure a project is selected and has focus in the CodeWarrior Projects View".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ohhh, I just found one simple problem, you cannot have the "Codewarrior Projects" window on a different monitor to the rest of the project... So for some reason, it must be docked in the same monitor... Anyway, moving on...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next section for changing the connection doesnt match the help files at all, so I will continue anyway... It now requests to 'create a new project', I dont want to do that, but i will continue yet again, (the help files say just to select the Multilink), so am forced to click next on the create project screen, then I select the Coldfile V2 MCF52259, and next, then I seelct P&amp;amp;E Universal/USB Multilink, then I press finish, and nothing happens, I press finish again, nothing happens... I restart, nothing happens still...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I get my Mutlilink to work in CW10? Why dont the help files match what happens in CW10.1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2011 07:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-1-Project-gt-Change-Device-Connection-issue/m-p/215109#M6143</guid>
      <dc:creator>CarlFST60L</dc:creator>
      <dc:date>2011-06-15T07:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: CW10.1, Project &gt; Change Device/Connection issue</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-1-Project-gt-Change-Device-Connection-issue/m-p/215110#M6144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Carl,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As you only wish to change the connection (not the device) there is a simpler process:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Open&amp;nbsp; &lt;STRONG&gt;Run-&amp;gt;Debug Configurations...&lt;/STRONG&gt; from the menu (or use the menu on the debug icon)&lt;/LI&gt;&lt;LI&gt;Make sure the correct launch configuration is selected at left and the &lt;STRONG&gt;Main&lt;/STRONG&gt; tab is selected at right&lt;/LI&gt;&lt;LI&gt;Click the &lt;STRONG&gt;EDIT&lt;/STRONG&gt; button under &lt;STRONG&gt;Remote Systems&lt;/STRONG&gt; panel&lt;/LI&gt;&lt;LI&gt;Use the drop-down list to change the item at &lt;STRONG&gt;Connection Type:&lt;/STRONG&gt; to the BDM you are using (&lt;STRONG&gt;P&amp;amp;E&lt;/STRONG&gt; something or other I suspect)&lt;/LI&gt;&lt;LI&gt;Fill in the rest of the dialogue&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;You may need to repeat this for any other launch configurations associated with your project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can also change the "remote systems" (the connection) through the &lt;STRONG&gt;Remote Systems&lt;/STRONG&gt; list &lt;STRONG&gt;&lt;EM&gt;Windows-&amp;gt;Show view-&amp;gt;Remote Systems&lt;/EM&gt;&lt;/STRONG&gt;&amp;nbsp; or &lt;STRONG&gt;&lt;EM&gt;Windows-&amp;gt;Show view-&amp;gt;Other-&amp;gt;Remote Systems&lt;/EM&gt;&lt;/STRONG&gt;﻿ directly&lt;EM&gt;&lt;STRONG&gt;.&lt;BR /&gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2011 07:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-1-Project-gt-Change-Device-Connection-issue/m-p/215110#M6144</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-06-15T07:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: CW10.1, Project &gt; Change Device/Connection issue</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-1-Project-gt-Change-Device-Connection-issue/m-p/215111#M6145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your quick reply, I just worked it out by finding another help file which is correct, (which also is a match to what you have posted).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The help file headed "&lt;SPAN&gt;P&amp;amp;E USB BDM &lt;SPAN&gt;Multilink&lt;/SPAN&gt; or USB &lt;SPAN&gt;Multilink&lt;/SPAN&gt; Universal&lt;/SPAN&gt;﻿" is not correct. The help file headed "&lt;SPAN&gt;P&amp;amp;E USB BDM &lt;SPAN&gt;Multilink&lt;/SPAN&gt; or USB &lt;SPAN&gt;Multilink&lt;/SPAN&gt; Universal&lt;/SPAN&gt;﻿" is correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2011 07:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW10-1-Project-gt-Change-Device-Connection-issue/m-p/215111#M6145</guid>
      <dc:creator>CarlFST60L</dc:creator>
      <dc:date>2011-06-15T07:55:48Z</dc:date>
    </item>
  </channel>
</rss>