<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unable to debug MRAM Ext Debug on Tower 52259 in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unable-to-debug-MRAM-Ext-Debug-on-Tower-52259/m-p/213580#M6098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am CodeWarrior 7.2 with MQX 3.6 along with a Tower MCF52259 CPU and TWRMEM card that contains a 512K MRAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The jumpers on the MCF52259 board and TWRMEM are set to default.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the onboard Coldfire V2-V4 JM60 OSBDM debugger&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can build the Web_hvac_twrmc52259.mcp in codewarrior to int_flash_debug , erase and program the internal flash and debug the project without any problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I build the project to ext_mram_debug the code is uploaded to the mram and the debugger is entered at __main.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can single step lots of instructions but as soon as I enter RUN I get the message&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;GDI Protocol Plugin&lt;/P&gt;&lt;P&gt;"The debugger cannot read memory"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paul H&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jul 2010 16:29:50 GMT</pubDate>
    <dc:creator>accutime</dc:creator>
    <dc:date>2010-07-16T16:29:50Z</dc:date>
    <item>
      <title>Unable to debug MRAM Ext Debug on Tower 52259</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unable-to-debug-MRAM-Ext-Debug-on-Tower-52259/m-p/213580#M6098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am CodeWarrior 7.2 with MQX 3.6 along with a Tower MCF52259 CPU and TWRMEM card that contains a 512K MRAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The jumpers on the MCF52259 board and TWRMEM are set to default.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the onboard Coldfire V2-V4 JM60 OSBDM debugger&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can build the Web_hvac_twrmc52259.mcp in codewarrior to int_flash_debug , erase and program the internal flash and debug the project without any problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I build the project to ext_mram_debug the code is uploaded to the mram and the debugger is entered at __main.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can single step lots of instructions but as soon as I enter RUN I get the message&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;GDI Protocol Plugin&lt;/P&gt;&lt;P&gt;"The debugger cannot read memory"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paul H&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jul 2010 16:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unable-to-debug-MRAM-Ext-Debug-on-Tower-52259/m-p/213580#M6098</guid>
      <dc:creator>accutime</dc:creator>
      <dc:date>2010-07-16T16:29:50Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to debug MRAM Ext Debug on Tower 52259</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unable-to-debug-MRAM-Ext-Debug-on-Tower-52259/m-p/213581#M6099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same problem. Can anyone help me wiht this problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Sep 2010 16:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unable-to-debug-MRAM-Ext-Debug-on-Tower-52259/m-p/213581#M6099</guid>
      <dc:creator>Awera</dc:creator>
      <dc:date>2010-09-10T16:43:21Z</dc:date>
    </item>
  </channel>
</rss>