<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: codewarrior 8.8.3  Unable to call the command line tool in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/codewarrior-8-8-3-Unable-to-call-the-command-line-tool/m-p/208213#M5811</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW can be used to debug u-boot, but cannot be used to build u-boot.&amp;nbsp;&amp;nbsp;Building u-boot&amp;nbsp;has to be done outside of CW and then the u-boot elf used to create a CW debugging project (file -&amp;gt; open).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To debug u-boot from CW running on windows you will need to copy the entire u-boot source directory to your windows machine.&amp;nbsp; When you import the u-boot elf file CW should ask you about the path to the file.&amp;nbsp; This happens because you have moved the elf file from the linux system and the paths associated with the build are not correct anymore.&amp;nbsp; You should browse to find the first file and then CW should be able to resolve the rest of the paths.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Aug 2009 00:13:20 GMT</pubDate>
    <dc:creator>fsl_linux_spt</dc:creator>
    <dc:date>2009-08-20T00:13:20Z</dc:date>
    <item>
      <title>codewarrior 8.8.3  Unable to call the command line tool</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/codewarrior-8-8-3-Unable-to-call-the-command-line-tool/m-p/208212#M5810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I`m using&amp;nbsp; codewarrior to debug uboot for mpc8379eRDB.&lt;/P&gt;&lt;P&gt;My CPU is mpc8379e&lt;/P&gt;&lt;P&gt;My OS is windowsXP&lt;/P&gt;&lt;P&gt;My codewarrior version is v8.8.3 with mpc837x patch.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I prepared uboot followed the document&amp;lt;Debugging the U-Boot Bootstrap Firmware&amp;gt; in cw help.&lt;/P&gt;&lt;P&gt;I opened uboot elf in cw and selected EPPC linux gnu linker to make the uboot source code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cw gave me this error:"unable to call the command line tool.check your path environment variable"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I googled this error and somebody said&amp;nbsp; the uboot source code path is too long.But my uboot source is just in C:\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anybody knew why this error happend?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2009 11:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/codewarrior-8-8-3-Unable-to-call-the-command-line-tool/m-p/208212#M5810</guid>
      <dc:creator>ironpie</dc:creator>
      <dc:date>2009-08-19T11:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: codewarrior 8.8.3  Unable to call the command line tool</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/codewarrior-8-8-3-Unable-to-call-the-command-line-tool/m-p/208213#M5811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW can be used to debug u-boot, but cannot be used to build u-boot.&amp;nbsp;&amp;nbsp;Building u-boot&amp;nbsp;has to be done outside of CW and then the u-boot elf used to create a CW debugging project (file -&amp;gt; open).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To debug u-boot from CW running on windows you will need to copy the entire u-boot source directory to your windows machine.&amp;nbsp; When you import the u-boot elf file CW should ask you about the path to the file.&amp;nbsp; This happens because you have moved the elf file from the linux system and the paths associated with the build are not correct anymore.&amp;nbsp; You should browse to find the first file and then CW should be able to resolve the rest of the paths.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2009 00:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/codewarrior-8-8-3-Unable-to-call-the-command-line-tool/m-p/208213#M5811</guid>
      <dc:creator>fsl_linux_spt</dc:creator>
      <dc:date>2009-08-20T00:13:20Z</dc:date>
    </item>
  </channel>
</rss>