<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックCodeWarrior Hardware Breakpoints</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-Hardware-Breakpoints/m-p/208206#M5808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;I am using CodeWarrior to debug a MC68332 CPU board.&amp;nbsp; My code is running in Flash ROM.&amp;nbsp; The datasheet for the MC68332 indicates that I should be able to set up to 4 hardware breakpoints, however, when I try to set one, I always get the following message from CodeWarrior:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;"Maximum number of hardware breakpoints (1) has been reached"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I do not see any&amp;nbsp; breakpoints set when I "View -&amp;gt;&amp;nbsp;Breakpoints"&amp;nbsp; from the codeWarrior.&amp;nbsp; I am using the P&amp;amp;E Micro BDM debugger to connect to my board.&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is there a certain configuration, or register setting that is unenabling hardware breakpoints??&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Dec 2008 07:58:40 GMT</pubDate>
    <dc:creator>davidcav</dc:creator>
    <dc:date>2008-12-09T07:58:40Z</dc:date>
    <item>
      <title>CodeWarrior Hardware Breakpoints</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-Hardware-Breakpoints/m-p/208206#M5808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;I am using CodeWarrior to debug a MC68332 CPU board.&amp;nbsp; My code is running in Flash ROM.&amp;nbsp; The datasheet for the MC68332 indicates that I should be able to set up to 4 hardware breakpoints, however, when I try to set one, I always get the following message from CodeWarrior:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;"Maximum number of hardware breakpoints (1) has been reached"&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I do not see any&amp;nbsp; breakpoints set when I "View -&amp;gt;&amp;nbsp;Breakpoints"&amp;nbsp; from the codeWarrior.&amp;nbsp; I am using the P&amp;amp;E Micro BDM debugger to connect to my board.&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is there a certain configuration, or register setting that is unenabling hardware breakpoints??&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2008 07:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-Hardware-Breakpoints/m-p/208206#M5808</guid>
      <dc:creator>davidcav</dc:creator>
      <dc:date>2008-12-09T07:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior Hardware Breakpoints</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-Hardware-Breakpoints/m-p/208207#M5809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;As far as remember, there's no hardware breakpoint support (except BKPT pin) on MC68332.&lt;BR /&gt;IMHO, the best thing to do, is to move your code to ram and use software breakpoints.&lt;BR /&gt;But I could be wrong, because I never used CW with 68332, I used an old Hiware compiler with the older BMdebug debugger.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Emmanuel,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2008 17:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-Hardware-Breakpoints/m-p/208207#M5809</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2008-12-09T17:49:05Z</dc:date>
    </item>
  </channel>
</rss>