<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: CW v10.2 (Eclipse IDE): Debugging DSC56F8037 using USB TAP</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206212#M5740</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which OS are you using? I have a similar problem. I am using Windows 7 64 bit.&lt;/P&gt;&lt;P&gt;I experienced some improvements using the "Windows 7 64bit" - compatible ccs of AN4338, but I am still unable to complete flash programming when the executable is a non trivial one (size around 28k).&lt;/P&gt;&lt;P&gt;I can debug a very simple processor expret project though, but only in single step mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My dsc is a 56f8025. The USB TAP is the same you are using and it works perfectly with classic CodeWarrior, so I suspect it's not a hardware problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has some ideas/news&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Mar 2012 00:05:28 GMT</pubDate>
    <dc:creator>jive74</dc:creator>
    <dc:date>2012-03-07T00:05:28Z</dc:date>
    <item>
      <title>CW v10.2 (Eclipse IDE): Debugging DSC56F8037 using USB TAP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206211#M5739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've just installed&amp;nbsp;&lt;SPAN&gt;CodeWarrior for Microcontrollers v10.2 which&amp;nbsp;&lt;SPAN&gt;integrates the development tools for the DSC's. &amp;nbsp;I've created a simple project just to debug it using USB TAP.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN style="text-decoration: underline;"&gt;Problem is that I can't connect to board&lt;/SPAN&gt; and next error is displayed:&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"Launching MC56F8037_Project_1_MC56F8037_Internal_PFlash_SDM_Freescale USB TAP BDM has encountered a problem ... Failed to resume target process, CCSProtocoPlugin: Could not connect to the probe (or other debug link)"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;In debug configuration I select the following:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Application:&amp;nbsp;MC56F8037_Internal_PFlash_SDM/MC56F8037_Prueba_1.elf&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Build configuration:&amp;nbsp;&lt;SPAN&gt;MC56F8037_Internal_PFlash_SDM&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Connection:&amp;nbsp;MC56F8037_Prueba_1_MC56F8037_Internal_PFlash_SDM_Freescale USB TAP BDM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This last is the only connection USB TAP type I can select. But the USB TAP I'm using is: &lt;SPAN style="text-decoration: underline;"&gt;CodeWarrior USB TAP OnCE probe. Is this the matter?&lt;/SPAN&gt; In freescale web page it is said that hosted target interface is&amp;nbsp;CodeWarrior USB TAP, but it is not specified if BDM, OnCE, JTAG connector ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2012 01:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206211#M5739</guid>
      <dc:creator>Miskha</dc:creator>
      <dc:date>2012-02-15T01:39:49Z</dc:date>
    </item>
    <item>
      <title>Re: CW v10.2 (Eclipse IDE): Debugging DSC56F8037 using USB TAP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206212#M5740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which OS are you using? I have a similar problem. I am using Windows 7 64 bit.&lt;/P&gt;&lt;P&gt;I experienced some improvements using the "Windows 7 64bit" - compatible ccs of AN4338, but I am still unable to complete flash programming when the executable is a non trivial one (size around 28k).&lt;/P&gt;&lt;P&gt;I can debug a very simple processor expret project though, but only in single step mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My dsc is a 56f8025. The USB TAP is the same you are using and it works perfectly with classic CodeWarrior, so I suspect it's not a hardware problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has some ideas/news&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2012 00:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206212#M5740</guid>
      <dc:creator>jive74</dc:creator>
      <dc:date>2012-03-07T00:05:28Z</dc:date>
    </item>
    <item>
      <title>Re: CW v10.2 (Eclipse IDE): Debugging DSC56F8037 using USB TAP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206213#M5741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Use the CodeWarrior New Project wizard to create a default project that targets your board.&lt;/P&gt;&lt;P&gt;2) Build and run the project.&lt;/P&gt;&lt;P&gt;3) See if you get a dialog stating that a new driver/firmware update for the probe is in progress and let it complete.&lt;/P&gt;&lt;P&gt;4) Ideally, you'll be able to work with your project now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If that doesn't work, I'd suggest going to the P&amp;amp;E Micro website (pemicro.com) and download their 64-bit compatible drivers and install those.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2012 22:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206213#M5741</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2012-03-07T22:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: CW v10.2 (Eclipse IDE): Debugging DSC56F8037 using USB TAP</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206214#M5742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I solved my problem installing ccs drivers, which are in:&lt;/P&gt;&lt;P&gt;C:\Freescale\CW MCU v10.2\MCU\ccs\drivers\usb&lt;/P&gt;&lt;P&gt;I just followed readme file and it worked fine.&lt;/P&gt;&lt;P&gt;I did it in two different computers, one holding windows 7 64 bits, and other one with Windows XP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2012 23:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-v10-2-Eclipse-IDE-Debugging-DSC56F8037-using-USB-TAP/m-p/206214#M5742</guid>
      <dc:creator>Miskha</dc:creator>
      <dc:date>2012-03-07T23:18:10Z</dc:date>
    </item>
  </channel>
</rss>