<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: using DMA and periodic timer  send data to DAC in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/using-DMA-and-periodic-timer-send-data-to-DAC/m-p/204231#M5631</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I managed to deal DMA transfer i tried to put receive a buffer data located in ram from UART and then to transmit back on same uart on request all buffer. with DMA support only and interrupts.&lt;/P&gt;&lt;P&gt;First u must configure the timer but don't start it, second configure the dac for DMA requests.&lt;/P&gt;&lt;P&gt;Afther that enable clock surce from SIM for DMA and DMAMUX and set channel source for DMA channel in your case is the timer surce wich will triger the dma.&lt;/P&gt;&lt;P&gt;Afther that you must set address source wichi will be the file start address and destination address wich will be the address of the DAC register, and the corresponding offsets.&lt;/P&gt;&lt;P&gt;THis is my example&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/105316#105316" title="https://community.freescale.com/message/105316#105316"&gt;https://community.freescale.com/message/105316#105316&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Feb 2012 22:23:52 GMT</pubDate>
    <dc:creator>Nana</dc:creator>
    <dc:date>2012-02-16T22:23:52Z</dc:date>
    <item>
      <title>using DMA and periodic timer  send data to DAC</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/using-DMA-and-periodic-timer-send-data-to-DAC/m-p/204230#M5630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Friends,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can anybody help me out....??? I am a fresher..and I have to send data from sdcard to DAC using DMA and TIMER( without using processor expert).If anyone have any code related to this please send me ASAP....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2012 14:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/using-DMA-and-periodic-timer-send-data-to-DAC/m-p/204230#M5630</guid>
      <dc:creator>sumy</dc:creator>
      <dc:date>2012-02-08T14:46:31Z</dc:date>
    </item>
    <item>
      <title>Re: using DMA and periodic timer  send data to DAC</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/using-DMA-and-periodic-timer-send-data-to-DAC/m-p/204231#M5631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I managed to deal DMA transfer i tried to put receive a buffer data located in ram from UART and then to transmit back on same uart on request all buffer. with DMA support only and interrupts.&lt;/P&gt;&lt;P&gt;First u must configure the timer but don't start it, second configure the dac for DMA requests.&lt;/P&gt;&lt;P&gt;Afther that enable clock surce from SIM for DMA and DMAMUX and set channel source for DMA channel in your case is the timer surce wich will triger the dma.&lt;/P&gt;&lt;P&gt;Afther that you must set address source wichi will be the file start address and destination address wich will be the address of the DAC register, and the corresponding offsets.&lt;/P&gt;&lt;P&gt;THis is my example&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/105316#105316" title="https://community.freescale.com/message/105316#105316"&gt;https://community.freescale.com/message/105316#105316&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Feb 2012 22:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/using-DMA-and-periodic-timer-send-data-to-DAC/m-p/204231#M5631</guid>
      <dc:creator>Nana</dc:creator>
      <dc:date>2012-02-16T22:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: using DMA and periodic timer  send data to DAC</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/using-DMA-and-periodic-timer-send-data-to-DAC/m-p/204232#M5632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have already maneged an example using DMA transfer the data through UART and its working but when I come to use DAC using DMA,I face difficulty.So please if you hav some more idea abt this then please reply me ASAP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sumy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 22:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/using-DMA-and-periodic-timer-send-data-to-DAC/m-p/204232#M5632</guid>
      <dc:creator>sumy</dc:creator>
      <dc:date>2012-02-27T22:00:37Z</dc:date>
    </item>
  </channel>
</rss>