<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックCW7.2 and CW10.1 optimisation performance for Coldfire</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW7-2-and-CW10-1-optimisation-performance-for-Coldfire/m-p/203411#M5603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone explain the following?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) I have a reference project that builds with CW7.2, CW10.1 and GCC&lt;/P&gt;&lt;P&gt;2) Each of the compiler targets are set up for maximum optimisation for size (in particular CW7.2 has register passing configured)&lt;/P&gt;&lt;P&gt;3) The code size (that is, the size of the code burned into FLASH) is:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW 7.2 = 82k&lt;/P&gt;&lt;P&gt;GCC = 88k&lt;/P&gt;&lt;P&gt;CW10.1 = 113k&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would expect that CW 7.2 be a bit better than GCC but I wonder why CW10.1 is generating 38% more code (28% more that GCC). With decreasing optimisation level the code size goes up, so it is not that it is not trying...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 May 2011 04:58:14 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2011-05-05T04:58:14Z</dc:date>
    <item>
      <title>CW7.2 and CW10.1 optimisation performance for Coldfire</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW7-2-and-CW10-1-optimisation-performance-for-Coldfire/m-p/203411#M5603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone explain the following?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) I have a reference project that builds with CW7.2, CW10.1 and GCC&lt;/P&gt;&lt;P&gt;2) Each of the compiler targets are set up for maximum optimisation for size (in particular CW7.2 has register passing configured)&lt;/P&gt;&lt;P&gt;3) The code size (that is, the size of the code burned into FLASH) is:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CW 7.2 = 82k&lt;/P&gt;&lt;P&gt;GCC = 88k&lt;/P&gt;&lt;P&gt;CW10.1 = 113k&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would expect that CW 7.2 be a bit better than GCC but I wonder why CW10.1 is generating 38% more code (28% more that GCC). With decreasing optimisation level the code size goes up, so it is not that it is not trying...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2011 04:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW7-2-and-CW10-1-optimisation-performance-for-Coldfire/m-p/203411#M5603</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-05-05T04:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: CW7.2 and CW10.1 optimisation performance for Coldfire</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW7-2-and-CW10-1-optimisation-performance-for-Coldfire/m-p/203412#M5604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks to Freescale support I compared a few other settings and managed quite an imporvement by setting the following processor options:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Register coloring&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Instruction scheduling&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Peephole&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CW10.1 code size is now 84k, which is very close to the CW7.2 code size.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2011 07:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW7-2-and-CW10-1-optimisation-performance-for-Coldfire/m-p/203412#M5604</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-05-05T07:00:22Z</dc:date>
    </item>
  </channel>
</rss>