<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Production Programming... in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132265#M560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I just turned out over 50 boards.&amp;nbsp; Since this is 'early production', I just hooked them up to the BDM via the 2x3 header and then brought up CodeWarrior and hit &amp;lt;F5&amp;gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Obviously I don't want to do that for 2000 boards on a regular basis.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;On a previous project, I put a 'section' of 0.156" cardedge on the board and made an adapter with a card cage and just have the board a 'drop in'.&amp;nbsp; That wasn't an option on this case.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What I'm looking for is some kind of 'clip' that I can 'plug in' to a PCB if I leave the 2x3 header pins off the boards.&amp;nbsp; Sorta of like a 'nail board' used to do for PCB testing years ago.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If I can't find one already made, I was thinking of taking 2 pieces of 1x3 header pin strips and putting a piece of foam in between them.&amp;nbsp; I could squeeze the foam, insert it into the 2x3 hole pattern, and when I left go, the foam would hold the pins in place as it expanded.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Ok, that's the mechanical&amp;nbsp;issue.&amp;nbsp; Now for the computer side.&amp;nbsp; I obviously don't want to have to do this by using CW, hitting F5 and bringing up the debugger for each board.&amp;nbsp; Is there any simple way to 'automate' the programming through the USB-BDM pod?&amp;nbsp; I'm sure there's got to be some kind of 'batch' language I can write a script for.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Mike&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Apr 2006 21:19:21 GMT</pubDate>
    <dc:creator>mke_et</dc:creator>
    <dc:date>2006-04-12T21:19:21Z</dc:date>
    <item>
      <title>Production Programming...</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132265#M560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I just turned out over 50 boards.&amp;nbsp; Since this is 'early production', I just hooked them up to the BDM via the 2x3 header and then brought up CodeWarrior and hit &amp;lt;F5&amp;gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Obviously I don't want to do that for 2000 boards on a regular basis.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;On a previous project, I put a 'section' of 0.156" cardedge on the board and made an adapter with a card cage and just have the board a 'drop in'.&amp;nbsp; That wasn't an option on this case.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What I'm looking for is some kind of 'clip' that I can 'plug in' to a PCB if I leave the 2x3 header pins off the boards.&amp;nbsp; Sorta of like a 'nail board' used to do for PCB testing years ago.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If I can't find one already made, I was thinking of taking 2 pieces of 1x3 header pin strips and putting a piece of foam in between them.&amp;nbsp; I could squeeze the foam, insert it into the 2x3 hole pattern, and when I left go, the foam would hold the pins in place as it expanded.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Ok, that's the mechanical&amp;nbsp;issue.&amp;nbsp; Now for the computer side.&amp;nbsp; I obviously don't want to have to do this by using CW, hitting F5 and bringing up the debugger for each board.&amp;nbsp; Is there any simple way to 'automate' the programming through the USB-BDM pod?&amp;nbsp; I'm sure there's got to be some kind of 'batch' language I can write a script for.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Mike&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2006 21:19:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132265#M560</guid>
      <dc:creator>mke_et</dc:creator>
      <dc:date>2006-04-12T21:19:21Z</dc:date>
    </item>
    <item>
      <title>Re: Production Programming...</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132266#M561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Mike:&lt;BR /&gt;&lt;BR /&gt;For those volumes, I would suggest to get the parts preprogrammed in a programming shop. There are many places that would take the reels, preprogram the parts and then pack them back for soldering in the production line, for a small fee per unit.&lt;BR /&gt;&lt;BR /&gt;If you don't want to go that way, you can get a Cyclone PRO unit from P&amp;amp;E Micro, that has stand-alone programming capabilities, and you can write scripts to it for automating programming.&lt;BR /&gt;&lt;BR /&gt;Check their website : &lt;A href="http://www.pemicro.com" rel="nofollow" target="_blank"&gt;&lt;BR /&gt;www.pemicro.com&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;Alex&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2006 22:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132266#M561</guid>
      <dc:creator>alex_spotw</dc:creator>
      <dc:date>2006-04-12T22:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: Production Programming...</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132267#M562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;That's fine, and I'll probably end up with a cyclone or a variant.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But for now I was just hoping to find something that would let me use one of the USB-BDM pods we have laying around without having to have a 'shop tech' bring up the source, hit F5...&amp;nbsp; and so on.&amp;nbsp; I see the potential for INCREDIBLE problems developing real fast with that scheme.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Apr 2006 00:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132267#M562</guid>
      <dc:creator>mke_et</dc:creator>
      <dc:date>2006-04-14T00:28:43Z</dc:date>
    </item>
    <item>
      <title>Re: Production Programming...</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132268#M563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Yeah, same problem here. You can run the debugger itself as a stand alone app. but you still need to make sure that whoever is running it knows what they're doing. It would be NICE if the&amp;nbsp;programmer came with some dedicated programming software rather than having to do this with the debugger.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2006 22:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Production-Programming/m-p/132268#M563</guid>
      <dc:creator>jrpav</dc:creator>
      <dc:date>2006-04-18T22:37:54Z</dc:date>
    </item>
  </channel>
</rss>