<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Debugging from two projects - CW 10.0</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Debugging-from-two-projects-CW-10-0/m-p/197342#M5183</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you consider using debugger command loadsym in Debugger Shell?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is what a help on command loadsym returns:&lt;/P&gt;&lt;PRE&gt;COMMAND    loadsym - load a symbolics file SHORTCUT   lsym SYNTAX     loadsym &amp;lt;filename&amp;gt; [PIC load addr (hex)] EXAMPLES            loadsym myapp.elf             Loads the debug information in myapp.elf into the debugger.            loadsym mypicapp.elf 0x40000             Loads the debug information in mypicapp.elf into the debugger; symbolics addresses are              adjusted based on the alternate load address of 0x40000.&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Apr 2011 14:30:27 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2011-04-12T14:30:27Z</dc:date>
    <item>
      <title>Debugging from two projects - CW 10.0</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Debugging-from-two-projects-CW-10-0/m-p/197341#M5182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;I have two independent projects (bootloader and application projects). I am able to program both of them to the uC and it works, executing first the code from the bootloader, later it jumps to app_main and executes the code from the app project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I want is when loading the app project, be able to "stop on access point" and see the code from the bootloader project, and not just the assembler.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to pass debug information from one project to the other one?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Rubén&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Apr 2011 21:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Debugging-from-two-projects-CW-10-0/m-p/197341#M5182</guid>
      <dc:creator>RValls</dc:creator>
      <dc:date>2011-04-07T21:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging from two projects - CW 10.0</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Debugging-from-two-projects-CW-10-0/m-p/197342#M5183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you consider using debugger command loadsym in Debugger Shell?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is what a help on command loadsym returns:&lt;/P&gt;&lt;PRE&gt;COMMAND    loadsym - load a symbolics file SHORTCUT   lsym SYNTAX     loadsym &amp;lt;filename&amp;gt; [PIC load addr (hex)] EXAMPLES            loadsym myapp.elf             Loads the debug information in myapp.elf into the debugger.            loadsym mypicapp.elf 0x40000             Loads the debug information in mypicapp.elf into the debugger; symbolics addresses are              adjusted based on the alternate load address of 0x40000.&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Apr 2011 14:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Debugging-from-two-projects-CW-10-0/m-p/197342#M5183</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2011-04-12T14:30:27Z</dc:date>
    </item>
  </channel>
</rss>