<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: CW 4.6 and Windows 7</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-4-6-and-Windows-7/m-p/193395#M4964</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you have access to installed CW files. I mean Program Files\... folders CW is installed to, then you can try Natep solution from here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="57404" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/57404" jivemacro="thread" title="https://community.freescale.com/thread/57404"&gt;https://community.freescale.com/thread/57404&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Don't know how on 32bits Win7, but on 64bits Win7 CW 5.0 installer just exits and you can't install it properly. Natep solution seems to work&amp;nbsp;with CW5.0. With new unit12_z.DLL&amp;nbsp;(see page 4 of that thread) I was able to debug using P&amp;amp;E USB Multilink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be nice if Freescale made installer working on 64bits Win7. Even without P&amp;amp;E target, users still could use CW to just compile code, or even to debug in simulator mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Apr 2010 13:25:16 GMT</pubDate>
    <dc:creator>kef</dc:creator>
    <dc:date>2010-04-20T13:25:16Z</dc:date>
    <item>
      <title>CW 4.6 and Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-4-6-and-Windows-7/m-p/193394#M4963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on my reading, I know I can't run CW in Windows 7 x64, but what about the 32 bit version of Windows 7, will CW 4.6 run in this environment? &amp;nbsp;I know the P&amp;amp;E drivers for debugging are certified for Windows 7 x32 AND x64&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Apr 2010 05:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-4-6-and-Windows-7/m-p/193394#M4963</guid>
      <dc:creator>robertp</dc:creator>
      <dc:date>2010-04-20T05:13:17Z</dc:date>
    </item>
    <item>
      <title>Re: CW 4.6 and Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-4-6-and-Windows-7/m-p/193395#M4964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you have access to installed CW files. I mean Program Files\... folders CW is installed to, then you can try Natep solution from here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="57404" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/57404" jivemacro="thread" title="https://community.freescale.com/thread/57404"&gt;https://community.freescale.com/thread/57404&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Don't know how on 32bits Win7, but on 64bits Win7 CW 5.0 installer just exits and you can't install it properly. Natep solution seems to work&amp;nbsp;with CW5.0. With new unit12_z.DLL&amp;nbsp;(see page 4 of that thread) I was able to debug using P&amp;amp;E USB Multilink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be nice if Freescale made installer working on 64bits Win7. Even without P&amp;amp;E target, users still could use CW to just compile code, or even to debug in simulator mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Apr 2010 13:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CW-4-6-and-Windows-7/m-p/193395#M4964</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-04-20T13:25:16Z</dc:date>
    </item>
  </channel>
</rss>