<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックMC56F8037 in-circuit debug interfaces problems</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8037-in-circuit-debug-interfaces-problems/m-p/190993#M4843</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm starting developing fw for MC56F8037 DSC, I downloaded CW 8.3SE and as a programming/debugging interface I can choose from Codewarrior USB TAP and PEmicro USB&amp;nbsp;Universal Multilink, but none of them works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to enter debug mode with USB TAP (that seems to be correctly configured in Debugger Settings panel), I've got error message : "CCS: Library not found".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the Universal Multilink, I can't select it from CW 8.3 available interfaces.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What should I do?&lt;/P&gt;&lt;P&gt;What Development tool and what interface do you suggest me to use?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Alan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Dec 2011 19:28:24 GMT</pubDate>
    <dc:creator>AlanPas</dc:creator>
    <dc:date>2011-12-19T19:28:24Z</dc:date>
    <item>
      <title>MC56F8037 in-circuit debug interfaces problems</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8037-in-circuit-debug-interfaces-problems/m-p/190993#M4843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm starting developing fw for MC56F8037 DSC, I downloaded CW 8.3SE and as a programming/debugging interface I can choose from Codewarrior USB TAP and PEmicro USB&amp;nbsp;Universal Multilink, but none of them works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to enter debug mode with USB TAP (that seems to be correctly configured in Debugger Settings panel), I've got error message : "CCS: Library not found".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the Universal Multilink, I can't select it from CW 8.3 available interfaces.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What should I do?&lt;/P&gt;&lt;P&gt;What Development tool and what interface do you suggest me to use?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Alan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2011 19:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8037-in-circuit-debug-interfaces-problems/m-p/190993#M4843</guid>
      <dc:creator>AlanPas</dc:creator>
      <dc:date>2011-12-19T19:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8037 in-circuit debug interfaces problems</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8037-in-circuit-debug-interfaces-problems/m-p/190994#M4844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hiya,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been developing on the MC56F8037 EVM using the USB TAP successfully. On Windows XP, mind you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One thing I have found is when I create a new project, there is a button next to the build selector (right name??) i.e. where I can select SDM_pFlash / SDM_Simulator / Build all. When I mouse over it, it appears as "SDM_pFlash Settings".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway, If I click that, in the Debugger\Remote Debugging selection, I have to select 56800E Local USBTAP Connection before I have any luck. If you select that, and click Edit Connection, just make sure the Connection Type is set to "USB TAP Connection." I didnt have to change any settings.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Failing that, check under edit\ Preferences - Debugger\Remote Connections that the USB TAP appears in there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good Luck!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Laurence&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jan 2012 13:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8037-in-circuit-debug-interfaces-problems/m-p/190994#M4844</guid>
      <dc:creator>Law</dc:creator>
      <dc:date>2012-01-14T13:43:58Z</dc:date>
    </item>
  </channel>
</rss>