<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: MPC8641D...The Debugger Does not enter Main.</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8641D-The-Debugger-Does-not-enter-Main/m-p/190038#M4771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have u resolved this issue?&lt;/P&gt;&lt;P&gt;We are also facing same issue. Could u plz share some information on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Akil &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Sep 2012 13:22:04 GMT</pubDate>
    <dc:creator>akil</dc:creator>
    <dc:date>2012-09-17T13:22:04Z</dc:date>
    <item>
      <title>MPC8641D...The Debugger Does not enter Main.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8641D-The-Debugger-Does-not-enter-Main/m-p/190037#M4770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am a Newbie to MPC family..i am using code warrior 8.7 PA compiler on windows xp and win7 platform..i have code warrior debugger. i Have gone throught the getting started manual ..and created a project . when i download the code to processor the compiler throws the following error : in one of its "WINDOW". I have break points in main ..but it does not reach..main...the __start.c file...it come to the first executing instruction and then stops...even after pressing F10 it is not stepping ahead.&lt;/P&gt;&lt;P&gt;The other observation is ..at the very first line of __start.c i had set a break point...and clicked on RUN ..the control after few time came again to the same place.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the processor is getting reseted..but unable to fine the reason is it due to hardware or software.&lt;/P&gt;&lt;P&gt;Can this issue be caused due to incorrect insertion of Jtag connector[COP]..inserted in opposite manner..but as i have gone through the pin connection..they are active high so..a vcc shoul result in zero.&lt;/P&gt;&lt;P&gt;Please suggest me if i need to do some software or debugger settings in the project which can fetch the control to main.........&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt; &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt; &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am Using MPCHPCN..argo navis Motherboard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Hrishikesh.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Program "debug.elf (chain position 2, core #2)" is executing. Choose Break from the Debug menu to stop it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2011 16:59:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8641D-The-Debugger-Does-not-enter-Main/m-p/190037#M4770</guid>
      <dc:creator>hrishikesh23</dc:creator>
      <dc:date>2011-12-13T16:59:16Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8641D...The Debugger Does not enter Main.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8641D-The-Debugger-Does-not-enter-Main/m-p/190038#M4771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have u resolved this issue?&lt;/P&gt;&lt;P&gt;We are also facing same issue. Could u plz share some information on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Akil &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Sep 2012 13:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8641D-The-Debugger-Does-not-enter-Main/m-p/190038#M4771</guid>
      <dc:creator>akil</dc:creator>
      <dc:date>2012-09-17T13:22:04Z</dc:date>
    </item>
  </channel>
</rss>