<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Fast code download to target(MPC8569E) in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Fast-code-download-to-target-MPC8569E/m-p/190007#M4769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;'setads', 'args' and 'go' are not a standard CCS commands.&amp;nbsp; I suspect you're running something other than the CCS that comes bunded with CodeWarrior Dev Studio, which means that the CCS used by the CodeWarrior debugger is different from the ccs that understands 'setads', which could very well explain the different performance results.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regardless, the 'ccs::set_max_tck' command determines the upper limit of your downloads.&amp;nbsp; The MPC8569 should be able to run at up to 32MHz so try increasing the 'ccs::set_max_tck' value from 12000 to 24000.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jun 2009 03:55:04 GMT</pubDate>
    <dc:creator>ronco</dc:creator>
    <dc:date>2009-06-18T03:55:04Z</dc:date>
    <item>
      <title>Fast code download to target(MPC8569E)</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Fast-code-download-to-target-MPC8569E/m-p/190006#M4768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have not checked "Do not use fast download" in my Connection Settings.&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;During by debugging in IDE, code is downloaded at faster rate.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But when I download the code to target using CCS, download speed is less(it does not use fast download).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;DriverVer=08/20/2007, 9.0.0&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN class="Apple-style-span"&gt;&lt;SPAN class="Apple-style-span"&gt;Commands used to run download and run the elf&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;setads 8569ads 1&lt;/DIV&gt;&lt;DIV&gt;reset&lt;/DIV&gt;&lt;DIV&gt;ccs::set_max_tck 0 12000&lt;/DIV&gt;&lt;DIV&gt;load TEST_RUN.elf&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;args 0x80 1770405119&lt;/DIV&gt;&lt;DIV&gt;clear&lt;/DIV&gt;&lt;DIV&gt;go&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jun 2009 14:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Fast-code-download-to-target-MPC8569E/m-p/190006#M4768</guid>
      <dc:creator>sathishkumarps</dc:creator>
      <dc:date>2009-06-13T14:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: Fast code download to target(MPC8569E)</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Fast-code-download-to-target-MPC8569E/m-p/190007#M4769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;'setads', 'args' and 'go' are not a standard CCS commands.&amp;nbsp; I suspect you're running something other than the CCS that comes bunded with CodeWarrior Dev Studio, which means that the CCS used by the CodeWarrior debugger is different from the ccs that understands 'setads', which could very well explain the different performance results.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regardless, the 'ccs::set_max_tck' command determines the upper limit of your downloads.&amp;nbsp; The MPC8569 should be able to run at up to 32MHz so try increasing the 'ccs::set_max_tck' value from 12000 to 24000.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2009 03:55:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Fast-code-download-to-target-MPC8569E/m-p/190007#M4769</guid>
      <dc:creator>ronco</dc:creator>
      <dc:date>2009-06-18T03:55:04Z</dc:date>
    </item>
  </channel>
</rss>