<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Simulator/Debugger &amp; License File questions on CW for HSC12(X) v4.6, build 6345</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189302#M4726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1- How are you starting the debugger?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; From the IDE? From the command line? From the explorer window?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Which is the command line you are using to start the debugger (if you start it from&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; the IDE you can see the command line in the "Build Extras" panel).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I did perform some tests on my side and working from the IDE, I can connect to the&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; same debugger again without any problem.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;2- Which versions of the tools are you refrying to when you say new and old version?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; Answer here really depends on the versions you are using.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; New version is probably V4.6.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; What&amp;nbsp;is old version?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; Is there any reason you cannot work with one single version of CodeWarrior?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Feb 2008 20:36:43 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2008-02-14T20:36:43Z</dc:date>
    <item>
      <title>Simulator/Debugger &amp; License File questions on CW for HSC12(X) v4.6, build 6345</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189301#M4725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I'm using CW for HSC12(X) v4.6, build 6345 and have a couple of questions.&lt;/DIV&gt;&lt;DIV&gt;1) When I run True-Time Simulator &amp;amp; Real-Time Debugger I have to close out the entire instance before I run another instance.&amp;nbsp; If I forget to close out the previous instance I will get a hardware error and have to close out both instances and run the True-Time Simulator &amp;amp; Real-Time Debugger again.&amp;nbsp; Is there anyway to always have the same window that is open to just update with the new information?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;2) I have a new version of CW with a current license file on my PC but is it possible to load an older&amp;nbsp;version of CW on my PC and use the&amp;nbsp;existing license file?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks in advance,&lt;/DIV&gt;&lt;DIV&gt;Christina&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2008 02:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189301#M4725</guid>
      <dc:creator>gator_n_tn</dc:creator>
      <dc:date>2008-02-14T02:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: Simulator/Debugger &amp; License File questions on CW for HSC12(X) v4.6, build 6345</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189302#M4726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1- How are you starting the debugger?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; From the IDE? From the command line? From the explorer window?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Which is the command line you are using to start the debugger (if you start it from&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; the IDE you can see the command line in the "Build Extras" panel).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I did perform some tests on my side and working from the IDE, I can connect to the&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; same debugger again without any problem.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;2- Which versions of the tools are you refrying to when you say new and old version?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; Answer here really depends on the versions you are using.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; New version is probably V4.6.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; What&amp;nbsp;is old version?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; Is there any reason you cannot work with one single version of CodeWarrior?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2008 20:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189302#M4726</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-02-14T20:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: Simulator/Debugger &amp; License File questions on CW for HSC12(X) v4.6, build 6345</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189303#M4727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;1) I start the debugger from within the IDE by clicking on the the green arrow with the bug icon.&amp;nbsp; In my "Build Extras" panel located under Edit&amp;gt;&amp;gt;P&amp;amp;E Multilink CyclonePro Settings&amp;gt;&amp;gt;Build Extras, I have the following under "Arguments": %targetFilePath -Prod=%projectFileDir\P&amp;amp;E_Multilink_CyclonePro.ini -instance=icd12.&amp;nbsp; From documents I've read, this statement should allow the debugger to open up the same instance but my debugger opens an entirely new debugger window.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;2) The new version I am running on my PC&amp;nbsp;has a license file that says&amp;nbsp;"HC12 V4.6 Special Edition."&amp;nbsp;The other version I would also like to install is HC12(X) v4.5 Service Pack XFR128, build 060515 with license file "(740): HC12 v4.5 Professional Edition.&amp;nbsp; The reason I'm asking is because another co-worker has an older version and he can not view my files from the new version and I'm getting errors on his version when I open his files with my version. So I was hoping to have one computer with all versions represented.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for responding to my last post and I hope this makes my questions a little clearer.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2008 22:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189303#M4727</guid>
      <dc:creator>gator_n_tn</dc:creator>
      <dc:date>2008-02-14T22:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: Simulator/Debugger &amp; License File questions on CW for HSC12(X) v4.6, build 6345</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189304#M4728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1- I have the exact same command line. And starting a new debug session uses the same instance of&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; external debugger.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; I would recommend you to submit a service request for that.&lt;BR /&gt;&lt;BR /&gt;Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR" rel="nofollow" target="_blank"&gt;here&lt;/A&gt; to submit a service request.&lt;BR /&gt;&lt;BR /&gt;Make sure to attach a reproducible project and installed product information to the service request.&lt;BR /&gt;To generate the required information:&lt;BR /&gt;- Start CodeWarrior&lt;BR /&gt;- Open the project&lt;BR /&gt;- Select "Help" -&amp;gt; "Pack and Go" and follow instructions on the screen.&lt;BR /&gt;&lt;BR /&gt;Attach the generated .zip file to the SR. Also provide exact reproducible steps with the SR.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;2- If you take a CodeWarrior for HC12 V4.5 professional license it should allow you to use both CodeWarrior for HC12 V4.5 and V4.6.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2008 16:24:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Simulator-Debugger-License-File-questions-on-CW-for-HSC12-X-v4-6/m-p/189304#M4728</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-02-15T16:24:35Z</dc:date>
    </item>
  </channel>
</rss>