<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックHow can I flash my application?</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-can-I-flash-my-application/m-p/187950#M4622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I write my application and tested it inside internal RAM. Now I wanna flash it to use it as a stand alone application.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Therefore I changed the debug configuration from MK60N512VMD100_INTERNAL_RAM to MK60N512VMD100_INTERNAL_FLASH, but it has no effect.&lt;/P&gt;&lt;P&gt;With the internal Flash configuration I can debug my program as before. But after a reset or after power up my application doesn t run.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using the flash might be more complicated than I expect.&lt;/P&gt;&lt;P&gt;So what must I do to get my program into flash?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also try to use the simple flash programmer that is part of Codewarrior, but I alway get error messages when I try to use it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use the TWR K60 Tower and CodeWarrior 10.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;May Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ulf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Dec 2011 17:53:47 GMT</pubDate>
    <dc:creator>UB39</dc:creator>
    <dc:date>2011-12-06T17:53:47Z</dc:date>
    <item>
      <title>How can I flash my application?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-can-I-flash-my-application/m-p/187950#M4622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I write my application and tested it inside internal RAM. Now I wanna flash it to use it as a stand alone application.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Therefore I changed the debug configuration from MK60N512VMD100_INTERNAL_RAM to MK60N512VMD100_INTERNAL_FLASH, but it has no effect.&lt;/P&gt;&lt;P&gt;With the internal Flash configuration I can debug my program as before. But after a reset or after power up my application doesn t run.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using the flash might be more complicated than I expect.&lt;/P&gt;&lt;P&gt;So what must I do to get my program into flash?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also try to use the simple flash programmer that is part of Codewarrior, but I alway get error messages when I try to use it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use the TWR K60 Tower and CodeWarrior 10.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;May Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ulf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2011 17:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-can-I-flash-my-application/m-p/187950#M4622</guid>
      <dc:creator>UB39</dc:creator>
      <dc:date>2011-12-06T17:53:47Z</dc:date>
    </item>
    <item>
      <title>Re: How can I flash my application?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-can-I-flash-my-application/m-p/187951#M4623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please do not cross post your question into other forums. I have answered it elswhere.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2011 20:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-can-I-flash-my-application/m-p/187951#M4623</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-12-06T20:37:53Z</dc:date>
    </item>
  </channel>
</rss>