<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Working with user parameters in data flash for Processor Expert project in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Working-with-user-parameters-in-data-flash-for-Processor-Expert/m-p/186417#M4525</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you can disable the generation of the linker command file:&lt;/P&gt;&lt;P&gt;go to the CPU bean/Bean Inspector for the CPU, then click on the 'Build options' tab: there is an option to disable the generation of the cmd/linker file.&lt;/P&gt;&lt;P&gt;There you can as well specify your own memory areas (on top of the generated ones), so this may be what you need?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jun 2009 15:08:48 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2009-06-01T15:08:48Z</dc:date>
    <item>
      <title>Working with user parameters in data flash for Processor Expert project</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Working-with-user-parameters-in-data-flash-for-Processor-Expert/m-p/186416#M4524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have PE project for DSP56F801 (Code Warrior DS for DSC56800/E v. 8.2.3 build 7 special edition.&lt;/P&gt;&lt;P&gt;I need write some parameters to data&amp;nbsp;flash during compiling &amp;amp;&amp;nbsp;&amp;nbsp;update later this parameters&amp;nbsp;via reserved copy to another page&amp;nbsp;from PC with&amp;nbsp;my config programm. How can I do it without intervention to .cmd linker file (THIS BEAN MODULE IS GENERATED BY THE TOOL. DO NOT MODIFY IT.)? &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2009 13:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Working-with-user-parameters-in-data-flash-for-Processor-Expert/m-p/186416#M4524</guid>
      <dc:creator>Dekabrist</dc:creator>
      <dc:date>2009-06-01T13:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: Working with user parameters in data flash for Processor Expert project</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Working-with-user-parameters-in-data-flash-for-Processor-Expert/m-p/186417#M4525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;you can disable the generation of the linker command file:&lt;/P&gt;&lt;P&gt;go to the CPU bean/Bean Inspector for the CPU, then click on the 'Build options' tab: there is an option to disable the generation of the cmd/linker file.&lt;/P&gt;&lt;P&gt;There you can as well specify your own memory areas (on top of the generated ones), so this may be what you need?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2009 15:08:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Working-with-user-parameters-in-data-flash-for-Processor-Expert/m-p/186417#M4525</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2009-06-01T15:08:48Z</dc:date>
    </item>
    <item>
      <title>Re: Working with user parameters in data flash for Processor Expert project</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Working-with-user-parameters-in-data-flash-for-Processor-Expert/m-p/186418#M4526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It obvious metod, but inconvenient.&amp;nbsp;Is the metod to define&amp;nbsp;constant data with init value &amp;amp; place it to hard address to&amp;nbsp;xflash from compiler or assembler?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2009 16:55:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Working-with-user-parameters-in-data-flash-for-Processor-Expert/m-p/186418#M4526</guid>
      <dc:creator>Dekabrist</dc:creator>
      <dc:date>2009-06-01T16:55:15Z</dc:date>
    </item>
  </channel>
</rss>