<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is &amp;quot;Include&amp;quot; in the MCP project? in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/What-is-quot-Include-quot-in-the-MCP-project/m-p/124755#M45</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It means to add the files to the project. That is:&lt;BR /&gt;&lt;BR /&gt;Project | Add Files...&lt;BR /&gt;&lt;BR /&gt;and then use the Add Files dialog window to navigate to the files you wish to become part of the build process.&lt;BR /&gt;&lt;BR /&gt;The files typically appear whatever "directory" you're using at the time in the CodeWarrior IE. I placed quotes around directory because the directory structure in the Project window is an artifice managed by the CodeWarrior IDE. It doesn't matter where the files appear in the Project window. If they're part of the build process, the IDE will use them.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2006 20:16:47 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2006-07-24T20:16:47Z</dc:date>
    <item>
      <title>What is "Include" in the MCP project?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/What-is-quot-Include-quot-in-the-MCP-project/m-p/124754#M44</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just wanted to know what it means when a document says&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"Include pwr.c and pwrlib.c in the MCP project"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Im not actually sure what the means. Does it mean that the two files are to be added to the "lib" or "sources" section of the project?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Im quite confused, any help will be apprieciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kris&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2006 20:07:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/What-is-quot-Include-quot-in-the-MCP-project/m-p/124754#M44</guid>
      <dc:creator>Shankman</dc:creator>
      <dc:date>2006-07-24T20:07:05Z</dc:date>
    </item>
    <item>
      <title>Re: What is "Include" in the MCP project?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/What-is-quot-Include-quot-in-the-MCP-project/m-p/124755#M45</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It means to add the files to the project. That is:&lt;BR /&gt;&lt;BR /&gt;Project | Add Files...&lt;BR /&gt;&lt;BR /&gt;and then use the Add Files dialog window to navigate to the files you wish to become part of the build process.&lt;BR /&gt;&lt;BR /&gt;The files typically appear whatever "directory" you're using at the time in the CodeWarrior IE. I placed quotes around directory because the directory structure in the Project window is an artifice managed by the CodeWarrior IDE. It doesn't matter where the files appear in the Project window. If they're part of the build process, the IDE will use them.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2006 20:16:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/What-is-quot-Include-quot-in-the-MCP-project/m-p/124755#M45</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2006-07-24T20:16:47Z</dc:date>
    </item>
  </channel>
</rss>