<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Codewarrior V6.2 Special edition not installing on Windows 7 64-bit!</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185332#M4461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is another solution, a rather awkward and kind of a PITA one, and that is to install a virtual machine such as VMWARE on your 64-bit host, then inside of that install your old 32-bit OS, then inside of that install your old version of CW. Set it up so that the host system resources are visible within the 32-bit OS, then you can run the old CW and communicate with your Freescale target hardware. I tried that once, and I thought it it just kind of buggered things up with regard to the target development process. Good luck!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Nov 2011 22:13:37 GMT</pubDate>
    <dc:creator>buckeyeman</dc:creator>
    <dc:date>2011-11-25T22:13:37Z</dc:date>
    <item>
      <title>Codewarrior V6.2 Special edition not installing on Windows 7 64-bit!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185329#M4458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am getting the following error message when I install codewarrior V6.2 SE onto my windows 7 64-bit computer. Cam someone suggest a fix or point out whats missing here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Nov 2011 14:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185329#M4458</guid>
      <dc:creator>karthick1987</dc:creator>
      <dc:date>2011-11-23T14:57:12Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior V6.2 Special edition not installing on Windows 7 64-bit!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185330#M4459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sadly, those older versions of CW run only on 32-bit hosts. You need a 10.x version, my experinece has demonstrated that. Freescale came late to the party regarding 64-bit host OS support, IMHO. Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2011 20:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185330#M4459</guid>
      <dc:creator>buckeyeman</dc:creator>
      <dc:date>2011-11-24T20:23:36Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior V6.2 Special edition not installing on Windows 7 64-bit!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185331#M4460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for that buckeyeman! Its a shame they dont work with 64-bit OS. I have windows 7 64 bit installed &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2011 11:00:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185331#M4460</guid>
      <dc:creator>karthick1987</dc:creator>
      <dc:date>2011-11-25T11:00:23Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior V6.2 Special edition not installing on Windows 7 64-bit!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185332#M4461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is another solution, a rather awkward and kind of a PITA one, and that is to install a virtual machine such as VMWARE on your 64-bit host, then inside of that install your old 32-bit OS, then inside of that install your old version of CW. Set it up so that the host system resources are visible within the 32-bit OS, then you can run the old CW and communicate with your Freescale target hardware. I tried that once, and I thought it it just kind of buggered things up with regard to the target development process. Good luck!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2011 22:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Codewarrior-V6-2-Special-edition-not-installing-on-Windows-7-64/m-p/185332#M4461</guid>
      <dc:creator>buckeyeman</dc:creator>
      <dc:date>2011-11-25T22:13:37Z</dc:date>
    </item>
  </channel>
</rss>