<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC56F8006Demo Stuck in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181390#M4169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Figured it out, I enabled "Wait for device to power up at connect". &amp;nbsp;When I program the board it pauses while it's waiting for power up then I'll unplug my board then plug it back in and it is able to program the board. &amp;nbsp;After that though, when I'm running the LED example it stops on the T1_Interrupt every time (there's no breakpoint there). &amp;nbsp;If I hit reset the program runs normally. &amp;nbsp;Still looking into it . . .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 07 Mar 2010 14:45:17 GMT</pubDate>
    <dc:creator>davefs</dc:creator>
    <dc:date>2010-03-07T14:45:17Z</dc:date>
    <item>
      <title>MC56F8006Demo Stuck</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181389#M4168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My MC56F8006DEMO is having problems. &amp;nbsp;When I connect it to power several of the LEDs come on, then all of them turn off except LED4, which just blinks. &amp;nbsp;When I connect my USB TAP to it then the "Run/Pause" LED comes on and stays on. &amp;nbsp;If I try and burn something to it via the USB TAP I get an error that says "CSS Protocol Plugin: Unknown Protocol Error". &amp;nbsp;Did I somehow brick my MC56F8006DEMO? &amp;nbsp;Is there a way to get it going again. &amp;nbsp;The code on the board right now shouldn't be causing any LEDs to blink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Mar 2010 16:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181389#M4168</guid>
      <dc:creator>davefs</dc:creator>
      <dc:date>2010-03-06T16:01:24Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8006Demo Stuck</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181390#M4169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Figured it out, I enabled "Wait for device to power up at connect". &amp;nbsp;When I program the board it pauses while it's waiting for power up then I'll unplug my board then plug it back in and it is able to program the board. &amp;nbsp;After that though, when I'm running the LED example it stops on the T1_Interrupt every time (there's no breakpoint there). &amp;nbsp;If I hit reset the program runs normally. &amp;nbsp;Still looking into it . . .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Mar 2010 14:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181390#M4169</guid>
      <dc:creator>davefs</dc:creator>
      <dc:date>2010-03-07T14:45:17Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8006Demo Stuck</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181391#M4170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also have same problem "CSS Protocol Plugging: Unknown Protocol Error" when using MC56F8006DEMO kit either with parallel port&amp;nbsp; JTAG or USB TAP adapters, but problem does not appear when I use MC56F8013DEMO kit:&lt;/P&gt;&lt;P&gt;This lead me to think the problem is something related to MC56F8006DEMO kit or MCU, but I can't find some app note about this issue.&lt;/P&gt;&lt;P&gt;¿What should I do to put this demo kit to work properly again?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Mar 2010 04:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181391#M4170</guid>
      <dc:creator>Heron</dc:creator>
      <dc:date>2010-03-19T04:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8006Demo Stuck</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181392#M4171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So the tools work with one board and not the other? Please file a service request on that. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_self"&gt;here&lt;/A&gt; to do that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Mar 2010 19:59:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181392#M4171</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-03-19T19:59:32Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8006Demo Stuck</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181393#M4172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Tom,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SR Number:&amp;nbsp; 1-614214891&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Mar 2010 03:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MC56F8006Demo-Stuck/m-p/181393#M4172</guid>
      <dc:creator>Heron</dc:creator>
      <dc:date>2010-03-22T03:13:02Z</dc:date>
    </item>
  </channel>
</rss>