<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FLEXlm: can compile but not link in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FLEXlm-can-compile-but-not-link/m-p/181213#M4155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was confused to, but now the problem is solved:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to compile a solution of a partner company just knowing that they are using a Coldfire processor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Being a Freescale/CodeWarrior newbie I didn't realise that there are two different Coldfires, a V1 and a V2 (the project was set up and I have only to maintenance/check some code in it). So I installed only the licence for the V2 and not the one for the V1 (including HCS08).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Obviously the V1 and V2 compiler use the same license, so I was able to start the IDE and compile files, but the linker of the two derivates does not have the same license...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I installed the the correct license and "happy linking" starts :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks CrasyCat for the fast response!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chris&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 May 2009 12:24:56 GMT</pubDate>
    <dc:creator>kusti_ch</dc:creator>
    <dc:date>2009-05-15T12:24:56Z</dc:date>
    <item>
      <title>FLEXlm: can compile but not link</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FLEXlm-can-compile-but-not-link/m-p/181211#M4153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed the CodeWarrior Development Studio (V6.2, build 8127)&amp;nbsp; for ColdFire V1 on my Windows XP machine. The Licence Server for my floating licence is (after having documentation troubles) set up und running - I can compile the project received from our partner company.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But thats all: I can compile but I can not link... the following message appears:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive-quote"&gt;Error&amp;nbsp;&amp;nbsp; : Unable to use the plugin "Embedded ColdFire Linker". It is licensed and a valid license key was not found.&lt;BR /&gt;License server does not support this feature&lt;BR /&gt;Feature:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Win32_ColdFireV1_Special_128&lt;BR /&gt;License path:&amp;nbsp; C:\Programme\Freescale\CodeWarrior for Microcontrollers -&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; V6.2\license.dat&lt;BR /&gt;FLEXlm error:&amp;nbsp; -18,147&lt;BR /&gt;For further information, refer to the FLEXlm End User Manual,&lt;BR /&gt;available at "&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.macrovision.com%2F" rel="nofollow" target="_blank"&gt;www.macrovision.com&lt;/A&gt;".&lt;/BLOCKQUOTE&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The error code explanation in the End User Manual does not really help and so I analysed the licence file: there is no such entry as Win32_ColdFireV1_Special_128 or Win32_ColdFireV1_Special_64.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know why I there is a different licence needed for compiling and linking?&amp;nbsp; What can I do to solve this problem?&amp;nbsp; (There was no reaction in any kind of the support so far)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any idea solving this problem!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Chris &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2009 13:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FLEXlm-can-compile-but-not-link/m-p/181211#M4153</guid>
      <dc:creator>kusti_ch</dc:creator>
      <dc:date>2009-05-14T13:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXlm: can compile but not link</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FLEXlm-can-compile-but-not-link/m-p/181212#M4154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am a bit confused here.&lt;/P&gt;&lt;P&gt;Are you using a special edition license or are you using a floating license on a FLEXlm license server?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using a floating license can you get me the log file generated on the license server?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2009 18:33:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FLEXlm-can-compile-but-not-link/m-p/181212#M4154</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-05-14T18:33:10Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXlm: can compile but not link</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FLEXlm-can-compile-but-not-link/m-p/181213#M4155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was confused to, but now the problem is solved:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to compile a solution of a partner company just knowing that they are using a Coldfire processor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Being a Freescale/CodeWarrior newbie I didn't realise that there are two different Coldfires, a V1 and a V2 (the project was set up and I have only to maintenance/check some code in it). So I installed only the licence for the V2 and not the one for the V1 (including HCS08).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Obviously the V1 and V2 compiler use the same license, so I was able to start the IDE and compile files, but the linker of the two derivates does not have the same license...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I installed the the correct license and "happy linking" starts :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks CrasyCat for the fast response!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chris&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2009 12:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/FLEXlm-can-compile-but-not-link/m-p/181213#M4155</guid>
      <dc:creator>kusti_ch</dc:creator>
      <dc:date>2009-05-15T12:24:56Z</dc:date>
    </item>
  </channel>
</rss>