<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to direct printf() to console or UART or other peripherals? in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176898#M3866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same question on codewarrior 8.8 for MPC8306 chip, I used project wizard to generate one project which puts out a message to the UART terminal on the MPC8306_SOM evaluation board, when I looked through the project, I saw it includes a library output file "UART2_8306_SOM.UC.a", but there is no ".h" file associated with it also when I am stepping through the project from .reset or __start, I didn't see it called any function to initilize the UART, but the board do put out message into the UART terminal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to know how to change the baudrate and other setups such as re-direct printf function into another UART on my own board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Nov 2011 05:07:42 GMT</pubDate>
    <dc:creator>HZ</dc:creator>
    <dc:date>2011-11-04T05:07:42Z</dc:date>
    <item>
      <title>How to direct printf() to console or UART or other peripherals?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176894#M3862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do you change the peripheral that will receive the printf() calls?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess it defaulkts in CW to console, I would like it to be a UART.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2011 19:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176894#M3862</guid>
      <dc:creator>tmf</dc:creator>
      <dc:date>2011-10-25T19:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to direct printf() to console or UART or other peripherals?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176895#M3863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; - Which CPU are you targeting (HC08, HC12, Coldfire, ..)&lt;BR /&gt;&amp;nbsp; - Which version of CodeWarrior are you using?&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2011 14:11:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176895#M3863</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2011-10-26T14:11:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to direct printf() to console or UART or other peripherals?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176896#M3864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW10.1 and Kinetis&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2011 21:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176896#M3864</guid>
      <dc:creator>tmf</dc:creator>
      <dc:date>2011-10-26T21:29:47Z</dc:date>
    </item>
    <item>
      <title>Re: How to direct printf() to console or UART or other peripherals?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176897#M3865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also need to knw how to correctly redirect console IO in the tower bareboard application to the serial port. I know how to do it under MQX, but not under a non-MQX project.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2011 02:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176897#M3865</guid>
      <dc:creator>JohnBabrick</dc:creator>
      <dc:date>2011-11-04T02:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to direct printf() to console or UART or other peripherals?</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176898#M3866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same question on codewarrior 8.8 for MPC8306 chip, I used project wizard to generate one project which puts out a message to the UART terminal on the MPC8306_SOM evaluation board, when I looked through the project, I saw it includes a library output file "UART2_8306_SOM.UC.a", but there is no ".h" file associated with it also when I am stepping through the project from .reset or __start, I didn't see it called any function to initilize the UART, but the board do put out message into the UART terminal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to know how to change the baudrate and other setups such as re-direct printf function into another UART on my own board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Nov 2011 05:07:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-direct-printf-to-console-or-UART-or-other-peripherals/m-p/176898#M3866</guid>
      <dc:creator>HZ</dc:creator>
      <dc:date>2011-11-04T05:07:42Z</dc:date>
    </item>
  </channel>
</rss>