<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Problem with Debug in CW for DSC56800/E v.8.0</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129194#M380</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It seems to me that the ccs.exe is not running on your machine. Typically, the installer sets it up so it is launched automatically. You should check if you have a ccc.exe task running on your machine (e.g. consult your windows task mananger).&lt;BR /&gt;You can launch it by hand too, it is lockated inside your installation of Hawk 8.0, probably for you at this location:&lt;BR /&gt;C:\Program Files\Freescale\Hawk 8.0\ccs\bin\ccs.exe&lt;BR /&gt;&lt;BR /&gt;Launch the .exe and check if the problem goes away.&lt;BR /&gt;&lt;BR /&gt;Additional considerations:&lt;BR /&gt;If you have any special firewall software (e.g. ZoneAlarm) installed, you may check the settings, as the debugger and the ccs.exe are communicating through TCP/IP (local on your machine).&lt;BR /&gt;&lt;BR /&gt;Hope this helps,&lt;BR /&gt;Erich&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Apr 2007 14:41:42 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2007-04-03T14:41:42Z</dc:date>
    <item>
      <title>Problem with Debug in CW for DSC56800/E v.8.0</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129193#M379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using a free version of CW for DSC56800/E v.8.0, and I would like to solve my problem which occurs when I try to &lt;/SPAN&gt;&lt;STRONG&gt;"Debug"&lt;/STRONG&gt;&lt;SPAN&gt; any of CodeWarrior_Examples. I allways get a message:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;"CSSProtocolPlugin: CSS: Command Converter not present."&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had some problems with CW for HC12 in the past, and it disapeared after instalation of new license file (obtained from Metrowerks). Is this the same case?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestion?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;I&gt;&lt;BR /&gt;SW: CW for DSC56800/E v.8.0&lt;BR /&gt;Target: MC56F8013&lt;BR /&gt;Installed plugins: see attached .zip&lt;BR /&gt;&lt;/I&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2007 13:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129193#M379</guid>
      <dc:creator>Andik</dc:creator>
      <dc:date>2007-04-03T13:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Debug in CW for DSC56800/E v.8.0</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129194#M380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It seems to me that the ccs.exe is not running on your machine. Typically, the installer sets it up so it is launched automatically. You should check if you have a ccc.exe task running on your machine (e.g. consult your windows task mananger).&lt;BR /&gt;You can launch it by hand too, it is lockated inside your installation of Hawk 8.0, probably for you at this location:&lt;BR /&gt;C:\Program Files\Freescale\Hawk 8.0\ccs\bin\ccs.exe&lt;BR /&gt;&lt;BR /&gt;Launch the .exe and check if the problem goes away.&lt;BR /&gt;&lt;BR /&gt;Additional considerations:&lt;BR /&gt;If you have any special firewall software (e.g. ZoneAlarm) installed, you may check the settings, as the debugger and the ccs.exe are communicating through TCP/IP (local on your machine).&lt;BR /&gt;&lt;BR /&gt;Hope this helps,&lt;BR /&gt;Erich&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2007 14:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129194#M380</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2007-04-03T14:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Debug in CW for DSC56800/E v.8.0</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129195#M381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Erich,&lt;BR /&gt;thank you for quick answer, it looks like "yes, that should be the reason of my troubles" but I tried both and the problem remains.&lt;BR /&gt;&lt;BR /&gt;I have the &lt;B&gt;ccs.exe started.&lt;/B&gt; Also my &lt;B&gt;ZoneAlarm is configured to trust&lt;/B&gt; the CodeWarrior Connection Server (ccs.exe). For certainty, I shut down the Firewall, CCS, restarted the CCS and CW, but still the same problem.&lt;BR /&gt;&lt;BR /&gt;Here is the CCS log.&lt;BR /&gt;&lt;I&gt;&lt;BR /&gt;CodeWarrior Connection Server console display active (Tcl8.4.6 / Tk8.4.6)&lt;BR /&gt;Loading CCSAPI Tcl interface (C:/Program Files/Metrowerks/CodeWarrior CW56_V8.0/ccs/bin/ccstcl.dll)...&lt;BR /&gt;Initializing arm namespace...&lt;BR /&gt;Initializing rnbo_sync namespace...&lt;BR /&gt;Initializing rnbo_mcore namespace...&lt;BR /&gt;Initializing rnbo_sc140 namespace...&lt;BR /&gt;Initializing rnbo_ipcm namespace...&lt;BR /&gt;Initializing sc140 namespace...&lt;BR /&gt;Initializing zassc namespace...&lt;BR /&gt;Initializing hawkv2 namespace...&lt;BR /&gt;Initializing dsp563 namespace...&lt;BR /&gt;Initializing dsp566 namespace...&lt;BR /&gt;Initializing dsp568 namespace...&lt;BR /&gt;Initializing msc8102_sync namespace...&lt;BR /&gt;Initializing msc8102_sc140 namespace...&lt;BR /&gt;Initializing ms116 namespace...&lt;BR /&gt;Initializing odyssey_sync namespace...&lt;BR /&gt;Initializing odyssey_ms1162 namespace...&lt;BR /&gt;Initializing mpc5500_sync namespace...&lt;BR /&gt;Initializing mpc5500_zen namespace...&lt;BR /&gt;Initializing mpc5500_npc namespace...&lt;BR /&gt;Initializing mpc5500_ndedi namespace...&lt;BR /&gt;Initializing mpc5500_nxdm namespace...&lt;BR /&gt;Initializing mpc5500_etpu namespace...&lt;BR /&gt;Initializing sjc namespace...&lt;BR /&gt;Initializing mpc603e namespace... Loading tppc.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing mpc603ei namespace... Loading tppc.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing e500 namespace... Loading te500.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing mpc7410 namespace... Loading tmpc7410.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing mpc74x7 namespace... Loading tmpc74x7.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing mpc7447a namespace... Loading tmpc7447a.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing j2i2c namespace...&lt;BR /&gt;Initializing mpc83xx namespace... Loading t83xx.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing mpc755 namespace... Loading tmpc755.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing arm11 namespace... Loading tarm11.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing mpc7448 namespace... Loading tmpc7448.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Initializing coldfire namespace...&lt;BR /&gt;Initializing mpc8641 namespace... Loading tmpc8641.tcl...Done&lt;BR /&gt;&lt;BR /&gt;Executing autoexec.tcl...&lt;BR /&gt;0: Parallel Port(SPP) (lpt:1) CC software ver. {3.3}&lt;BR /&gt;Server listening on port: 41475&lt;BR /&gt;Clients accepted from all hosts&lt;BR /&gt;Connection #1 accepted from localhost at Tue Apr 03 09:53:34 2007&lt;BR /&gt;Connection #1 from localhost closed at Tue Apr 03 09:53:34 2007&lt;BR /&gt;(bin) 1 %&lt;BR /&gt;&lt;/I&gt;&lt;BR /&gt;&lt;BR /&gt;Now I'm wondering, if it is possible to run the example code in simulation-like mode (without hardware connected). I just want to try, how the DSC56 core works to get a practice with ASM. The project target is set to "smm internal memory with pROM-to-xRAM copy"&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2007 15:13:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129195#M381</guid>
      <dc:creator>Andik</dc:creator>
      <dc:date>2007-04-03T15:13:54Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Debug in CW for DSC56800/E v.8.0</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129196#M382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Andik,&lt;BR /&gt;yes, you can use the simulator. The easiest way is if you simply create a working base and go from there. You can do this with File &amp;gt; New, DSP56800x New Project Wizard &amp;gt; Simulators and go through the rest of the steps. You will see that this sets up a connection to the simulator (ALT-F7, or project preferences -&amp;gt; Debugger &amp;gt; Remote Debugging).&lt;BR /&gt;&lt;BR /&gt;The setup and capabilities of the simulator vs hardware are a little bit different, but above sample should give you a good starting point.&lt;BR /&gt;&lt;BR /&gt;As for your original problem (still existing): you may check the CCS console output. And check (of course) if your run control/connection to the hardware is working fine?&lt;BR /&gt;&lt;BR /&gt;Erich&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2007 15:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-Debug-in-CW-for-DSC56800-E-v-8-0/m-p/129196#M382</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2007-04-03T15:28:48Z</dc:date>
    </item>
  </channel>
</rss>