<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Metrowerks PCS for Linux: Problems with UTS_MACHINE</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Metrowerks-PCS-for-Linux-Problems-with-UTS-MACHINE/m-p/128929#M375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I can not install PCS to Suse 10.0 ? is it not compatible???&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2006 13:39:17 GMT</pubDate>
    <dc:creator>qwe</dc:creator>
    <dc:date>2006-06-13T13:39:17Z</dc:date>
    <item>
      <title>Metrowerks PCS for Linux: Problems with UTS_MACHINE</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Metrowerks-PCS-for-Linux-Problems-with-UTS-MACHINE/m-p/128928#M374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello to everybody.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have imported one modified kernel (based on 2.4.18) with the Linux Kernel Imported Tool. I have compiled the kernel with the default compiler (as started project I have used the BSP for Motorola mpc860fads) successfully.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But now I want to use the gcc 3.3.2 to compile my kernel.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Then, with the GNU Toolchain Import Tool, I&amp;nbsp; import the gcc 3.3.2 that come with CodeWarrior Development Studio (Linux Platform Edition) 2.5. It's ok.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Next, I configure the kernel package to use the new toolchain and force rebuild the component.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;There is a compilation error with the file init/version.c. This file uses UTS_MACHINE define, that is defined in the command line with option -D (command line defined in the Makefile at the top of the kernel directory). This define must be "ppc" (with double quotes), but is defined as ppp (without double quotes).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Why does it work with the default compiler but doesn't work with the imported toolchain? Some idea?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Mar 2006 16:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Metrowerks-PCS-for-Linux-Problems-with-UTS-MACHINE/m-p/128928#M374</guid>
      <dc:creator>fjpse</dc:creator>
      <dc:date>2006-03-16T16:50:29Z</dc:date>
    </item>
    <item>
      <title>Re: Metrowerks PCS for Linux: Problems with UTS_MACHINE</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Metrowerks-PCS-for-Linux-Problems-with-UTS-MACHINE/m-p/128929#M375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I can not install PCS to Suse 10.0 ? is it not compatible???&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2006 13:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Metrowerks-PCS-for-Linux-Problems-with-UTS-MACHINE/m-p/128929#M375</guid>
      <dc:creator>qwe</dc:creator>
      <dc:date>2006-06-13T13:39:17Z</dc:date>
    </item>
    <item>
      <title>Re: Metrowerks PCS for Linux: Problems with UTS_MACHINE</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Metrowerks-PCS-for-Linux-Problems-with-UTS-MACHINE/m-p/128930#M376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;This page describes system requirements for the CodeWarrior Platform Creation Suite:&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CWS-PCS-CX&amp;amp;parentCode=null&amp;amp;nodeId=01272686888587" rel="nofollow" target="_blank"&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/A&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CWS-PCS-CX&amp;amp;parentCode=null&amp;amp;nodeId=01272686888587" target="test_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CWS-PCS-CX&amp;amp;parentCode=null&amp;amp;nodeId=01272686888587&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;What problem do you encounter exactly?&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Marc.&lt;/FONT&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2006 01:11:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Metrowerks-PCS-for-Linux-Problems-with-UTS-MACHINE/m-p/128930#M376</guid>
      <dc:creator>marc_paquette</dc:creator>
      <dc:date>2006-06-14T01:11:07Z</dc:date>
    </item>
  </channel>
</rss>