<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CodeWarrior can not run in Ubuntu-8.10 in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174743#M3670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After I install CodeWarrior in my Ubuntu-8.10, When I run cwide, it will be exception, the error message as following:&lt;/P&gt;&lt;P&gt;$./cwide&lt;/P&gt;&lt;P&gt;[: 241: closing paren expected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;gcc: 4.1.2. /cwide: 241: Bad substitution&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Btw, CodeWarrior Version: CWX-MGT-LLAPP-EX Rev. D Lot #111408-4009 How to solve the problem? Thanks for any help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Apr 2009 10:55:29 GMT</pubDate>
    <dc:creator>cowley</dc:creator>
    <dc:date>2009-04-23T10:55:29Z</dc:date>
    <item>
      <title>CodeWarrior can not run in Ubuntu-8.10</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174743#M3670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After I install CodeWarrior in my Ubuntu-8.10, When I run cwide, it will be exception, the error message as following:&lt;/P&gt;&lt;P&gt;$./cwide&lt;/P&gt;&lt;P&gt;[: 241: closing paren expected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;gcc: 4.1.2. /cwide: 241: Bad substitution&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Btw, CodeWarrior Version: CWX-MGT-LLAPP-EX Rev. D Lot #111408-4009 How to solve the problem? Thanks for any help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2009 10:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174743#M3670</guid>
      <dc:creator>cowley</dc:creator>
      <dc:date>2009-04-23T10:55:29Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior can not run in Ubuntu-8.10</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174744#M3671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According FreeScale support rely from e-mail:&amp;nbsp; for this question, gcc should downgrade to 4.1.2 version,&lt;/P&gt;&lt;P&gt;I did it, but the exception is stillexistence, Does anyone give me a solution, Thanks!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To downgrade&amp;nbsp; gcc and reinstall CodeWarrior, when run, the same exceptions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;cowely@cowely-desktop:/media/cdrom$ /usr/local/Freescale/CodeWarrior-MGT-9.2/CodeWarriorIDE/cwide&lt;BR /&gt;[: 241: closing paren expected&lt;BR /&gt;gcc: 4.1.2&lt;BR /&gt;/usr/local/Freescale/CodeWarrior-MGT-9.2/CodeWarriorIDE/cwide: 241: Bad substitution&lt;BR /&gt;cowely@cowely-desktop:/media/cdrom$ gcc -v&lt;BR /&gt;Using built-in specs.&lt;BR /&gt;Target: i486-linux-gnu&lt;BR /&gt;Configured with: ../src/configure -v --enable-languages=c,c++,fortran,objc,obj-c++,treelang --prefix=/usr --enable-shared --with-system-zlib --libexecdir=/usr/lib --without-included-gettext --enable-threads=posix --enable-nls --program-suffix=-4.1 --enable-__cxa_atexit --enable-clocale=gnu --enable-libstdcxx-debug --enable-mpfr --with-tune=i686 --enable-checking=release i486-linux-gnu&lt;BR /&gt;Thread model: posix&lt;BR /&gt;gcc version 4.1.2 20061115 (prerelease) (Debian 4.1.1-21)&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2009 15:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174744#M3671</guid>
      <dc:creator>cowley</dc:creator>
      <dc:date>2009-04-27T15:10:13Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior can not run in Ubuntu-8.10</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174745#M3672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Code warrior can be made to run in Ubuntu 8.10 by&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)Downgrading the libx11-6 to version 1.0.3-7 .But this can be done by removing of libx11-xcb and compiz packages as 1.0.3-7 is not compatible with these packages.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2)Also change the script in cwide from #!/bin/sh&amp;nbsp; to #!/bin/bash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;enjoy !!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2009 15:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174745#M3672</guid>
      <dc:creator>gnk</dc:creator>
      <dc:date>2009-06-04T15:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior can not run in Ubuntu-8.10</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174746#M3673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, just change the ./cwide !#/bin/sh to&amp;nbsp; !#/bin/bash to get further.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No, i wouldn't recomment libX11 downgrading. Just get a new libX11 from git, configure it with "--without-xcb" option and build it. The resulted libs will be installed by default in /usr/local/lib.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edit again cwide script and change LD_LIBRARY_PATH= to&amp;nbsp; LD_LIBRARY_PATH"/usr/local/lib".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Start CW and have fun!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2009 17:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-can-not-run-in-Ubuntu-8-10/m-p/174746#M3673</guid>
      <dc:creator>Reky</dc:creator>
      <dc:date>2009-06-16T17:06:32Z</dc:date>
    </item>
  </channel>
</rss>