<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Code Warrior for MCU V10.2 (Eclipse) - Import Export Issues</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174185#M3632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey all, so I've tried copying a project folder from one computer into the workspace folder on a second computer and it still only allowed the config that was active on the last computer (RAM, not FLASH) to be built... Does this work for anyone else?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jun 2012 12:34:46 GMT</pubDate>
    <dc:creator>Schwac</dc:creator>
    <dc:date>2012-06-25T12:34:46Z</dc:date>
    <item>
      <title>Code Warrior for MCU V10.2 (Eclipse) - Import Export Issues</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174182#M3629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;I have a question that I could really use some help with. I have tried to use the import/export procedure to import and export projects between two installations of Codewarrior for MCU V10.2 (Eclipse) on different computers (both windows). When I clean and rebuild the project on the pc I transfer the project to, it will only build the last configuration that was used (FLASH OR RAM). I develop by using RAM most of the time, then deploy by programming to the FLASH, so I really need these two configurations. When I try to build the nonworking of the two configs, I get the following error (for example):&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;E:\\CW MCU v10.2\\gnu\\bin\\mingw32-make -j16 all&lt;BR /&gt;mingw32-make: *** No rule to make target `../Project_Settings/Linker_Files/MCF52259_Internal_Flash.lcf\’, needed by `PATH_PLAYER_6_20_12.elf\’. Stop.&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;The one workaround I have is to build the other config on the other PC and copy to file ”MCF52259_Internal_Flash.lcf” or ”MCF52259_Internal_Ram.lcf” (depending upon which one it’s missing) to the ”/Project_Settings/Linker_Files/” folder on the PC I’ve transferred the project to. That said, this is obviously not the proper way to do this; After all, isn't that what built in import/export functionality is for? Has anyone else had luck building the ”other” configuration once you’ve moved the file?&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;Thank You,&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;Cory&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2012 23:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174182#M3629</guid>
      <dc:creator>Schwac</dc:creator>
      <dc:date>2012-06-21T23:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior for MCU V10.2 (Eclipse) - Import Export Issues</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174183#M3630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears that the Export function is only exporting the information for the project's active configuration.&lt;/P&gt;&lt;P&gt;Have you tried just copying the project folder out of the Eclipse workspace directory from the first system and placing it in the workspace folder on the second system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jun 2012 20:03:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174183#M3630</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2012-06-22T20:03:16Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior for MCU V10.2 (Eclipse) - Import Export Issues</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174184#M3631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply. I will try to simply move the whole folder over later today.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does this import/export, move to a new computer, then build both configs cause any errors for you Tom? Anyone else?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jun 2012 02:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174184#M3631</guid>
      <dc:creator>Schwac</dc:creator>
      <dc:date>2012-06-23T02:28:05Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior for MCU V10.2 (Eclipse) - Import Export Issues</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174185#M3632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey all, so I've tried copying a project folder from one computer into the workspace folder on a second computer and it still only allowed the config that was active on the last computer (RAM, not FLASH) to be built... Does this work for anyone else?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2012 12:34:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Code-Warrior-for-MCU-V10-2-Eclipse-Import-Export-Issues/m-p/174185#M3632</guid>
      <dc:creator>Schwac</dc:creator>
      <dc:date>2012-06-25T12:34:46Z</dc:date>
    </item>
  </channel>
</rss>