<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Sine, Cos functions without float data types</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169696#M3316</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, due to memory issues, I prefer to follow Taylor series for my function instead of Look up table.&lt;/P&gt;&lt;P&gt;Infact, it is the requirement for me to use Taylor series method.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I update something in my sample code in the attachment.&lt;/P&gt;&lt;P&gt;Kindly guide me please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Oct 2011 08:52:18 GMT</pubDate>
    <dc:creator>Kasu</dc:creator>
    <dc:date>2011-10-06T08:52:18Z</dc:date>
    <item>
      <title>Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169692#M3312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have to write Sine and Cos Math functions but without using the standard library functions from math.h file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because, I dont want to write these functions with integer data type. But library functions support floating point.&lt;/P&gt;&lt;P&gt;I tried to do some research, but most of the algorithms are based on floating point itself (using Taylor series, horner method).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can any one please provide sample code for Sin, Cos algorithms based on Integers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using Codewarrior compiler v2.7 for MPC5604P.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 25 Sep 2011 11:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169692#M3312</guid>
      <dc:creator>Kasu</dc:creator>
      <dc:date>2011-09-25T11:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169693#M3313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You do not mention the angular resolution that you require?&amp;nbsp; I assume that the return value&amp;nbsp;could be presented as a signed 16-bit binary fraction.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One&amp;nbsp;alternative approach might utilise a look-up table to represent one quadrant of a sinusoid, with linear interpolation used to increase the angular resolution.&amp;nbsp; The first quadrant angle may be easily derived from an arbitrary angle, and the sign determined, for both sine and cosine functions.&amp;nbsp; Since the binary fraction does not incorporate the values +1 and -1, these might need to be treated as&amp;nbsp;special cases.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For&amp;nbsp;this approach, it might be simpler to base your input on degree units, rather than radians.&amp;nbsp; With a one degree table increment, the table size would be 90 words.&amp;nbsp; For the linear interpolation process, you might have an 8-bit value as the fractional part of the&amp;nbsp;angle input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Sep 2011 06:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169693#M3313</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-09-26T06:01:20Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169694#M3314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mac,&amp;nbsp;Sorry the late reply.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1. I would like to have angular resolution of -pi to +pi (-180deg to 180 deg)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. And return value of my function would be unsigned short (Frac16)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, I'm not quite familiar in this type of coding (i.e. Sine function and also converting the code from floating point type to support integer type)..&amp;nbsp;I attached my sample code here, kindly check it please.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2011 02:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169694#M3314</guid>
      <dc:creator>Kasu</dc:creator>
      <dc:date>2011-10-06T02:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169695#M3315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You might be better off with using the tabular method bigmac suggested. Your Taylor series expansion looks like it'll will really suffer from truncation errors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Oh, and I'm not sure if your compiler supports modulus operations or not...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2011 04:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169695#M3315</guid>
      <dc:creator>AirDragon</dc:creator>
      <dc:date>2011-10-06T04:05:26Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169696#M3316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, due to memory issues, I prefer to follow Taylor series for my function instead of Look up table.&lt;/P&gt;&lt;P&gt;Infact, it is the requirement for me to use Taylor series method.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I update something in my sample code in the attachment.&lt;/P&gt;&lt;P&gt;Kindly guide me please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2011 08:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169696#M3316</guid>
      <dc:creator>Kasu</dc:creator>
      <dc:date>2011-10-06T08:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169697#M3317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Taylor series are infinite!. Dropping the most and leaving just few nonzero coefficients (in general) gives very poor accuracy.&amp;nbsp;There are methods to optimize series order by slightly tuning series coefficients and greatly improving resulting accuracy. Google for Minimax Polynomial etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now about your code.&lt;/P&gt;&lt;P&gt;1)&amp;nbsp;ss16_tmp_Angle_In_Rad = 32767*(((s16_tmp_Angle_In_Deg) * pi)/180);&lt;/P&gt;&lt;P&gt;Is pi floating point number here? So why not to just use FP sin()? If indeed integer, then you should first do all multiplies, and divide after all mulls are done. As you may know integer divide drops remainder. Dividing at the end should give you more procise result.&lt;/P&gt;&lt;P&gt;2) 90degs is pi/2, which is above 1. pi/2 won't fit signed /32768 integer fraction! You need to use long integers.&lt;/P&gt;&lt;P&gt;3) I'm not sure if you know it, but to multiply two /32768 integer fructions you should multiply them first (producing long integer), and then divide the product by 32768. All those 32bit calculations can take compareable time to what you may have using standard sin().&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See attached two excel files, isin.xls for /32768 fractions and isin8.xls for /256 fractions. To emulate integer math, I was&amp;nbsp;using excell INT() function. Series coefficient are optimized to produce smaller error. BTW /256 sine still is good enough with just two series members, s7=0. So go ahead implementing it all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2011 16:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169697#M3317</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-10-06T16:22:22Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169698#M3318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hm, don't you have spare 720 bytes of flash on MPC5604P for full sin table (360 degs * 2bytes)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2011 16:32:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169698#M3318</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-10-06T16:32:48Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169699#M3319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kef,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks alot for your help.. Your excel sheet helped me to implement the Sin, Cos functions properly to my requirement.&lt;/P&gt;&lt;P&gt;I understand now, how to scale the normal sine/cos function for the integer data type..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i.e. &amp;nbsp; Sin(x) = x - (x^3)/3! + (x^5)/5! - (x^7)/7! ......-&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;can be scaled as x-((x/32768)^3)/3! +&amp;nbsp;((x/32768)^5)/5! - ((x/32768)^7)/7! ..........&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, the following website gave me valuable information... &amp;nbsp;it might be helpful for the guys who wants to implement Trig functions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://mathonweb.com/help_ebook/html/algorithms.htm" rel="nofollow" target="_blank"&gt;http://mathonweb.com/help_ebook/html/algorithms.htm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Have a nice weekend.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Oct 2011 04:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169699#M3319</guid>
      <dc:creator>Kasu</dc:creator>
      <dc:date>2011-10-15T04:05:37Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169700#M3320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm glad it helped.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;i.e. &amp;nbsp; Sin(x) = x - (x^3)/3! + (x^5)/5! - (x^7)/7! ......-&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;can be scaled as x-((x/32768)^3)/3! +&amp;nbsp;((x/32768)^5)/5! - ((x/32768)^7)/7! ..........&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Not at all. Formula doesn't look right. But those /32768 after each multiplication are required to preserve fixed point format of 15bits fractional part. You translate real numbers X to integer fraction x doing x = X*32768. Now with integer fractions you do x+x for X+X, x-x for X-X. But you need to do x*x/32768 for X*X and x*32768/x&amp;nbsp; for X/X.&lt;/P&gt;&lt;P&gt;Example that should explain it a bit. What if you use &lt;FONT color="#ff00ff"&gt;1000&lt;/FONT&gt; instead of 32768 factor. You convert real &lt;FONT color="#0000ff"&gt;0.1&lt;/FONT&gt; to integer &lt;FONT color="#ff0000"&gt;100&lt;/FONT&gt;, &lt;FONT color="#0000ff"&gt;0.01&lt;/FONT&gt; to integer &lt;FONT color="#ff0000"&gt;10&lt;/FONT&gt; etc. So product &lt;FONT color="#0000ff"&gt;0.1&lt;/FONT&gt;*&lt;FONT color="#0000ff"&gt;0.1&lt;/FONT&gt;=&lt;FONT color="#0000ff"&gt;0.01&lt;/FONT&gt; should translate to &lt;FONT color="#ff0000"&gt;100&lt;/FONT&gt;*&lt;FONT color="#ff0000"&gt;100&lt;/FONT&gt;=&lt;FONT color="#ff0000"&gt;10&lt;/FONT&gt;, while in reality you get 100*100=10000. You need to divide product by &lt;FONT color="#ff00ff"&gt;1000&lt;/FONT&gt; to get right fixed point result.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Oct 2011 22:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169700#M3320</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2011-10-15T22:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169701#M3321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks alot for the correction Kef. I understand it now !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Oct 2011 23:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169701#M3321</guid>
      <dc:creator>Kasu</dc:creator>
      <dc:date>2011-10-17T23:55:28Z</dc:date>
    </item>
    <item>
      <title>Re: Sine, Cos functions without float data types</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169702#M3322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using the truncated series method, per the&amp;nbsp;supplied link, it seems possible to slightly rearrange the&amp;nbsp;expressions to simplify the processing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The first three terms of the sine series can alternatively be expressed as:&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;x*( 1 - (x*x)*( 1 - (x*x)/20 )/6 )&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;and the first four terms of the cosine series&amp;nbsp;can be expressed as:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;1 - (x*x)*( 1 - (x*x)*( 1 - (x*x)/30 )/12 )/2&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;The following code appears to produce the expected result for fractional integer arithmetic.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;#define P4 25736L   // pi / 4 * 32768// Integer sine function for angles &amp;lt;= 45 degreesint sin_( int deg){   long xrad, sxr;   long a = 32768;   long b = 196608;             // 6 * a      xrad = deg * P4 / 45;        // Convert to radians   sxr = xrad * xrad / a;      return ((int)(xrad * (a - sxr * (a - sxr / 20) / b) / a));}// Integer cosine function for angles &amp;lt;= 45 degreesint cos_( int deg){   long xrad, sxr;   long a = 32768;   long b = 65536;              // 2 * a   long c = 393216;             // 12 * a      if (deg == 0)        return (int)(a - 1);      // Maximum limit for signed 16-bit      xrad = deg * P4 / 45;        // Convert to radians   sxr = xrad * xrad / a;      return ((int)(a - sxr * (a - sxr * (a - sxr / 30) / c) / b));}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:17:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Sine-Cos-functions-without-float-data-types/m-p/169702#M3322</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2020-10-29T09:17:54Z</dc:date>
    </item>
  </channel>
</rss>