<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169617#M3310</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello, could you please tell me where is that forum?,&amp;nbsp; there are to many topics and it is difficoult to find it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Aug 2010 22:57:19 GMT</pubDate>
    <dc:creator>Juanes</dc:creator>
    <dc:date>2010-08-11T22:57:19Z</dc:date>
    <item>
      <title>CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169612#M3305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hye,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use codeWarrior for MCF 52259 DEMO BOARD(with JM60 OSBDM).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can erase flash but when i try to program the flash, an alert appear : GDI PROTOCOL PLUGIN, The Debugger can not write memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;this message don't appear necessary at beginning of programming flash but sometimes at the middle or at the end, sometimes programation is successful but when i try to debug i have the same message.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;what is the problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(i have already can program and debug the demo board without problem, this error appear without reason)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2010 15:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169612#M3305</guid>
      <dc:creator>benoit_rey</dc:creator>
      <dc:date>2010-01-25T15:29:28Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169613#M3306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;when i program succesfully, when i debug and when programm access to breakpoint, i make the same message but when i stop the debug, an other message appear: "COLDFIRE GDI PROTOCOL ADAPTER : An invalid preference was passed to the coldfire gdi protocol"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;any idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2010 22:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169613#M3306</guid>
      <dc:creator>benoit_rey</dc:creator>
      <dc:date>2010-01-26T22:50:51Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169614#M3307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What version of the operating system are you running? And is it 64-bit, by any chance?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2010 21:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169614#M3307</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-01-27T21:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169615#M3308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I use Windows XP but it is in 32-bit.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2010 17:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169615#M3308</guid>
      <dc:creator>benoit_rey</dc:creator>
      <dc:date>2010-01-28T17:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169616#M3309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, it is not the 64-bit OS problem, then. You have two choices:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Since you are using an OSBDM connection, go to the new Freescale OSBDM for ColdFire forum (they turned it on yesterday) and ask your question there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) File a service request for this. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_self"&gt;here&lt;/A&gt; to do that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2010 21:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169616#M3309</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-01-28T21:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169617#M3310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello, could you please tell me where is that forum?,&amp;nbsp; there are to many topics and it is difficoult to find it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Aug 2010 22:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169617#M3310</guid>
      <dc:creator>Juanes</dc:creator>
      <dc:date>2010-08-11T22:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 7.1.2 for MCF52259 : the debugger can not write memory</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169618#M3311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The OSBDM forum is one of the community forums, which is separate from the CodeWarrior forums. That probably makes it a bit harder to find. &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt; The Community forums, which contains several OSBDM projects, can be found &lt;A href="http://forums.freescale.com/t5/Community-Projects/ct-p/COMPROJ" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Aug 2010 23:16:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-7-1-2-for-MCF52259-the-debugger-can-not-write-memory/m-p/169618#M3311</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-08-11T23:16:44Z</dc:date>
    </item>
  </channel>
</rss>