<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with QuickStart tool r2.3 in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-QuickStart-tool-r2-3/m-p/169087#M3244</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed the DSP56800EQUICKSTARTSW.exe on my CodeWarrior for DSC56800E v8.2.3 installation.&lt;/P&gt;&lt;P&gt;On my side the DSP56800E_Quick_Start r2.3 project in the File ¦ New is available.&lt;/P&gt;&lt;P&gt;This is defined during the quickstart installation. You must select the CodeWarrior Installation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The project wizard is defined in the \Stationery folder.&lt;/P&gt;&lt;P&gt;After to have installed quickstart, the DSP56800E_Quick_Start r2.3 under the \Stationery.&lt;/P&gt;&lt;P&gt;If it's not the case, you can:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- re install Quickstart and select the right CodeWarrior installation,&lt;/P&gt;&lt;P&gt;&amp;nbsp;- move it manually.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I recommend you the first solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Apr 2009 19:29:29 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2009-04-06T19:29:29Z</dc:date>
    <item>
      <title>Problem with QuickStart tool r2.3</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-QuickStart-tool-r2-3/m-p/169086#M3243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; I'm a beginner using codewarrior 8.2 &amp;amp; I m working with 56F8XXX DSCs. I have problem with quick start tool. I have installed quick start &amp;amp; I have done all the required settings (in prefernces &amp;amp; key bindings). But when I start creating new project I'm not getting the DSP56800E Quick start r2.3 stationery option which I should get.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;IMG border="0" src="https://community.nxp.com/" /&gt;I have attached the picture also that shows what I should get.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has any one encountered similiar problem or does any one know the solution for this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;P&gt;Saran&lt;IMG border="0" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2009 19:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-QuickStart-tool-r2-3/m-p/169086#M3243</guid>
      <dc:creator>z3Lxru</dc:creator>
      <dc:date>2009-04-02T19:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with QuickStart tool r2.3</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-QuickStart-tool-r2-3/m-p/169087#M3244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed the DSP56800EQUICKSTARTSW.exe on my CodeWarrior for DSC56800E v8.2.3 installation.&lt;/P&gt;&lt;P&gt;On my side the DSP56800E_Quick_Start r2.3 project in the File ¦ New is available.&lt;/P&gt;&lt;P&gt;This is defined during the quickstart installation. You must select the CodeWarrior Installation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The project wizard is defined in the \Stationery folder.&lt;/P&gt;&lt;P&gt;After to have installed quickstart, the DSP56800E_Quick_Start r2.3 under the \Stationery.&lt;/P&gt;&lt;P&gt;If it's not the case, you can:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- re install Quickstart and select the right CodeWarrior installation,&lt;/P&gt;&lt;P&gt;&amp;nbsp;- move it manually.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I recommend you the first solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Apr 2009 19:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Problem-with-QuickStart-tool-r2-3/m-p/169087#M3244</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2009-04-06T19:29:29Z</dc:date>
    </item>
  </channel>
</rss>