<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to test EVM board in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-test-EVM-board/m-p/168203#M3189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am using DSP56F801 EVM board. Further i am using an evaluation version of Code Warrior 8.2.3. The EVM was working fine but all of a suddent I am not able to download the code onto the EVM board. I get the following error "CCS protocol Plugin: Unknown Protocol error". I think the JTAG IC could be spoilt. Is there a way to test if the JTAG on the EVM works properly. I would also like to know if there is any application to test the DSP56801 EVM board as a whole.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Rak**bleep**h.S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Mar 2009 12:21:40 GMT</pubDate>
    <dc:creator>rakshith</dc:creator>
    <dc:date>2009-03-31T12:21:40Z</dc:date>
    <item>
      <title>How to test EVM board</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-test-EVM-board/m-p/168203#M3189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am using DSP56F801 EVM board. Further i am using an evaluation version of Code Warrior 8.2.3. The EVM was working fine but all of a suddent I am not able to download the code onto the EVM board. I get the following error "CCS protocol Plugin: Unknown Protocol error". I think the JTAG IC could be spoilt. Is there a way to test if the JTAG on the EVM works properly. I would also like to know if there is any application to test the DSP56801 EVM board as a whole.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Rak**bleep**h.S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2009 12:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-test-EVM-board/m-p/168203#M3189</guid>
      <dc:creator>rakshith</dc:creator>
      <dc:date>2009-03-31T12:21:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to test EVM board</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-test-EVM-board/m-p/168204#M3190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We support 2 interfaces:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- USBTAP,&lt;/P&gt;&lt;P&gt;&amp;nbsp;- sample parallel cable.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is a jumper on the board to switch between the 2 interfaces.&lt;/P&gt;&lt;P&gt;On the project, the connection settings must be addapted too to support USBTap or Sample parallel cable.&lt;/P&gt;&lt;P&gt;There are some examples available on the installation.&lt;/P&gt;&lt;P&gt;You can get it via the wizard (File New) or other ones under the folder \(CodeWarrior_Examples).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See below more details about the connections checking.&lt;/P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;Did you tried with an example delivered on the installation ?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;If you get the same problem with an example delivered on the installation, the problem should be:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- with the USBTap,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- or with the PC configuration,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- or with the board,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- or with the project config.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Check the USBTap.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;When you plug it to the PC, the USBTap must be detected.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;If this is not the case may be the interface is damaged.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;When the interface is connected to the board and to the PC, the 2 light should be on. Is it the case ?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Check the board.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Check that the Jtag connection is selected. This is done by a jumper. This jumper define if the Jtag or the // connector is used. Is it working using a sample // cable as interface ? Do you have another board ?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Check the PC.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Can you install the tool on another PC ?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Check the project.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;After to start the debug session, the ccs tool is automatically launched too.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Be sure that the right settings are selected in the target settings panels.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Open it and go to Debugger | Remote Debugging and select 56800 Local USBTAP connection.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2009 14:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/How-to-test-EVM-board/m-p/168204#M3190</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2009-04-01T14:53:48Z</dc:date>
    </item>
  </channel>
</rss>