<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Symbolics in library in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Symbolics-in-library/m-p/167691#M3126</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you sure you built the library with debug settings that would include the symbolics?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To add another file path to CodeWarrior's search function, proceed as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Go to the Target Settings panel (type ALT + F7).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Click on the Access Paths choice in the pane at the left.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3) Click Add, navigate to the folder your library is in, then click OK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The folder should appear in the panel display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jan 2010 22:00:39 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2010-01-19T22:00:39Z</dc:date>
    <item>
      <title>Symbolics in library</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Symbolics-in-library/m-p/167690#M3125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i tried to move some file from a project in a new library, and then to link the library with the project.&lt;/P&gt;&lt;P&gt;All the code works well but the library symbols are not visible during the debug.&lt;/P&gt;&lt;P&gt;I think this is a path problem. Anybody can tell how explicitate the library path in the main project?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Paolo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2010 19:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Symbolics-in-library/m-p/167690#M3125</guid>
      <dc:creator>PaoloRozzi</dc:creator>
      <dc:date>2010-01-15T19:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: Symbolics in library</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Symbolics-in-library/m-p/167691#M3126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you sure you built the library with debug settings that would include the symbolics?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To add another file path to CodeWarrior's search function, proceed as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Go to the Target Settings panel (type ALT + F7).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Click on the Access Paths choice in the pane at the left.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3) Click Add, navigate to the folder your library is in, then click OK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The folder should appear in the panel display.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2010 22:00:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Symbolics-in-library/m-p/167691#M3126</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-01-19T22:00:39Z</dc:date>
    </item>
  </channel>
</rss>