<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CodeWarrior USB TAP connectivity in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-USB-TAP-connectivity/m-p/128657#M312</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Are you still having problems with the USBTAP?&amp;nbsp; Do you have something other than a USBTAP to connect to your board?&amp;nbsp; Can you connect to your EVM board using the parallel port cable?&amp;nbsp; When you hit the debug button in the IDE it will create a CodeWarrior Icon in the system toolbar.&amp;nbsp; This icon is for the Command Converter Server.&amp;nbsp; If you click on this icon it will bring up&amp;nbsp;the Command Converter Server window.&amp;nbsp; In this window type the following:&lt;/DIV&gt;&lt;DIV&gt;log verbose test.log&lt;/DIV&gt;&lt;DIV&gt;After you have done this try to connect again to the board by hitting the debug icon in the project window.&amp;nbsp; You can send this issue and this log file to &lt;A href="mailto:support@freescale.com" rel="nofollow" target="_blank"&gt;support@freescale.com&lt;/A&gt; for further investigation.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Mar 2006 06:36:48 GMT</pubDate>
    <dc:creator>Irene</dc:creator>
    <dc:date>2006-03-24T06:36:48Z</dc:date>
    <item>
      <title>CodeWarrior USB TAP connectivity</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-USB-TAP-connectivity/m-p/128656#M311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am using the USB TAP CWH-UTP-ONCE-HX Rev B. to debug software written for the DSP56F803. Two days ago when I left my project everything was working fine, I could program the chip, set breakpoints, read memory, etc. Today when I went to load the newest version of my software the USB TAP can't communicate and I get a message back saying "CCS: core not responding." Nothing has changed since it last worked. The board / chip / USB TAP / computer have not even been touched. I have tried rebooting, restarting the DSP, different computer, different USB cable, different DSP chip, etc. The USB TAP can't even program my DSP56F803 eval board. When I do try to program the chip the TX/RX led goes from blinking green to orange quickly and then back to blinking green. The Run/Pause led initally is off but lights up solid red after the error is displayed. Is there anything else I can do to troubleshoot? I am starting to worry that my USB TAP is fried and I absolutely need this thing working over the next two days or my project will fall off schedule. Please help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Matt&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2006 05:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-USB-TAP-connectivity/m-p/128656#M311</guid>
      <dc:creator>mchabot</dc:creator>
      <dc:date>2006-03-14T05:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior USB TAP connectivity</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-USB-TAP-connectivity/m-p/128657#M312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Are you still having problems with the USBTAP?&amp;nbsp; Do you have something other than a USBTAP to connect to your board?&amp;nbsp; Can you connect to your EVM board using the parallel port cable?&amp;nbsp; When you hit the debug button in the IDE it will create a CodeWarrior Icon in the system toolbar.&amp;nbsp; This icon is for the Command Converter Server.&amp;nbsp; If you click on this icon it will bring up&amp;nbsp;the Command Converter Server window.&amp;nbsp; In this window type the following:&lt;/DIV&gt;&lt;DIV&gt;log verbose test.log&lt;/DIV&gt;&lt;DIV&gt;After you have done this try to connect again to the board by hitting the debug icon in the project window.&amp;nbsp; You can send this issue and this log file to &lt;A href="mailto:support@freescale.com" rel="nofollow" target="_blank"&gt;support@freescale.com&lt;/A&gt; for further investigation.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2006 06:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-USB-TAP-connectivity/m-p/128657#M312</guid>
      <dc:creator>Irene</dc:creator>
      <dc:date>2006-03-24T06:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior USB TAP connectivity</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-USB-TAP-connectivity/m-p/128658#M313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I was able to program the EVM board with the parallel port and I have built a parallel port programmer for my prototype board using some old cables and IC's I had around the lab. I think the USB TAP is just plain dead. I have a warranty return request in with Freescale right now. Thanks for the help.&lt;BR /&gt;&lt;BR /&gt;Matt&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2006 21:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-USB-TAP-connectivity/m-p/128658#M313</guid>
      <dc:creator>mchabot</dc:creator>
      <dc:date>2006-03-24T21:04:36Z</dc:date>
    </item>
  </channel>
</rss>