<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックConfigurations are not remembered unless complete project is inside the default workspace directory.</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Configurations-are-not-remembered-unless-complete-project-is/m-p/167330#M3109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When making different configurations off the same source, unless the complete project is inside the default workspace directory, only the original configuration is remembered. I have to recreate it if I leave CodeWarrior 10.2. It also does not save the "make this workspace the default" setting.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have CW10.2 installed on Windows 7 in C:\Freescale.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 May 2012 03:20:14 GMT</pubDate>
    <dc:creator>davezawislak</dc:creator>
    <dc:date>2012-05-30T03:20:14Z</dc:date>
    <item>
      <title>Configurations are not remembered unless complete project is inside the default workspace directory.</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Configurations-are-not-remembered-unless-complete-project-is/m-p/167330#M3109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When making different configurations off the same source, unless the complete project is inside the default workspace directory, only the original configuration is remembered. I have to recreate it if I leave CodeWarrior 10.2. It also does not save the "make this workspace the default" setting.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have CW10.2 installed on Windows 7 in C:\Freescale.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2012 03:20:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Configurations-are-not-remembered-unless-complete-project-is/m-p/167330#M3109</guid>
      <dc:creator>davezawislak</dc:creator>
      <dc:date>2012-05-30T03:20:14Z</dc:date>
    </item>
    <item>
      <title>Re: Configurations are not remembered unless complete project is inside the default workspace direct</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Configurations-are-not-remembered-unless-complete-project-is/m-p/167331#M3110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to file&amp;nbsp; service request on this problem. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_self"&gt;here&lt;/A&gt; to go to the online service request page.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2012 19:08:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Configurations-are-not-remembered-unless-complete-project-is/m-p/167331#M3110</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2012-05-30T19:08:13Z</dc:date>
    </item>
  </channel>
</rss>