<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: CodeWarrior 6.3 Installation Error</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-6-3-Installation-Error/m-p/167126#M3096</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you check the VISTA limitation in Welcome_CW_MCUs.txt?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;WINDOWS VISTA SPECIFIC LIMITATIONS:&lt;BR /&gt;-----------------------------------&lt;/P&gt;&lt;P&gt;The following limitations are applicable only if you are installing the product on Windows Vista:&lt;/P&gt;&lt;P&gt;(1) During installation, security messages may pop up concerning drivers being installed. It is highly&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; recommended to click on the option "continue anyway..", so the drivers can be installed.&lt;/P&gt;&lt;P&gt;(2) When opening the Codewarrior components (IDE, Debugger etc.) Firewall warnings may appear&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; with the option to block or unblock the application. It is advisable to click on the unblock option to&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; continue.&lt;/P&gt;&lt;P&gt;(3) For more VISTA specific limitations after the installation, please refer to:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "{INSTALLATION DIRECTORY}\Release_Notes\HC08\Notes_CW_MCUs_V6 3_Vista.txt"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;GENERAL LIMITATIONS:&lt;BR /&gt;--------------------&lt;/P&gt;&lt;P&gt;The following limitations are applicable to Windows Vista, Windows XP:&lt;/P&gt;&lt;P&gt;(1) It is highly recommended to have at least 400 MB of free space on the Windows system disk.&lt;BR /&gt;(2) Product supports 32-bit versions of Windows XP, Windows Vista.&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Dec 2010 21:48:06 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2010-12-06T21:48:06Z</dc:date>
    <item>
      <title>CodeWarrior 6.3 Installation Error</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-6-3-Installation-Error/m-p/167125#M3095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to install CW 6.3 in my computer that is running in Vista.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;During the installation, an error occur:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error 1305:&lt;/P&gt;&lt;P&gt;It asks me to find a dll file called "ics08dll_ics08grz_v130.dll" and make sure I can access it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, this file in my folder is actually 0kB, so I cannot access it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know how to solve this problem? Where can I get this file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kwok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Dec 2010 11:22:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-6-3-Installation-Error/m-p/167125#M3095</guid>
      <dc:creator>Kwok</dc:creator>
      <dc:date>2010-12-05T11:22:44Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior 6.3 Installation Error</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-6-3-Installation-Error/m-p/167126#M3096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you check the VISTA limitation in Welcome_CW_MCUs.txt?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;WINDOWS VISTA SPECIFIC LIMITATIONS:&lt;BR /&gt;-----------------------------------&lt;/P&gt;&lt;P&gt;The following limitations are applicable only if you are installing the product on Windows Vista:&lt;/P&gt;&lt;P&gt;(1) During installation, security messages may pop up concerning drivers being installed. It is highly&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; recommended to click on the option "continue anyway..", so the drivers can be installed.&lt;/P&gt;&lt;P&gt;(2) When opening the Codewarrior components (IDE, Debugger etc.) Firewall warnings may appear&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; with the option to block or unblock the application. It is advisable to click on the unblock option to&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; continue.&lt;/P&gt;&lt;P&gt;(3) For more VISTA specific limitations after the installation, please refer to:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "{INSTALLATION DIRECTORY}\Release_Notes\HC08\Notes_CW_MCUs_V6 3_Vista.txt"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;GENERAL LIMITATIONS:&lt;BR /&gt;--------------------&lt;/P&gt;&lt;P&gt;The following limitations are applicable to Windows Vista, Windows XP:&lt;/P&gt;&lt;P&gt;(1) It is highly recommended to have at least 400 MB of free space on the Windows system disk.&lt;BR /&gt;(2) Product supports 32-bit versions of Windows XP, Windows Vista.&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Dec 2010 21:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-6-3-Installation-Error/m-p/167126#M3096</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-12-06T21:48:06Z</dc:date>
    </item>
  </channel>
</rss>