<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: Windows 7 Unhandled Exception</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165201#M2975</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Codewarrior 6.2.1 (fully patched) for Microcontrollers (RS08 specifically).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a good machine, and I'd hate to waste a lot of RAM having to run Vista 32-bit. So far I've tried Vista 64-bit and Windows 7, neither of which will alllow CodeWarrior to run. Might look at trying to run a 32-bit Windows on 64-bit Windows just for CodeWarrior - sad that I have to do that. The only common changes for both have to do with the absence of the 16-bit layer, no support for 32-bit drivers, strict kernel protection&amp;nbsp;and enforced driver signing. Not sure which/where would be causing the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Mar 2009 21:01:44 GMT</pubDate>
    <dc:creator>nonarKitten</dc:creator>
    <dc:date>2009-03-23T21:01:44Z</dc:date>
    <item>
      <title>Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165199#M2973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When starting the IDE in Windows 7, the proram will work fine until a project is loaded at which point it will report an error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CodeWarrior encountered an unhandled exception 0xc0000005 at address {different each time} (The memory at address {different random address} could not be read)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Location: IDE.EXE:{same as the first random address}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Crash dump written to MEM_FREE.b2830.20090320.122156A.dump&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Choose 'Abort' to end the program, 'Retry' to debug, or 'Ignore' to continue (at your own risk!)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Abort will kill it, Retry will cause it to be unresponsive, and Ignore just brings the same error back up a few times until I get this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Generic Error 32770. An unknown error has occured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Neither running as Administrator nor taking ownership of the Program Files folder seems to help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Mar 2009 01:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165199#M2973</guid>
      <dc:creator>nonarKitten</dc:creator>
      <dc:date>2009-03-21T01:27:22Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165200#M2974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Which CPU are you targeting (HC08, HC12, Coldfire, ..)&lt;BR /&gt;- Which version of CodeWarrior are you using?&lt;BR /&gt;To retrieve that info:&lt;BR /&gt;- Start CodeWarrior&lt;BR /&gt;- Select Help -&amp;gt; About Freescale CodeWarrior&lt;BR /&gt;- Click on "Install Products"&lt;BR /&gt;- CodeWarrior version used is displayed on top in the Installed Products dialog.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2009 16:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165200#M2974</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-03-23T16:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165201#M2975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Codewarrior 6.2.1 (fully patched) for Microcontrollers (RS08 specifically).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a good machine, and I'd hate to waste a lot of RAM having to run Vista 32-bit. So far I've tried Vista 64-bit and Windows 7, neither of which will alllow CodeWarrior to run. Might look at trying to run a 32-bit Windows on 64-bit Windows just for CodeWarrior - sad that I have to do that. The only common changes for both have to do with the absence of the 16-bit layer, no support for 32-bit drivers, strict kernel protection&amp;nbsp;and enforced driver signing. Not sure which/where would be causing the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2009 21:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165201#M2975</guid>
      <dc:creator>nonarKitten</dc:creator>
      <dc:date>2009-03-23T21:01:44Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165202#M2976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This looks to be related to either your project r our installation.&lt;/P&gt;&lt;P&gt;I would recommend you to submit a service request for that.&lt;BR /&gt;&lt;BR /&gt;Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR" rel="nofollow" target="_blank"&gt;here&lt;/A&gt; to submit a service request.&lt;BR /&gt;&lt;BR /&gt;Make sure to attach a reproducible project and installed product information to the service request.&lt;BR /&gt;To generate the required information:&lt;BR /&gt;- Start CodeWarrior&lt;BR /&gt;- Open the project&lt;BR /&gt;- Select "Help" -&amp;gt; "Pack and Go" and follow instructions on the screen.&lt;BR /&gt;&lt;BR /&gt;Attach the generated .zip file to the SR.&lt;/P&gt;&lt;P&gt;Also attach the crash dump file (MEM_FREE.b2830.20090320.122156A.dump)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2009 16:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165202#M2976</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-03-25T16:56:53Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165203#M2977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello, I am having the exact same problem with CW v6.3 and Windows 7 x86. Have you found any solution?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2010 06:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165203#M2977</guid>
      <dc:creator>jajomafa</dc:creator>
      <dc:date>2010-01-21T06:45:13Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165204#M2978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have the same problem. I was reading other forums about this problem but all recommendations, compatibilities, run as admin, etc.... but I still having the problem with CW 6.2 and 7.1... anybody with ideas?...&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jan 2010 04:36:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165204#M2978</guid>
      <dc:creator>plugas</dc:creator>
      <dc:date>2010-01-23T04:36:59Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165205#M2979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Add me to the list.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 32-bit Windows 7&lt;/P&gt;&lt;P&gt;&amp;nbsp; CW 5.9&lt;/P&gt;&lt;P&gt;&amp;nbsp; MC9S processor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2010 21:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165205#M2979</guid>
      <dc:creator>Audi</dc:creator>
      <dc:date>2010-01-26T21:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165206#M2980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;service request submitted&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2010 23:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165206#M2980</guid>
      <dc:creator>jajomafa</dc:creator>
      <dc:date>2010-01-26T23:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165207#M2981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Possible work-around #1&amp;nbsp;- uninstall everything CodeWarrior related. Go to your user folder (e.g., C:\Users\MyUserName\) and create a folder called Apps. Then reinstall and when you're given the choice of where to install, select the Apps folder you created (e.g., C:\Users\MyUserName\Apps). It seems MOST of the problems are caused by Windows' new security on the Program Files folder(s).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note - still unresolved issues include: CodeWarrior crashing if you attempt to move it to a second display (e.g., if you have more than one LCD hooked up), and programming via USB devices may be hit-or-miss. I've as of yet been unable to program via our SofTec unit. However, some&amp;nbsp;of these problems may be because I'm also running x64 edition of Windows 7, so your mileage may vary.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Possible work-around #2 - Install XP Mode. This raises its own issues, namely that the USB handling is really poor and you often have to reconnect the programmer until XP Mode "catches" the device. It also has many other limitations (e.g., it's slow, randomly disconnects local drives, won't work with dual displays, and isn't the reason you got Windows 7 anyway).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2010 23:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165207#M2981</guid>
      <dc:creator>nonarKitten</dc:creator>
      <dc:date>2010-01-26T23:50:54Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165208#M2982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found this work-around. . .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Again, I am using 32-bit Win7 Pro.&amp;nbsp; I run CW with the "Disble desktop composition" enabled (checked).&amp;nbsp; You can find that option on the Compatability tab of CW's Properties dialog.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2010 00:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165208#M2982</guid>
      <dc:creator>Audi</dc:creator>
      <dc:date>2010-01-27T00:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165209#M2983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;thank you Nonar and Audi for those "work-around". I tried Audi's and worked fine ... Thank you very much&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2010 05:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165209#M2983</guid>
      <dc:creator>jajomafa</dc:creator>
      <dc:date>2010-01-27T05:28:25Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165210#M2984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Audi:You are a hero!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Freescale: Pull your pants up...&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Feb 2010 22:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165210#M2984</guid>
      <dc:creator>looxonline</dc:creator>
      <dc:date>2010-02-13T22:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165211#M2985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also meet this problem. I think your graphic card is nvidia series and the driver is the latest one. With the same, I am using a notebook with the graphic card of Quadro NVS160M, when I install the old driver(179.**), everything works well. But when I install the latest drivers ( For example, 18*.** or 19*.**), codewarrior will have some unlandled exceptions. It seams that some dll file is not compatible with the new graphic driver!&lt;/P&gt;&lt;P&gt;Hope freescale solve this problem early!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2010 13:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165211#M2985</guid>
      <dc:creator>onemoretouch</dc:creator>
      <dc:date>2010-02-23T13:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165212#M2986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;U&gt;Thanks Audi, it work fine&lt;/U&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2010 12:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165212#M2986</guid>
      <dc:creator>Teto</dc:creator>
      <dc:date>2010-02-24T12:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165213#M2987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another option that works is to "Run As Administrator".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Apr 2010 07:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165213#M2987</guid>
      <dc:creator>nallyn</dc:creator>
      <dc:date>2010-04-02T07:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165214#M2988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Audi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I run the CW as an Administrator But still getting the unhandled Exception error.&lt;/P&gt;&lt;P&gt;Please tell where I can find this Desktop compatibility option in the CW.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Randhawa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Jul 2010 07:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165214#M2988</guid>
      <dc:creator>Randhawa</dc:creator>
      <dc:date>2010-07-10T07:22:09Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165215#M2989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using 32-bit Win7 Pro, right-click on the CW short-cut in your Start menu.&amp;nbsp; Select properties.&amp;nbsp; Select the Compatability tab.&amp;nbsp; Check the "Disble desktop composition" option.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jul 2010 23:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165215#M2989</guid>
      <dc:creator>Audi</dc:creator>
      <dc:date>2010-07-12T23:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165216#M2990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Audi's right!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Aug 2010 19:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165216#M2990</guid>
      <dc:creator>MPCMpy</dc:creator>
      <dc:date>2010-08-23T19:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165217#M2991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;@Audi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the hint, that solved the persistens crashes with Codewarrior 2.7 for MPC 56xx under Windows 7 x64, too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Oct 2010 00:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165217#M2991</guid>
      <dc:creator>MoveX</dc:creator>
      <dc:date>2010-10-07T00:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 Unhandled Exception</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165218#M2992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I thought CW5.1 for S12(X) should work natively on Win7. I tried it on Win7 PRO x86&amp;nbsp; and got the same annoying Unhandled Exception.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks Audi for solution!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Dec 2010 17:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-Unhandled-Exception/m-p/165218#M2992</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-01T17:02:19Z</dc:date>
    </item>
  </channel>
</rss>