<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックCodeWarrior not working with other Companies Software</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-not-working-with-other-Companies-Software/m-p/162454#M2784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been fighting to get CodeWarrior for DSC`s to work for a little more than a week with no luck.&amp;nbsp; I have been unsuccessful in get my Windows XP machine - service pack 3, to recognize the USB TAP device I have.&amp;nbsp; It will recognize the device after a Windows reset with the utap plugged into the USB port.&amp;nbsp; I did an installation of the software on my Vista notebook and it was recognized and CCS also opened a connection for the utap and worked as expected with the MC56F8013 Demo.&amp;nbsp; This indicates to me that there is nothing wrong with the utap.&lt;/P&gt;&lt;P&gt;The Windows box&amp;nbsp;must have a conflict with some of the other installed software.&amp;nbsp; This XP machine has Orcad 15.7, ONET 14.5, Visual Studio 2005, Microsoft SQL Server 2005 as well as CodeWarrior.&amp;nbsp; My Vista notebook has none of this software installed.&lt;/P&gt;&lt;P&gt;Have you seen anything like this before, if not do you have any troubleshooting ideas?&lt;/P&gt;&lt;P&gt;Should there be a Jungo device in the device manager? There is one on my Vista machine but not on the XP box.&lt;/P&gt;&lt;P&gt;Under System Devices in the device manager there is an appearance for CodeWarrior&amp;nbsp;USB TAP as well as XP after reset recognition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for Any help you can give&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 27 Aug 2011 03:24:42 GMT</pubDate>
    <dc:creator>Confuseduser</dc:creator>
    <dc:date>2011-08-27T03:24:42Z</dc:date>
    <item>
      <title>CodeWarrior not working with other Companies Software</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-not-working-with-other-Companies-Software/m-p/162454#M2784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been fighting to get CodeWarrior for DSC`s to work for a little more than a week with no luck.&amp;nbsp; I have been unsuccessful in get my Windows XP machine - service pack 3, to recognize the USB TAP device I have.&amp;nbsp; It will recognize the device after a Windows reset with the utap plugged into the USB port.&amp;nbsp; I did an installation of the software on my Vista notebook and it was recognized and CCS also opened a connection for the utap and worked as expected with the MC56F8013 Demo.&amp;nbsp; This indicates to me that there is nothing wrong with the utap.&lt;/P&gt;&lt;P&gt;The Windows box&amp;nbsp;must have a conflict with some of the other installed software.&amp;nbsp; This XP machine has Orcad 15.7, ONET 14.5, Visual Studio 2005, Microsoft SQL Server 2005 as well as CodeWarrior.&amp;nbsp; My Vista notebook has none of this software installed.&lt;/P&gt;&lt;P&gt;Have you seen anything like this before, if not do you have any troubleshooting ideas?&lt;/P&gt;&lt;P&gt;Should there be a Jungo device in the device manager? There is one on my Vista machine but not on the XP box.&lt;/P&gt;&lt;P&gt;Under System Devices in the device manager there is an appearance for CodeWarrior&amp;nbsp;USB TAP as well as XP after reset recognition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for Any help you can give&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Aug 2011 03:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-not-working-with-other-Companies-Software/m-p/162454#M2784</guid>
      <dc:creator>Confuseduser</dc:creator>
      <dc:date>2011-08-27T03:24:42Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior not working with other Companies Software</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-not-working-with-other-Companies-Software/m-p/162455#M2785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, there should be a Jungo driver present. Are you using a P&amp;amp;E Microsystems USB TAP?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Try the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) If there is any sort of USB TAP deriver visible in the Device Manager window, remove it.&lt;/P&gt;&lt;P&gt;2) Unplug the USB TAP.&lt;/P&gt;&lt;P&gt;3) Download the latest P&amp;amp;E Microsystems drivers for the USB TAP from &lt;A href="http://www.pemicro.com." rel="nofollow" target="_blank"&gt;www.pemicro.com.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;4) Install the driver package. You might have to restart.&lt;/P&gt;&lt;P&gt;5) Now plug in the USB TAP and you should get a "new USB hardware detected" message, and then the Windows Device Manager Wizard appears.&lt;/P&gt;&lt;P&gt;6) Let the Wizard install the driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hopefully that will enable CodeWarrior to interface with the TAP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2011 00:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/CodeWarrior-not-working-with-other-Companies-Software/m-p/162455#M2785</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-08-30T00:50:54Z</dc:date>
    </item>
  </channel>
</rss>