<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Re: error message &amp;quot;CCSProtocalPlugin: CCS: Cable disconnected &amp;quot;, help!!</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159729#M2621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Windows doesn't manage anymore the parallel port.&lt;/DIV&gt;&lt;DIV&gt;Since NT we meet problem with all interfaces using the host parallel port.&lt;/DIV&gt;&lt;DIV&gt;To avoid that we introduced an usb interface: USBTap.&lt;/DIV&gt;&lt;DIV&gt;We recommend to use this interface to avoid this case of situation.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;See below some other tips for parallel issues.&lt;/DIV&gt;&lt;DIV&gt;Hope this will help you.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV align="left"&gt;&lt;SPAN class="438311209-09062006"&gt;&lt;FONT color="#0000ff" face="Arial" size="2"&gt;Restart the computer with the parallel cable disconnected&amp;nbsp;from the computer completely. After the system reboot is complete,&amp;nbsp;use the parallel cable to reconnect the equipment.&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV align="left"&gt;&lt;SPAN class="438311209-09062006"&gt;&lt;FONT color="#0000ff" size="2"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV align="left"&gt;&lt;SPAN class="438311209-09062006"&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;P&gt;&lt;FONT size="2"&gt;Just in case anyone else has similar problems, it turns out that the inbuilt parallel "command converter: on the DSP56858EVM (and my own cable based on that design) were the problem. The DSP56858EVM has only a 3.3V buffer on the lines going to the PC. While this does might meet the specs for VIHmin on the original PC's input buffers, it seems to be OK on some PC's today but not on others. There must also be some difference between the timing of the CCS in version 7.0 and version 7.2, because the former worked and the latter didn't.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Making a new parallel command converter cable using Motorola's schematic, which includes a 5V buffer as well as the 3.3V one fixed the problem. I would have bought one for AU$250, but couldn't afford the 6 week delivery time.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/P&gt;Pascal&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Dec 2007 18:34:59 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2007-12-17T18:34:59Z</dc:date>
    <item>
      <title>error message "CCSProtocalPlugin: CCS: Cable disconnected ", help!!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159725#M2617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi everybody:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have a problem with JTAG interface plugged into parallel port to PC (from demo board 56F8013),&lt;/DIV&gt;&lt;DIV&gt;before it worked fine, until now it always gives me an error message "CCSProtocalPlugin: CCS: Cable disconnected&amp;nbsp;", I checked everything is connectted as fine as before, and the strange thing is: when everything worked before, I cliked the "make" button, it showed a warning, which is fine (still can be downloaded to the demoboard), while but now, when I clicked the "make" button, it shows me nothing, why?&lt;/DIV&gt;&lt;DIV&gt;and I also want to know for sure if it is the problem with the JATG interface,&amp;nbsp;or with&amp;nbsp;the 56F8013 chip itself?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Many thanks!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Oct 2007 23:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159725#M2617</guid>
      <dc:creator>duck</dc:creator>
      <dc:date>2007-10-30T23:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: error message "CCSProtocalPlugin: CCS: Cable disconnected ", help!!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159726#M2618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I had the same problem. Try it with a demo program. Upload the Demo program into the demoboard. I'm sure it will work. After that you can upload your program and continue with your program.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2007 20:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159726#M2618</guid>
      <dc:creator>Diplomand</dc:creator>
      <dc:date>2007-11-06T20:40:16Z</dc:date>
    </item>
    <item>
      <title>Re: error message "CCSProtocalPlugin: CCS: Cable disconnected ", help!!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159727#M2619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you still meet some problem about your connection.&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;We experienced several problem when the parallel on host was used with a sample parallel cable or via the wiggler interface.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;To avoid them an USBTap can be used.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;For details, please have a look to our web site:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CWH-UTP-ONCE-HX" rel="nofollow" target="_blank"&gt;&lt;U&gt;&lt;FONT color="#0000ff" size="2"&gt;&lt;/FONT&gt;&lt;/U&gt;&lt;/A&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CWH-UTP-ONCE-HX" target="test_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CWH-UTP-ONCE-HX&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;FONT size="2"&gt;Some customer meets a problem similar to your issue due to the voltage of the Parallel port.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;FONT size="2"&gt;See below details:&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;FONT size="2"&gt;Customer engineers examined the parallel port and found that the voltage supplied to the wiggler through the parallel port was about 1v. At least 3v must be supplied to the wiggler for proper operation.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;FONT size="2"&gt;Several users meet the same problem.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;FONT size="2"&gt;Can you please check it on your side ?&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;See below some tips fixing XP problems.&lt;/FONT&gt;&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; (A) In windows XP/2000, the parallel port dialog checkbox entitled&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; "Enable Legacy Plug and Play" should be checked. This setting is located&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; in the Control Panel--&amp;gt;System--&amp;gt;Hardware-&amp;gt;Device Manager-&amp;gt;Ports-&amp;gt;Printer&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; Port (LPTX) dialog.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; (B) Here are the steps to modify the parallel port registry key&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; appropriately:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; 1. save the winxp1.reg file to your hard drive&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; 2. make sure you are logged in as the system administrator&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; 3. run the winxp1.reg file (by double clicking on it)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; 4. A question will be displayed "Are you sure you want to add the&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; information in c:\winxp1.reg to the registry?"&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; 5. Click the Yes button&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; 6. A message will display "Information in c:\winxp1.reg has been&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; successfully entered into the registry."&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;gt; 7. restart your computer to apply the new changes&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Try the following steps in the CCS Console window:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;1. ‘show wdv’ à"WinDriver V5.05b Jungo (c)2002 Build Date: Aug 4 2002 X86 SYS"&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;2. Start à Settings à Control Panel à System à Hardware à Device Manager&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Ports à Printer Port(LPT1) double click on this and on the window go to the Resources tab.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Look at the I/O Range. The first I/O range is the address of the parallel port.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;3. delete all&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;config cc parallel:0x0378&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;After doing this you should connect to the board without any problems.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;This error was appearing when a customer would try to connect to the debugger.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Pascal&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2007 17:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159727#M2619</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2007-11-09T17:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: error message "CCSProtocalPlugin: CCS: Cable disconnected ", help!!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159728#M2620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I ran into a similar problem and tried this solution you propose here. It makes absolutely no difference - there are still connection problems wiht 95% of the connections, each time spurting out a different error message (":can't read registers" , "cable unconnected", "core not responding" etc.)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Dec 2007 23:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159728#M2620</guid>
      <dc:creator>eliben</dc:creator>
      <dc:date>2007-12-16T23:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: error message "CCSProtocalPlugin: CCS: Cable disconnected ", help!!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159729#M2621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Windows doesn't manage anymore the parallel port.&lt;/DIV&gt;&lt;DIV&gt;Since NT we meet problem with all interfaces using the host parallel port.&lt;/DIV&gt;&lt;DIV&gt;To avoid that we introduced an usb interface: USBTap.&lt;/DIV&gt;&lt;DIV&gt;We recommend to use this interface to avoid this case of situation.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;See below some other tips for parallel issues.&lt;/DIV&gt;&lt;DIV&gt;Hope this will help you.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV align="left"&gt;&lt;SPAN class="438311209-09062006"&gt;&lt;FONT color="#0000ff" face="Arial" size="2"&gt;Restart the computer with the parallel cable disconnected&amp;nbsp;from the computer completely. After the system reboot is complete,&amp;nbsp;use the parallel cable to reconnect the equipment.&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV align="left"&gt;&lt;SPAN class="438311209-09062006"&gt;&lt;FONT color="#0000ff" size="2"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV align="left"&gt;&lt;SPAN class="438311209-09062006"&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;P&gt;&lt;FONT size="2"&gt;Just in case anyone else has similar problems, it turns out that the inbuilt parallel "command converter: on the DSP56858EVM (and my own cable based on that design) were the problem. The DSP56858EVM has only a 3.3V buffer on the lines going to the PC. While this does might meet the specs for VIHmin on the original PC's input buffers, it seems to be OK on some PC's today but not on others. There must also be some difference between the timing of the CCS in version 7.0 and version 7.2, because the former worked and the latter didn't.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Making a new parallel command converter cable using Motorola's schematic, which includes a 5V buffer as well as the 3.3V one fixed the problem. I would have bought one for AU$250, but couldn't afford the 6 week delivery time.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/P&gt;Pascal&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Dec 2007 18:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/error-message-quot-CCSProtocalPlugin-CCS-Cable-disconnected-quot/m-p/159729#M2621</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2007-12-17T18:34:59Z</dc:date>
    </item>
  </channel>
</rss>