<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Deadstripping in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159639#M2615</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you both, eGuy and stanish!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm really looking for a global handling - running an RTOS that indirectly uses lots of unlabeled pointers. Manually linking with a postpended '+' on each obj works fine, and I was hoping there's a way I didn't see to do that.&amp;nbsp; I guess maybe a linker.bat to add the '+' might have to be it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I appreciate it!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Dec 2009 02:06:00 GMT</pubDate>
    <dc:creator>asmjockey</dc:creator>
    <dc:date>2009-12-08T02:06:00Z</dc:date>
    <item>
      <title>Deadstripping</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159634#M2610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've not found a way to turn off deadstripping within the IDE.&amp;nbsp; Is there a way to do this without linking at the command line? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Dec 2009 03:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159634#M2610</guid>
      <dc:creator>asmjockey</dc:creator>
      <dc:date>2009-12-05T03:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: Deadstripping</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159635#M2611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From Target Setting Panels -&amp;gt; ColdFire Linker -&amp;gt; Select "Disable Deadstripping"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;J&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Dec 2009 04:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159635#M2611</guid>
      <dc:creator>eGuy</dc:creator>
      <dc:date>2009-12-05T04:16:34Z</dc:date>
    </item>
    <item>
      <title>Re: Deadstripping</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159636#M2612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, being explicit might be helpful, huh?&amp;nbsp; I'm using the HCS12 (ver 5) and the 56800E.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Dec 2009 04:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159636#M2612</guid>
      <dc:creator>asmjockey</dc:creator>
      <dc:date>2009-12-05T04:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: Deadstripping</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159637#M2613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for CW for HCS12: &amp;nbsp;you can add the objects that you don't want to optimize into the ENTRIES section of your .prm file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&amp;amp;message.id=3900&amp;amp;query.id=97484#M3900" target="_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&amp;amp;message.id=3900&amp;amp;query.id=97484#M3900&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stanish&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Dec 2009 17:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159637#M2613</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2009-12-07T17:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: Deadstripping</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159638#M2614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can also try this: ( I used it on my 52259 project)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#pragma force_active on&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//&amp;nbsp; put the code you wish to keep ( not optimized away) here&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#pragma force_active off&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Dec 2009 21:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159638#M2614</guid>
      <dc:creator>eGuy</dc:creator>
      <dc:date>2009-12-07T21:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: Deadstripping</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159639#M2615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you both, eGuy and stanish!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm really looking for a global handling - running an RTOS that indirectly uses lots of unlabeled pointers. Manually linking with a postpended '+' on each obj works fine, and I was hoping there's a way I didn't see to do that.&amp;nbsp; I guess maybe a linker.bat to add the '+' might have to be it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I appreciate it!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2009 02:06:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159639#M2615</guid>
      <dc:creator>asmjockey</dc:creator>
      <dc:date>2009-12-08T02:06:00Z</dc:date>
    </item>
    <item>
      <title>Re: Deadstripping</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159640#M2616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Notation to use is different for DSP56800E and for HC12.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For HC12 if you want to disable dead striping for a module called myfile.c, use following notation in your application .prm file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ENTRIES&lt;BR /&gt;&amp;nbsp; myfile.c.o:*&lt;BR /&gt;END&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can enumerate several files in the ENTRIES block.&amp;nbsp;Just use&amp;nbsp;space character as separator.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For DSP58000E, you can disable dead striping for a specific section using linker command KEEP_SECTION.&lt;/P&gt;&lt;P&gt;You just have to place whole code from that module in a user defined section and disable dead striping for that section.&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2009 00:11:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Deadstripping/m-p/159640#M2616</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-12-09T00:11:14Z</dc:date>
    </item>
  </channel>
</rss>