<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Unpredictable output while working with numeric user input in C</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159204#M2571</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure if this is your issue, but the printf shown prints the address of the variable, not the value.&lt;/P&gt;&lt;P&gt;Should be&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; printf("The number entered by the user is : %d", user_ans);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also decimal &lt;SPAN class="Apple-style-span"&gt;536935188 &lt;SPAN class="Apple-style-span"&gt;is in hex 0x2000FB14, looks like a regular address. Is the stack in this area?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Dec 2009 11:59:23 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2009-12-04T11:59:23Z</dc:date>
    <item>
      <title>Unpredictable output while working with numeric user input in C</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159201#M2568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am new to the CodeWarrior IDE and trying to get familiar with the IDE by writing simple C programs.&lt;/P&gt;&lt;P&gt;The board I am using is MCF5234BCCKIT eval board and the version of CodeWarrior is the special freely downloadable version 7.1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried writing very simple code with scanf() and fgets() type of functions to get user input and do some arithmetic operations on them. The target is console internal RAM. The output of the program is usually large numbers which could possibly be garbage values or&amp;nbsp;addresses. for example, if a value of 20 in entered in a scanf() and assigned to a varibale, and I try printing the variable value to the console with a printf() is shows up as something like 536935188. Also, within the code if the value id incremented by say, 1, I see the output as 1 added to this large value.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I doing wrong? &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2009 03:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159201#M2568</guid>
      <dc:creator>net11</dc:creator>
      <dc:date>2009-12-03T03:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: Unpredictable output while working with numeric user input in C</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159202#M2569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear net11,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Please post a simple example of the code you are having a problem with.&amp;nbsp; It's a bit hard to know if its a setup or code problem otherwise &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2009 08:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159202#M2569</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-12-03T08:59:53Z</dc:date>
    </item>
    <item>
      <title>Re: Unpredictable output while working with numeric user input in C</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159203#M2570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for taking a look at my post... I will try to be more specific this time. The major problem I am facing is that I am not able to use printf() statements to correctly print the value of a variable or scanf() to get user input for the value. For example, in the code :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int main(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int correct_ans = 53;&lt;/P&gt;&lt;P&gt;int user_ans;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;printf("Enter an integer between 1 and 100 as guess :");&lt;/P&gt;&lt;P&gt;scanf("%d", &amp;amp;user_ans);&lt;/P&gt;&lt;P&gt;printf("The number entered by the user is : %d", &amp;amp;user_ans);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if(user_ans == correct_ans)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;printf("Correct!");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;printf("Wrong!");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;return 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The value of the variable user_ans shows some large value(&lt;SPAN class="Apple-style-span"&gt;536935188&lt;SPAN class="Apple-style-span"&gt;) at every step of the code execution in the debugger's "register values" pane. The same value is printed to the console when the printf() is executed. However, if this code is modified to hard-code the variable values like&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int main(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int correct_ans = 53;&lt;/P&gt;&lt;P&gt;int user_ans = 53;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if(user_ans == correct_ans)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;printf("Correct!");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;printf("Wrong!");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;return 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;it works, and at every step, the variable values(53) shown are as expected. I suppose then, that there is a problem with the way printf() and scanf() are working ? If so, I am not sure how to read and write register values to the console correctly...&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2009 09:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159203#M2570</guid>
      <dc:creator>net11</dc:creator>
      <dc:date>2009-12-04T09:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: Unpredictable output while working with numeric user input in C</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159204#M2571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure if this is your issue, but the printf shown prints the address of the variable, not the value.&lt;/P&gt;&lt;P&gt;Should be&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; printf("The number entered by the user is : %d", user_ans);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also decimal &lt;SPAN class="Apple-style-span"&gt;536935188 &lt;SPAN class="Apple-style-span"&gt;is in hex 0x2000FB14, looks like a regular address. Is the stack in this area?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2009 11:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159204#M2571</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2009-12-04T11:59:23Z</dc:date>
    </item>
    <item>
      <title>Re: Unpredictable output while working with numeric user input in C</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159205#M2572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Daniel, my bad for an error like that. That was not the issue here though, when I fixed and ran the code. Apparently not flushing the buffer between the printf and scanf statements caused the problems. I fixed it though....&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the stack is in this area btw.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;CompilerGuru wrote:&lt;BR /&gt;&lt;P&gt;Not sure if this is your issue, but the printf shown prints the address of the variable, not the value.&lt;/P&gt;&lt;P&gt;Should be&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; printf("The number entered by the user is : %d", user_ans);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also decimal &lt;SPAN&gt;536935188 &lt;SPAN&gt;is in hex 0x2000FB14, looks like a regular address. Is the stack in this area?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 May 2010 07:59:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Unpredictable-output-while-working-with-numeric-user-input-in-C/m-p/159205#M2572</guid>
      <dc:creator>net11</dc:creator>
      <dc:date>2010-05-16T07:59:27Z</dc:date>
    </item>
  </channel>
</rss>