<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: USB Tap on Windows 7</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156685#M2419</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is an application note, AN4338, which provides an updated CCS build. Use AN4338 and the Enter Keyword search to locate it. That build was for the Classic (non-Eclipse) CodeWarrior IDE, though. Is this the same build?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Dec 2011 22:15:35 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2011-12-20T22:15:35Z</dc:date>
    <item>
      <title>USB Tap on Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156680#M2414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone gotten a USB Tap to work with Windows 7?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My current workaround is to install the XP virtual machine, and then&amp;nbsp;install Codwarrior within the virtual OS. However, I was having an issue with programming speed (the download was taking up to 3 minutes). I tried to install the Jungo driver that comes with CodeWarrior, and now all I get is "CCS: USB Open Failed" when I attempt to flash the chip (16 bit MCF8322 via JTAG).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I could just work from within Windows 7, it would save a lot of headache. If there's not any support for the USB Tap, what programmers do work with CodeWarrior on a 64 bit machine?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2011 20:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156680#M2414</guid>
      <dc:creator>azguard</dc:creator>
      <dc:date>2011-08-05T20:51:18Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tap on Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156681#M2415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got past my virtual machine issues, so I'm back to a working workaround. I would still like to know what everyone is using to program these chips from Windows 7 if the USB tap is not going to be supported. Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2011 21:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156681#M2415</guid>
      <dc:creator>azguard</dc:creator>
      <dc:date>2011-08-05T21:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tap on Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156682#M2416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same problem: I can't use the USB Tap to program an MC56F8025 with my new 64bit Win7 notebook.&lt;/P&gt;&lt;P&gt;The USB Tap connects to the processor, blanks the flash, but then writes:&lt;/P&gt;&lt;P&gt;"CCCSClient::WriteMemoryDirect: Core not responding"&lt;/P&gt;&lt;P&gt;Has anybody found a solution?&lt;/P&gt;&lt;P&gt;BTW, on the Virtual XP machine the USB Tap does work, but it's not an attractive environment...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Nov 2011 22:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156682#M2416</guid>
      <dc:creator>8_Floppy</dc:creator>
      <dc:date>2011-11-08T22:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tap on Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156683#M2417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you looked at this &lt;A __default_attr="57404" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/57404" jivemacro="thread" title="forum thread"&gt;forum thread&lt;/A&gt;?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Nov 2011 21:19:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156683#M2417</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-11-09T21:19:21Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tap on Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156684#M2418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I finally SOLVED the problem: I just obtained from Freescale a new build of the "ccs" directory (for CodeWarrior or FlashProgramming).&lt;/P&gt;&lt;P&gt;I just replaced the old "ccs" directory with the new one, and now the USB Tap is working fine even under Windows 7.&lt;/P&gt;&lt;P&gt;Hope it can help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 21:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156684#M2418</guid>
      <dc:creator>8_Floppy</dc:creator>
      <dc:date>2011-12-20T21:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tap on Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156685#M2419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is an application note, AN4338, which provides an updated CCS build. Use AN4338 and the Enter Keyword search to locate it. That build was for the Classic (non-Eclipse) CodeWarrior IDE, though. Is this the same build?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 22:15:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156685#M2419</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-12-20T22:15:35Z</dc:date>
    </item>
    <item>
      <title>Re: USB Tap on Windows 7</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156686#M2420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No it's not the same.&lt;/P&gt;&lt;P&gt;I already tried the "ccs" inside AN4338SW.zip: with it the USB Tap installed correctly on win7, but using it I had the error as in my previous post.&lt;/P&gt;&lt;P&gt;The new "ccs" seems really new, I received it today ("ccs_bld000_win.zip").&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Dec 2011 01:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/USB-Tap-on-Windows-7/m-p/156686#M2420</guid>
      <dc:creator>8_Floppy</dc:creator>
      <dc:date>2011-12-21T01:06:39Z</dc:date>
    </item>
  </channel>
</rss>