<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Windows 7 problem - cwide.exe has stopped working - in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-problem-cwide-exe-has-stopped-working/m-p/155828#M2387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe that DE.exe is the CodeWarrior debugger engine being activated when you run or debug a project. That is normal behavior. You need to file an on-line service request to report this problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Aug 2011 19:50:57 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2011-08-03T19:50:57Z</dc:date>
    <item>
      <title>Windows 7 problem - cwide.exe has stopped working -</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-problem-cwide-exe-has-stopped-working/m-p/155827#M2386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since I moved to Windows 7 I receive an error almost everytime I close CodeWarrior IDE v10.1. I use CodeWarrior to create bareboard projects for the HCS08QE family devices, and this is the error I get:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;A href="http://img232.imageshack.us/img232/3061/errorcw2.jpg"&gt;&lt;IMG border="0" src="http://img232.imageshack.us/img232/3061/errorcw2.jpg" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've investigated a bit and it seems the error is thrown if I run or debug an application. If I open CodeWarrior and do not run or debug any project, I can close CW without any error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Going further, when running or debugging a project, I noticed a new process called &lt;STRONG&gt;DE.exe&lt;/STRONG&gt; is launched by CodeWarrior, see it selected in the following image:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://img641.imageshack.us/img641/7435/errorcw1.jpg"&gt;&lt;IMG border="0" src="http://img641.imageshack.us/img641/7435/errorcw1.jpg" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That process is initialized when transferring the project to the CPU, but it is not closed when finished. So, I think the error I receive when closing CW can be caused because that process is still alive or something. As I said, if that process is not initialized I can close CW without errors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anyone seen the same behavior? Is there any possible fix? It is a bit annoying receiving that error anytime I close CW...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2011 17:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-problem-cwide-exe-has-stopped-working/m-p/155827#M2386</guid>
      <dc:creator>DiegoE</dc:creator>
      <dc:date>2011-08-02T17:35:46Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 problem - cwide.exe has stopped working -</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-problem-cwide-exe-has-stopped-working/m-p/155828#M2387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe that DE.exe is the CodeWarrior debugger engine being activated when you run or debug a project. That is normal behavior. You need to file an on-line service request to report this problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Aug 2011 19:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Windows-7-problem-cwide-exe-has-stopped-working/m-p/155828#M2387</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2011-08-03T19:50:57Z</dc:date>
    </item>
  </channel>
</rss>