<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックMPC8313E Debuger in ROM</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8313E-Debuger-in-ROM/m-p/155807#M2383</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have a MPC8313ERDB and USBTAP,i want to debug the project wizard made in ROM VERSION mode,but&amp;nbsp;the README say&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif"&gt;&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&lt;/A&gt;nce the image is in ROM, you can debug it with the ROM Version&lt;BR /&gt;target. but,i download the .elf file to&amp;nbsp;which addr? 0xFFF00000? the&amp;nbsp;xor flash has 8MB Memory,and RCW write to 0xFE000000,there have many range ,it can't work in my board.who can give me a particular way to debug the project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Nov 2009 17:17:32 GMT</pubDate>
    <dc:creator>kala</dc:creator>
    <dc:date>2009-11-20T17:17:32Z</dc:date>
    <item>
      <title>MPC8313E Debuger in ROM</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8313E-Debuger-in-ROM/m-p/155807#M2383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;I have a MPC8313ERDB and USBTAP,i want to debug the project wizard made in ROM VERSION mode,but&amp;nbsp;the README say&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif"&gt;&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&lt;/A&gt;nce the image is in ROM, you can debug it with the ROM Version&lt;BR /&gt;target. but,i download the .elf file to&amp;nbsp;which addr? 0xFFF00000? the&amp;nbsp;xor flash has 8MB Memory,and RCW write to 0xFE000000,there have many range ,it can't work in my board.who can give me a particular way to debug the project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2009 17:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8313E-Debuger-in-ROM/m-p/155807#M2383</guid>
      <dc:creator>kala</dc:creator>
      <dc:date>2009-11-20T17:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313E Debuger in ROM</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8313E-Debuger-in-ROM/m-p/155808#M2384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you have built the program using the CodeWarrior New Project wizard and chose the ROM build target, the proper addresses for download into non-volatile memory should be preset. If the processor supports hardware breakpoints, you can set set a few breakpoints in the firmware memory and the processor will trap on them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Nov 2009 22:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8313E-Debuger-in-ROM/m-p/155808#M2384</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-11-30T22:14:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313E Debuger in ROM</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8313E-Debuger-in-ROM/m-p/155809#M2385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can indeed debug the ROM VERSION of your project but the code must be programmed into flash memory first.&amp;nbsp; Use the CodeWarrior Flash Programmer to program your ROM.elf file into flash.&amp;nbsp; Refer to the CodeWarrior documentation for working with the Flash Programmer.&amp;nbsp; Then once you get your code into flash you should be able to debug the ROM VERSION of your project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Dec 2009 05:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/MPC8313E-Debuger-in-ROM/m-p/155809#M2385</guid>
      <dc:creator>ronco</dc:creator>
      <dc:date>2009-12-02T05:28:17Z</dc:date>
    </item>
  </channel>
</rss>