<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic symbol created in init_IRQ bean is undefined vector.obj in Classic/Legacy CodeWarrior</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/symbol-created-in-init-IRQ-bean-is-undefined-vector-obj/m-p/153999#M2289</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have created a new bean (Init_IRQ) for an external interrupt - in the bean properities under interrupts I create a name for the ISR which I call "ShutOff". When I compile the program I get an error "Symbol ShutOff in file ./Generated_Code\Vectors.obj is undefined".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can see ShutOff in the vector.c file&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; "ShutOff, /* Int.no.&amp;nbsp; 2 Virq (at FFFA)&amp;nbsp; Used */&lt;/P&gt;&lt;P&gt;I guess I need to define the ISR "ShutOff" somewhere else in the program - but where?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Apr 2012 22:43:26 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2012-04-12T22:43:26Z</dc:date>
    <item>
      <title>symbol created in init_IRQ bean is undefined vector.obj</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/symbol-created-in-init-IRQ-bean-is-undefined-vector-obj/m-p/153999#M2289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have created a new bean (Init_IRQ) for an external interrupt - in the bean properities under interrupts I create a name for the ISR which I call "ShutOff". When I compile the program I get an error "Symbol ShutOff in file ./Generated_Code\Vectors.obj is undefined".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can see ShutOff in the vector.c file&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; "ShutOff, /* Int.no.&amp;nbsp; 2 Virq (at FFFA)&amp;nbsp; Used */&lt;/P&gt;&lt;P&gt;I guess I need to define the ISR "ShutOff" somewhere else in the program - but where?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2012 22:43:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/symbol-created-in-init-IRQ-bean-is-undefined-vector-obj/m-p/153999#M2289</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-04-12T22:43:26Z</dc:date>
    </item>
    <item>
      <title>Re: symbol created in init_IRQ bean is undefined vector.obj</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/symbol-created-in-init-IRQ-bean-is-undefined-vector-obj/m-p/154000#M2290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You need to provide an implementation of interrupt function ShutOff in one of your application source file (.c).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Do not encode that in a file located in the Generated Code folder. Files within this folder may be overwritten by&lt;/P&gt;&lt;P&gt;&amp;nbsp; Processor Expert&amp;nbsp; later on.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2012 13:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/symbol-created-in-init-IRQ-bean-is-undefined-vector-obj/m-p/154000#M2290</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2012-04-13T13:58:55Z</dc:date>
    </item>
  </channel>
</rss>