<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 Arduino to HCS12 Serial input POrt output..!!!!!!!!</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Arduino-to-HCS12-Serial-input-POrt-output/m-p/153369#M2228</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can someone help me tranlate the following code I found for Arduino to HC12 language... I am pretty much trying receive information using the serial input on the microcontroller to read the information and then process the following information back to PORTB. the project consist of a GUI that sends information using the arrow pad on the keyboard and translate that to the controller 4 ports which is Port B which will send 3.3v to another chip which will control the direction of a robot. I have attached some sample codes that I want to use in a word document.. that can be reviewed.. Please help.. I have attached what we have so far...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 Jul 2011 05:39:22 GMT</pubDate>
    <dc:creator>Looney</dc:creator>
    <dc:date>2011-07-23T05:39:22Z</dc:date>
    <item>
      <title>Arduino to HCS12 Serial input POrt output..!!!!!!!!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Arduino-to-HCS12-Serial-input-POrt-output/m-p/153369#M2228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can someone help me tranlate the following code I found for Arduino to HC12 language... I am pretty much trying receive information using the serial input on the microcontroller to read the information and then process the following information back to PORTB. the project consist of a GUI that sends information using the arrow pad on the keyboard and translate that to the controller 4 ports which is Port B which will send 3.3v to another chip which will control the direction of a robot. I have attached some sample codes that I want to use in a word document.. that can be reviewed.. Please help.. I have attached what we have so far...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2011 05:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Arduino-to-HCS12-Serial-input-POrt-output/m-p/153369#M2228</guid>
      <dc:creator>Looney</dc:creator>
      <dc:date>2011-07-23T05:39:22Z</dc:date>
    </item>
    <item>
      <title>Re: Arduino to HCS12 Serial input POrt output..!!!!!!!!</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Arduino-to-HCS12-Serial-input-POrt-output/m-p/153370#M2229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a sample code of what I am trying to accomplish from teh arduino..&lt;/P&gt;&lt;P&gt;#define DEBUG 0&lt;/P&gt;&lt;P&gt;#define WAIT_FOR_START 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;unsigned char incomingByte = 0;&lt;/P&gt;&lt;P&gt;unsigned long loop_count = 0;&lt;/P&gt;&lt;P&gt;unsigned char horn = 32;&lt;/P&gt;&lt;P&gt;unsigned char redLED = 64;&lt;/P&gt;&lt;P&gt;unsigned char greenLED = 128;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;unsigned char forward = 1;&lt;/P&gt;&lt;P&gt;unsigned char backward = 2;&lt;/P&gt;&lt;P&gt;unsigned char left = 4;&lt;/P&gt;&lt;P&gt;unsigned char right = 8;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;unsigned char PORTB_val;&lt;/P&gt;&lt;P&gt;unsigned char PORTD_val;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;unsigned char in_char = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void setup()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;//PORTD = digital IO 0-7&lt;/P&gt;&lt;P&gt;//horn, redLED, greenLED&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinMode(5, OUTPUT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the digital pin as output&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinMode(6, OUTPUT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the digital pin as output&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinMode(7, OUTPUT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the digital pin as output&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//PORTB = digital IO 8 - 13&amp;nbsp;&lt;/P&gt;&lt;P&gt;//right, left, backwards, forward&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinMode(8, OUTPUT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the digital pin as output&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinMode(9, OUTPUT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the digital pin as output&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinMode(10, OUTPUT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the digital pin as output&lt;/P&gt;&lt;P&gt;&amp;nbsp; pinMode(11, OUTPUT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the digital pin as output&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Serial.begin(9600);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // set up Serial library at 9600 bps&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTD = redLED;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; // turn on the red LED&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; #if DEBUG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; flash_led(3,500);&lt;/P&gt;&lt;P&gt;&amp;nbsp; #endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; wait_for_start();&amp;nbsp; //Waits for startup message from router serial port&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;//continues after receiving it.&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void flash_led(unsigned int count, unsigned int rate)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;// debug routine that flashes an LED&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;int n_count = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;while (n_count &amp;lt; count)&lt;/P&gt;&lt;P&gt;&amp;nbsp;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; n_count++;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; digitalWrite(13, HIGH);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the LED on&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; delay(rate);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // waits for a bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; digitalWrite(13, LOW);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // sets the LED off&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; delay(rate);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // waits for a bit&lt;/P&gt;&lt;P&gt;&amp;nbsp;}&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;char get_char()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;//Function that waits for a character from the serial port&lt;/P&gt;&lt;P&gt;//If none are received, it returns 0.&lt;/P&gt;&lt;P&gt;//The timeout is so that if the router stops sending data to the microcontroller,&lt;/P&gt;&lt;P&gt;//the micrcontroller will stop driving the car, rather than just going forever with&lt;/P&gt;&lt;P&gt;//the last command.&amp;nbsp; Timeout is around 250mS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; while (loop_count &amp;lt; 30000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; loop_count++;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (Serial.available() &amp;gt; 0)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; incomingByte = Serial.read();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; loop_count = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return incomingByte;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; loop_count = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; #if DEBUG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Serial.print('X', BYTE);&lt;/P&gt;&lt;P&gt;&amp;nbsp; #endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;unsigned char wait_for_start()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;//Waits for startup message from router serial port&lt;/P&gt;&lt;P&gt;#if WAIT_FOR_START&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; #if DEBUG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Serial.println("Waiting...");&lt;/P&gt;&lt;P&gt;&amp;nbsp; #endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; while(1)&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (get_char() == 'j' &amp;amp;&amp;amp; get_char() == 'b' &amp;amp;&amp;amp; get_char() == 'p' &amp;amp;&amp;amp; get_char() == 'r' &amp;amp;&amp;amp; get_char() == 'o')&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; #if DEBUG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Serial.print("Passcode Accepted");&lt;/P&gt;&lt;P&gt;&amp;nbsp; #endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void loop()&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;{&amp;nbsp;&lt;/P&gt;&lt;P&gt;//Function that processes input from serial port and drives the car based&lt;/P&gt;&lt;P&gt;//on that input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; in_char = get_char();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; //Split byte received in to upper and lower halves.&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTB_val = in_char &amp;amp; 0x0F;&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTD_val = in_char &amp;amp; 0xF0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; //Make sure the greenLED is turned on now.&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((PORTD_val &amp;amp; greenLED) == 0)&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTD_val = PORTD_val + greenLED;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; //The following IF statements are sanity checks to make sure that FORWARD and BACKWARD cannot be on at the same time&lt;/P&gt;&lt;P&gt;&amp;nbsp; //and that LEFT and RIGHT can't be on at the same time.&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((PORTB_val &amp;amp; (left + right)) == (left + right))&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTB_val = PORTB_val - right;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; if ((PORTB_val &amp;amp; (forward + backward)) == (forward + backward))&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTB_val = PORTB_val - backward;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; //Write the processed values to the ports.&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTD = PORTD_val;&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTB = PORTB_val;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; #if DEBUG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Serial.print(PORTD, HEX);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Serial.print(PORTB, HEX);&lt;/P&gt;&lt;P&gt;&amp;nbsp; #endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2011 05:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Arduino-to-HCS12-Serial-input-POrt-output/m-p/153370#M2229</guid>
      <dc:creator>Looney</dc:creator>
      <dc:date>2011-07-23T05:41:10Z</dc:date>
    </item>
  </channel>
</rss>