<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarrior中的主题 SPI and SS Pin problem</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SPI-and-SS-Pin-problem/m-p/153301#M2221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi I'm using a&amp;nbsp; dsp 56f803. My problem at the moment, I need to raise down the SS pin during sending a spi message an then the SS has to be high(nothing to send). I looked in the Processor Expert, but there it seems that I only can set up the SS signal as an Input but not as an output signal. Has anybody expereince in this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Feb 2009 20:16:16 GMT</pubDate>
    <dc:creator>Freacky2002</dc:creator>
    <dc:date>2009-02-16T20:16:16Z</dc:date>
    <item>
      <title>SPI and SS Pin problem</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SPI-and-SS-Pin-problem/m-p/153301#M2221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi I'm using a&amp;nbsp; dsp 56f803. My problem at the moment, I need to raise down the SS pin during sending a spi message an then the SS has to be high(nothing to send). I looked in the Processor Expert, but there it seems that I only can set up the SS signal as an Input but not as an output signal. Has anybody expereince in this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Feb 2009 20:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SPI-and-SS-Pin-problem/m-p/153301#M2221</guid>
      <dc:creator>Freacky2002</dc:creator>
      <dc:date>2009-02-16T20:16:16Z</dc:date>
    </item>
    <item>
      <title>Re: SPI and SS Pin problem</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SPI-and-SS-Pin-problem/m-p/153302#M2222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;The MCU does not support automatic SS pin handling, therefore you have to set the "Slave select pin" property to "Disabled" and handle the SS pin using BitIO bean and it's methods.&lt;BR /&gt;&lt;BR /&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;BR /&gt;UNIS&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Feb 2009 22:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/SPI-and-SS-Pin-problem/m-p/153302#M2222</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2009-02-17T22:31:38Z</dc:date>
    </item>
  </channel>
</rss>