<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Classic/Legacy CodeWarriorのトピックRe: Crash when stepping into routines - Codewarrior 9.5 (Build 1809) for Macintosh OS 10.5</title>
    <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Crash-when-stepping-into-routines-Codewarrior-9-5-Build-1809-for/m-p/151635#M2131</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm sorry. I made a mistake.&lt;BR /&gt;I'm running this project on OS 10.4.11 - Tiger, not Leopard.&lt;BR /&gt;Code Warrior works mostly fine.&lt;BR /&gt;In my regular "C" project it is prefect.&lt;BR /&gt;It is only in the "C++" project that it fails to step into overloaded methods where there is "glue" code (which I can see in assembly language view).&lt;BR /&gt;-- Bill&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Feb 2009 02:33:07 GMT</pubDate>
    <dc:creator>TigerCoder</dc:creator>
    <dc:date>2009-02-12T02:33:07Z</dc:date>
    <item>
      <title>Crash when stepping into routines - Codewarrior 9.5 (Build 1809) for Macintosh OS 10.5</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Crash-when-stepping-into-routines-Codewarrior-9-5-Build-1809-for/m-p/151633#M2129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I have taken on a project that uses CodeWarrior 9.5 in Mac OS 10.5&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When debugging, if I step into a routine that is unique it works fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But if the routine is a method that is overriding other methods then it crashes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I switch CodeWarrior into Mixed view mode in the debugger, and step via assembly language, stepping over the glue routines, I can arrive at the correct subroutine and switch back to source mode and continue debugging.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But this is horribly time consuming.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I read somewhere that that someone said this started happening after a Mac OS X upgrade.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have any more information on this or a work around so I can get back to work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thankyou so much.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-- Bill.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2009 07:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Crash-when-stepping-into-routines-Codewarrior-9-5-Build-1809-for/m-p/151633#M2129</guid>
      <dc:creator>TigerCoder</dc:creator>
      <dc:date>2009-02-11T07:57:51Z</dc:date>
    </item>
    <item>
      <title>Re: Crash when stepping into routines - Codewarrior 9.5 (Build 1809) for Macintosh OS 10.5</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Crash-when-stepping-into-routines-Codewarrior-9-5-Build-1809-for/m-p/151634#M2130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;CodeWarrior hasn't supported desktop programming for Mac OS and Windows for several years now. Sorry. I'm amazed that CodeWarrior even works at all on Leopard.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2009 21:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Crash-when-stepping-into-routines-Codewarrior-9-5-Build-1809-for/m-p/151634#M2130</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-02-11T21:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: Crash when stepping into routines - Codewarrior 9.5 (Build 1809) for Macintosh OS 10.5</title>
      <link>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Crash-when-stepping-into-routines-Codewarrior-9-5-Build-1809-for/m-p/151635#M2131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm sorry. I made a mistake.&lt;BR /&gt;I'm running this project on OS 10.4.11 - Tiger, not Leopard.&lt;BR /&gt;Code Warrior works mostly fine.&lt;BR /&gt;In my regular "C" project it is prefect.&lt;BR /&gt;It is only in the "C++" project that it fails to step into overloaded methods where there is "glue" code (which I can see in assembly language view).&lt;BR /&gt;-- Bill&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2009 02:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Classic-Legacy-CodeWarrior/Crash-when-stepping-into-routines-Codewarrior-9-5-Build-1809-for/m-p/151635#M2131</guid>
      <dc:creator>TigerCoder</dc:creator>
      <dc:date>2009-02-12T02:33:07Z</dc:date>
    </item>
  </channel>
</rss>